这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

射频与微波

为了满足您的大多数射频和微波测量需求,您可以在这里找到适合的应用和解决方案信息。

请务必查看一下应用指南资料库,详细了解如何使用您的设备以及如何成功完成所需的测量。

是德科技射频和数字技术学习中心――行业专家坐镇,为您的学习提供专业指导

缩小范围

行业/技术

按内容类型

按产品类别

151-175 / 572

排序:
How to Setup and Run Load Pull Simulations: The Basics 
This video introduces basic concepts regarding running load pull simulations. It then uses load pull simulation to find a load impedance that enables you to obtain greater than 43 dBm output power and greater than 55% PAE from a Cree FET.

视频演示 2015-01-27

 
How to Make Accurate, Automated RF Wafer-level Measurements 
The video introduces automation as a way to increase productivity and efficiency. Keysight WaferPro Express measurement software is used to illustrate the various steps in combination with Cascade Microtech Velox software for prober control and Cascade WinCalXE software for automated calibration.

视频演示 2015-01-27

 
How to Design an RF Power Amplifier: Class F 
This short video will provide an introduction to Class F Power Amplifier Design by first building a nonlinear device model and then using this model in a circuit simulation environment to generate the idealized “square” Class F waveforms.

视频演示 2015-01-27

 
How to Design an RF Power Amplifier: Class A, AB and B 
This video provides an introduction to the most basic modes of power amplifier operation by first building a nonlinear device model from scratch and then using this model in a circuit simulation environment to demonstrate various modes of power amplifier operation.

视频演示 2015-01-15

 
How to Apply EM Port Calibration to Improve Simulation Accuracy (MoM) 
This video covers 5 different Momentum calibration methods and shows how the different types of calibration methods impact simulation results along with where and how to use them properly.

视频演示 2015-01-15

 
How to Characterize and Optimize Connector to Board Transition Designs 
This video demonstrates how to accurately model an SMA to PCB transition to obtain agreement between simulated and measured results and how to improve the transition performance.

视频演示 2015-01-15

 
How to Design an RF Power Amplifier: The Basics  
This video provides a foundation for understanding how power amplifier circuits work. If you are new to High Frequency Power Amplifier Circuit Design, this is the place to start.

视频演示 2015-01-15

 
How to Use “Design of Experiments” to Create Robust Designs With High Yield 
This video explains how to use the DOE methodology to help you create and produce robust designs with first pass success and high yield.

视频演示 2015-01-14

 
How to Optimize the Performance of Your RF Layout 
This video shows a practical and effective approach to optimize the performance of your RF layout by parameterizing it and performing EM optimization prior to going to fabrication – thus helping to achieve fist pass success.

视频演示 2015-01-14

 
How to Design RF and Microwave Impedance Matching Networks 
This video describes how to design RF and Microwave impedance matching networks.

视频演示 2015-01-14

 
Keysight Technologies’ GoldenGate Software Release Delivers New and Enhanced Capabilities 
Keysight announces the latest release of GoldenGate software, the industry's most trusted and proven simulation, analysis and verification solution for large-scale RFIC circuit design.

新闻资料 2015-01-13

 
Keysight Unveils Silicon RFIC Interoperability in Latest Advanced Design System Software Release 
Keysight introduces the latest release of its powerful ADS software, ADS 2015. Featuring silicon RFIC interoperability with Cadence’s Virtuoso, GoldenGate-in-ADS, and a host of capabilities intended to increase design efficiency, the Keysight EEsof EDA software, ADS 2015, is changing how silicon RFIC and multi-technology module design is performed.

新闻资料 2015-01-06

 
Keysight Silicon RFIC Design Solutions 
In this video we show the Keysight Silicon RFIC design solutions that help you achieve your goals for designing today´s challenging RFICs and successfully going beyond the IC to verify its performance in higher levels of integration.

基本演示 2015-01-05

 
Keysight Donates $120 Mil. Gift of Software, Support and Training to Georgia Institute of Technology 
Keysight announces the largest in-kind software donation in its longstanding relationship with the Georgia Institute of Technology.

新闻资料 2014-12-10

 
Keysight Receives Global Frost & Sullivan Award for Market Leadership in Instrumentation Software 
Keysight Technologies announces that Frost & Sullivan has recognized Keysight with the 2014 Global Frost & Sullivan Award for Market Leadership in Instrumentation Software for excellence in capturing the highest market revenue within its industry. The award is based on Frost & Sullivan's recent analysis of the instrumentation software market.

新闻资料 2014-12-08

 
Keysight Technologies Unveils Significant FEM Simulation Speed Increase in Latest 3-D EM Simulation  
Keysight announces the latest release of Electromagnetic Professional (EMPro) software, its 3-D electromagnetic simulation software.

新闻资料 2014-12-02

 
Accurate testing of the dielectric properties of powders, liquids and pliable materials – MWI Labora 
Accurate testing of the dielectric properties of powders, liquids and pliable materials – MWI Laboratories and Keysight

Solution Brief 2014-12-01

 
探索 ADS 
Keysight EEsof EDA ADS 视频演示和教程集锦

基本演示 2014-10-28

 
The Impact of Electro-Thermal Coupling on HBT Power Amplifiers 
This paper describes the use of electrothermal simulation to understand, predict, and account for cross-circuit thermal coupling in a commercial HBT power amplifier.

应用说明 2014-10-19

 
Keysight to Demonstrate Latest RF Circuit, System and 3D EM Design and Simulation Solutions at CSICS 
Keysight announces it will demonstrate its latest RF circuit, system and 3D electromagnetic design and simulation solutions at the Compound Semiconductor IC Symposium (CSICS 2014), Hyatt Regency La Jolla at Aventine, San Diego, California, Oct. 19-22. Keysight EEsof EDA is a silver-level sponsor of the event.

新闻资料 2014-10-14

 
ADS Overview Video 
In this video we show the Advanced Design System, ADS, the powerful, easy, and complete design solution for RF, microwave, and high-speed digital designers. See capabilities such as a complete multi-technology design flow including layout and verification, integrated EM, and advanced models such as X-parameters.

基本演示 2014-10-06

 
Millimeter-wave spectrum analysis – OML 
Millimeter-wave spectrum analysis from OML and Keysight

Solution Brief 2014-09-30

 
Keysight Technologies Introduces Industry's Most Comprehensive Reference Solution for Full Character 
Keysight Technologies, Inc. today announced a new PXI Reference Solution for RF power amplifier (PA) characterization and test. The Reference Solution, which performs S-parameter, harmonic distortion, power and demodulation measurements, enables rapid, full characterization of next-generation power amplifier modules, such as a power amplifier-duplexer (PAD).

新闻资料 2014-09-15

 
Keysight Technologies Introduces Design and Test Solutions at European Microwave Week 
Keysight announces that it will demonstrate a wide range of new, high-performance flexible test solutions at the European Microwave Week 2014, Oct. 7–9, Rome, Fiera di Roma, Booth F100. The test solutions are used by engineers for designing and testing components for radar systems, antennas and next-generation wireless devices.

新闻资料 2014-09-03

 
GoldenGate RFIC Solutions 
This brochure highlights the benefits of the GoldenGate RFIC Simulator.GoldenGate is the most trusted simulation, analysis and verification solution available for integrated RF circuit design within Cadence Virtuoso.

手册 2014-09-03

PDF PDF 954 KB

以前 1 2 3 4 5 6 7 8 9 10 ... 下一页