这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

射频与微波

为了满足您的大多数射频和微波测量需求,您可以在这里找到适合的应用和解决方案信息。

请务必查看一下应用指南资料库,详细了解如何使用您的设备以及如何成功完成所需的测量。

是德科技射频和数字技术学习中心――行业专家坐镇,为您的学习提供专业指导

缩小范围

行业/技术

按内容类型

按产品类别

101-125 / 569

排序:
5 Reasons to Buy the X-Series Noise Figure Analyzer - Flyer 
This 2-page flyer lists 5 reasons to buy the X-Series noise figure analyzers

应用说明 2016-01-26

PDF PDF 643 KB
Genesys 2015 Software Enables Industry’s Fastest Realization of RF Systems and Circuits 
Keysight announces the latest release of its industry leading, affordable RF simulation and synthesis software, Genesys 2015. Designed for circuit and system designers, the software features breakthrough Keysight Sys-Parameters that enables RF system simulation with off-the-shelf component datasheets; and comprehensive RF circuit synthesis to enable the industry’s fastest realization of RF systems and circuits.

新闻资料 2016-01-26

 
The Modelithics COMPLETE Library v12.3 for Keysight Technologies' Genesys RF Simulation Tool 
Modelithics announces the release of a new version of The Modelithics® COMPLETE Library, version 12.3, for use with Genesys RF simulation and synthesis software.

新闻资料 2016-01-08

 
TowerJazz Announces New Interoperable PDK for ADS on TPSCo's Advanced 65nm RF CMOS Platform 
TowerJazz's new interoperable PDK targets various applications such as WiFi, Transmitters/Receivers (Tx/Rx), cell phones, tuners, and automotive radar, among others.

新闻资料 2015-12-23

 
Minimizing Design Risk, Shortening Development Time of a Digital Transmission System 
Powerful design and simulation software provides valuable insights to help uncover and solve difficult design challenges at every stage of the design process.

案例分析 2015-12-15

PDF PDF 1.17 MB
Using Automatic Synthesis of RF, Microwave & Analog Circuits to Increase Design Productivity by 10x 
Microwave Product Digest's October 2015 Featured Article written by How-Siang Yap of Keysight Technologies.

专访 2015-10-28

 
Keysight Technologies to Demonstrate Latest Simulation Software Solutions at CSICS 
Keysight announces it will demonstrate its latest RF circuit, system and 3-D electromagnetic design and electro-thermal simulation software solutions at the Compound Semiconductor IC Symposium (CSICS 2015), Sheraton New Orleans, Booth 601, New Orleans, Oct. 11-14.

新闻资料 2015-10-08

 
Keysight Announces RF, Microwave Software Donation to Korea’s Chungnam National University 
Keysight announces its donation of Keysight EDA software to Chungnam National University (CNU) in Daejeon, Korea, as part of the Keysight EEsof EDA University Educational Support Program. This is the third software donation this year, following earlier donations to Korea’s Sogang and Dongguk Universities, and is intended to help CNU foster well-rounded electronics engineering experts.

新闻资料 2015-09-21

 
Keysight EEsof EDA makes it easy to get back to school—at least virtually 
Rick Nelson, executive editor of Evaluation Engineering, visited Keysight Technologies and had this to say about Keysight EEsof EDA.

文章 2015-09-11

 
Discovering Genesys 
A collection of Keysight EEsof EDA Genesys video demonstrations and tutorials

基本演示 2015-08-27

 
Accelerate Your MEMS Device Development & Manufacturing Efficiency Using Impedance Test Instruments 
This brochure describes a general overview of Keysight’s capabilities in MEMS device testing and generates awareness of Keysight impedance MEMS test solution to customer.

手册 2015-08-25

PDF PDF 1.70 MB
How to Design DC-to-DC Converters 
This video introduces basic DC-to-DC converter operation, explains why voltage spikes occur in these circuits, and shows the importance of modeling PC board layout effects. There is an example in which current visualization is used to see potential problem areas in the PC board. The layout is then modified to improve performance.

视频演示 2015-08-24

 
Keysight Demonstrates Latest Design, Test, Characterization Solutions at European Microwave Week 
Keysight announces that it will demonstrate a wide range of design, test and characterization solutions at European Microwave Week 2015, Palais des Congrès, Booth E 110, Paris, Sept. 8–10.

新闻资料 2015-08-24

 
Keysight Technologies' University Educational Support Programs Now in More Than 200 Universities 
Keysight announces that more than 200 universities in North America are now participating in the Keysight EEsof EDA University Educational Support Programs, which provide several thousand students with EDA software licenses.

新闻资料 2015-08-20

 
Oscillator Synthesis 
Learn the foundations of practical RF oscillation design in understanding the interaction of loop gain, zero phase crossing, phase slope and resonator characteristics on oscillator performance and transient startup. Then know how to select from 19 types of oscillator topologies and design them quickly with automatic calculation and optimization of component values through oscillator circuit synthesis.

基本演示 2015-08-15

 
Splitter, Coupler, Balun and Attenuation Synthesis 
Learn about RF/microwave signal control using splitters, combiners, couplers, baluns and attenuators. Then quickly design from 27 different popular topologies such as Wilkinson splitter, Lange Coupler and 90 degree branch line including generation of their distributed layouts on microstrips using signal control synthesis.

基本演示 2015-08-15

 
Equalization Network Synthesis 
Learn how to quickly design active and passive equalization networks to correct for group delay and phase distortions in your RF systems or circuits such as filters and amplifiers defined by measured S-parameters or equivalent circuits. Automatically calculate and optimize component values of analog equalization networks with equalization network synthesis.

基本演示 2015-08-15

 
Phase Locked Loop PLL Synthesis 
Designing phase locked loops (PLL) for frequency synthesizers or frequency/phase modulator/demodulator can be a daunting task because of the multiple interactions of the PLL components such as reference source, loop filter, phase-frequency-detector, divider and VCO. PLL synthesis interactively guides the designer in selecting the appropriate specs for these components in order to achieve the desired balance of loop stability, phase noise and lock time.

基本演示 2015-08-15

 
Passive Filter Synthesis 
Learn how to quickly design LPF, BPF, HPF and Bandstop filters from a complete selection of response shapes such as Chebyshev, Butterworth, Cauer, Bessel or user-defined G-value tables. Automatically calculate LC component values for single-ended or balanced differential topologies for fast realization with passive filter synthesis. Includes singly terminated topologies for diplexer and multiplexer designs.

基本演示 2015-08-15

 
WhatIF Frequency Planning Synthesis 
When selecting LO and IF frequencies in RF systems for receivers or transmitters, it is extremely tideous to identify all interfering frequency mixing spurious and intemod signals that result near the desired IF. Learn how to do frequency planning quickly and interactively compare high-side or low-side mixing to obtain a spurious-free frequency plan that requires minimal filtering. This video also shows how to perform multi-band down conversion frequency planning to a common IF for economical realization.

基本演示 2015-08-15

 
RF Mixer Synthesis 
Learn about RF mixer characteristics and how to select from 11 different passive and active topologies including single ended, balanced, double-balanced and Gilbert Cell for achieving the required frequency translation conversion gain and LO-RF-IF isolation. Then design them quickly with automatic calculation of component values through mixer circuit synthesis.

基本演示 2015-08-15

 
Transmission Line and Advanced Tline Synthesis 
Transmission line synthesis provides 24 types of rectangular and circular transmission line structures for interactive electrical-to-physical or physical-to-electrical synthesis of transmission line parameters such as impedance, even-odd mode impedance, coupling, spacing and width. Learn how to automatically convert a distributed electrical schematic into transmission line structures with automatic insertion and absorption of discontinuities such as chamfered bends, Tee’s, steps and end effects with Advanced Tline synthesis.

基本演示 2015-08-15

 
Active Analog Filter Synthesis 
Learn how to quickly design active analog filters with op-amps from a complete selection of response shapes such as Chebyshev, Butterworth, Bessel Cauer or user-defined G-value tables. Select from all popular topologies such as biquad, elliptic, single or multiple feedback for fast realization with active filter synthesis. Includes singly terminated topologies for diplexer and multiplexer designs.

基本演示 2015-08-15

 
Speed, Accuracy, and Performance in Your RF Module Testing - Eljay Microwave 
Speed, accuracy, and performance in your RF module testing – Eljay Microwave and Keysight

Solution Brief 2015-08-01

 
Optimizing RF and Microwave Spectrum Analyzer Dynamic Range -- Application Note 
The dynamic range of a spectrum analyzer is traditionally defined as the ratio, in dB, of the largest to the smallest signals simultaneously present at the input of the spectrum analyzer that allows measurement of the smaller to a given degree of uncertainty. The signals of interest can either be...

应用说明 2015-07-24

以前 1 2 3 4 5 6 7 8 9 10 ... 下一页