Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Радиоизмерения

Уточнить список

По Отрасли/Технологии

По типу содержания

По типу оборудования

151-175 из 555

Упорядочить:
Recommendations for Port Setup When Using ADS Momentum and Modelithics Models 
This application note is intended to help Advanced Design System (ADS) users using Modelithics models, simulate RF & Microwave circuits. The focus is on finding the optimum port setup for EM simulation of circuit layouts that include surface-mount technology (SMT) devices.

Руководство по применению 2015-02-05

PDF PDF 1.43 MB
How to Setup and Run Load Pull Simulations: The Basics 
This video introduces basic concepts regarding running load pull simulations. It then uses load pull simulation to find a load impedance that enables you to obtain greater than 43 dBm output power and greater than 55% PAE from a Cree FET.

Видеоролики, демонстрирующие решение прикладных задач 2015-01-27

 
How to Design an RF Power Amplifier: Class F 
This short video will provide an introduction to Class F Power Amplifier Design by first building a nonlinear device model and then using this model in a circuit simulation environment to generate the idealized “square” Class F waveforms.

Видеоролики, демонстрирующие решение прикладных задач 2015-01-27

 
How to Make Accurate, Automated RF Wafer-level Measurements 
The video introduces automation as a way to increase productivity and efficiency. Keysight WaferPro Express measurement software is used to illustrate the various steps in combination with Cascade Microtech Velox software for prober control and Cascade WinCalXE software for automated calibration.

Видеоролики, демонстрирующие решение прикладных задач 2015-01-27

 
How to Design an RF Power Amplifier: The Basics  
This video provides a foundation for understanding how power amplifier circuits work. If you are new to High Frequency Power Amplifier Circuit Design, this is the place to start.

Видеоролики, демонстрирующие решение прикладных задач 2015-01-15

 
How to Apply EM Port Calibration to Improve Simulation Accuracy (MoM) 
This video covers 5 different Momentum calibration methods and shows how the different types of calibration methods impact simulation results along with where and how to use them properly.

Видеоролики, демонстрирующие решение прикладных задач 2015-01-15

 
How to Design an RF Power Amplifier: Class A, AB and B 
This video provides an introduction to the most basic modes of power amplifier operation by first building a nonlinear device model from scratch and then using this model in a circuit simulation environment to demonstrate various modes of power amplifier operation.

Видеоролики, демонстрирующие решение прикладных задач 2015-01-15

 
How to Characterize and Optimize Connector to Board Transition Designs 
This video demonstrates how to accurately model an SMA to PCB transition to obtain agreement between simulated and measured results and how to improve the transition performance.

Видеоролики, демонстрирующие решение прикладных задач 2015-01-15

 
How to Optimize the Performance of Your RF Layout 
This video shows a practical and effective approach to optimize the performance of your RF layout by parameterizing it and performing EM optimization prior to going to fabrication – thus helping to achieve fist pass success.

Видеоролики, демонстрирующие решение прикладных задач 2015-01-14

 
How to Use “Design of Experiments” to Create Robust Designs With High Yield 
This video explains how to use the DOE methodology to help you create and produce robust designs with first pass success and high yield.

Видеоролики, демонстрирующие решение прикладных задач 2015-01-14

 
How to Design RF and Microwave Impedance Matching Networks 
This video describes how to design RF and Microwave impedance matching networks.

Видеоролики, демонстрирующие решение прикладных задач 2015-01-14

 
Keysight Technologies’ GoldenGate Software Release Delivers New and Enhanced Capabilities 
Keysight announces the latest release of GoldenGate software, the industry's most trusted and proven simulation, analysis and verification solution for large-scale RFIC circuit design.

Материалы для прессы 2015-01-13

 
Keysight Unveils Silicon RFIC Interoperability in Latest Advanced Design System Software Release 
Keysight introduces the latest release of its powerful ADS software, ADS 2015. Featuring silicon RFIC interoperability with Cadence’s Virtuoso, GoldenGate-in-ADS, and a host of capabilities intended to increase design efficiency, the Keysight EEsof EDA software, ADS 2015, is changing how silicon RFIC and multi-technology module design is performed.

Материалы для прессы 2015-01-06

 
Keysight Silicon RFIC Design Solutions 
In this video we show the Keysight Silicon RFIC design solutions that help you achieve your goals for designing today´s challenging RFICs and successfully going beyond the IC to verify its performance in higher levels of integration.

Демонстрация 2015-01-05

 
Keysight Donates $120 Mil. Gift of Software, Support and Training to Georgia Institute of Technology 
Keysight announces the largest in-kind software donation in its longstanding relationship with the Georgia Institute of Technology.

Материалы для прессы 2014-12-10

 
Keysight Receives Global Frost & Sullivan Award for Market Leadership in Instrumentation Software 
Keysight Technologies announces that Frost & Sullivan has recognized Keysight with the 2014 Global Frost & Sullivan Award for Market Leadership in Instrumentation Software for excellence in capturing the highest market revenue within its industry. The award is based on Frost & Sullivan's recent analysis of the instrumentation software market.

Материалы для прессы 2014-12-08

 
Innovative Passive Intermodulation (PIM) and S-parameter Measurement Solution with the ENA 
This application note introduces the solution that combines PIM and S-parameter measurements by using the vector network analyzer.

Руководство по применению 2014-12-05

Keysight Technologies Unveils Significant FEM Simulation Speed Increase in Latest 3-D EM Simulation  
Keysight announces the latest release of Electromagnetic Professional (EMPro) software, its 3-D electromagnetic simulation software.

Материалы для прессы 2014-12-02

 
Accurate testing of the dielectric properties of powders, liquids and pliable materials – MWI Labora 
Accurate testing of the dielectric properties of powders, liquids and pliable materials – MWI Laboratories and Keysight

Совместное решение 2014-12-01

 
Discovering ADS 
A collection of Keysight EEsof EDA ADS video demonstrations and tutorials

Демонстрация 2014-10-28

 
Realistic Ultra-Wideband Radar Signal Generation Using Keysight SystemVue  
To lower test costs SystemVue can be used with Keysight test equipment to model realistic environment and jamming scenarios, which often involve costly outdoor ranges, chambers, and real-time hardware simulators. Watch the YouTube video to see how.

Демонстрация 2014-10-24

 
The Impact of Electro-Thermal Coupling on HBT Power Amplifiers 
This paper describes the use of electrothermal simulation to understand, predict, and account for cross-circuit thermal coupling in a commercial HBT power amplifier.

Руководство по применению 2014-10-19

 
Keysight to Demonstrate Latest RF Circuit, System and 3D EM Design and Simulation Solutions at CSICS 
Keysight announces it will demonstrate its latest RF circuit, system and 3D electromagnetic design and simulation solutions at the Compound Semiconductor IC Symposium (CSICS 2014), Hyatt Regency La Jolla at Aventine, San Diego, California, Oct. 19-22. Keysight EEsof EDA is a silver-level sponsor of the event.

Материалы для прессы 2014-10-14

 
ADS Overview Video 
In this video we show the Advanced Design System, ADS, the powerful, easy, and complete design solution for RF, microwave, and high-speed digital designers. See capabilities such as a complete multi-technology design flow including layout and verification, integrated EM, and advanced models such as X-parameters.

Демонстрация 2014-10-06

 
Millimeter-wave spectrum analysis – OML 
Millimeter-wave spectrum analysis from OML and Keysight

Совместное решение 2014-09-30

 

Назад 1 2 3 4 5 6 7 8 9 10 ... Следующие