Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Радиоизмерения

1-25 из 48

Упорядочить:
Using Advanced Design System to Design an MMIC Amplifier 
This AN illustrates the design of a MMIC amplifier, problems faced in designing, simulating, and producing a physical layout of an MMIC circuit, validation steps needed to verify that the physical layout.

Руководство по применению 2017-12-05

Программа аттестации студентов по профессиональной подготовке в области разработки ВЧ /СВЧ-устройств 
Программа компании Keysight по аттестации студентов на профессиональную подготовленность в области разработки ВЧ- и СВЧ-устройств позволяет подтвердить уровень технических знаний студентов, наличие у них практических навыков проектирования и измерений при использовании систем автоматизированного проектирования (САПР) радиоэлектронного оборудования Keysight EEsof и измерительных приборов Keysight.

Брошюра 2017-12-01

PDF PDF 681 KB
How to Estimate Voltage Spikes from Layout Parasitic Inductance in Switched-Mode Power Supplies 
We showed you how to deal with layout parasitic inductance in our previous video entitled “How to design DC-to-DC power converters”, but a frequently asked question was “When should I start to worry about layout parasitics inductance? Is there a quick rule of thumb that says kind of ‘Caution: Further investigation’s needed?’” The answer is yes and this follow up video is about how to make these estimates.

Видеоролики, демонстрирующие решение прикладных задач 2017-07-17

 
Keysight EEsof EDA Premier Communications Design Software 
Keysight EEsof EDA premier communications design software product overview brochure.

Брошюра 2017-01-24

PDF PDF 2.54 MB
Unlocking Millimeter Wave Insights 
It is easy to underestimate the challenges at millimeter-wave frequencies, and this amplifies the importance of integrated tools for design, simulation, measurement, and analysis. Learn more about how Keysight is taking the mystique out of millimeter waves and unlocking new insights.

Демонстрация 2016-09-30

 
How to Design Custom RF, Microwave and Analog Filters 
This video shows a custom filter design technique based on Direct or Exact Synthesis in which the filter response is first shaped and customized to meet specifications before a suitable topology is extracted and transformed for the most economical realization.

Видеоролики, демонстрирующие решение прикладных задач 2016-09-01

 
How to Eliminate Layout Induced Oscillations 
This video describes how to predict and ultimately eliminate layout induced oscillation using electromagnetic analysis.

Видеоролики, демонстрирующие решение прикладных задач 2016-06-14

 
Keysight Technologies Announces ADS 2016, its Latest Advanced Design System Software Release 
Keysight introduces the latest release of its powerful Advanced Design System (ADS) software, ADS 2016.

Материалы для прессы 2016-02-04

 
TowerJazz Announces New Interoperable PDK for ADS on TPSCo's Advanced 65nm RF CMOS Platform 
TowerJazz's new interoperable PDK targets various applications such as WiFi, Transmitters/Receivers (Tx/Rx), cell phones, tuners, and automotive radar, among others.

Материалы для прессы 2015-12-23

 
Minimizing Design Risk, Shortening Development Time of a Digital Transmission System 
Powerful design and simulation software provides valuable insights to help uncover and solve difficult design challenges at every stage of the design process.

Пример реального применения 2015-12-15

PDF PDF 1.17 MB
Keysight EEsof EDA makes it easy to get back to school—at least virtually 
Rick Nelson, executive editor of Evaluation Engineering, visited Keysight Technologies and had this to say about Keysight EEsof EDA.

Статья 2015-09-11

 
How to Design DC-to-DC Converters 
This video introduces basic DC-to-DC converter operation, explains why voltage spikes occur in these circuits, and shows the importance of modeling PC board layout effects. There is an example in which current visualization is used to see potential problem areas in the PC board. The layout is then modified to improve performance.

Видеоролики, демонстрирующие решение прикладных задач 2015-08-24

 
Keysight Technologies' University Educational Support Programs Now in More Than 200 Universities 
Keysight announces that more than 200 universities in North America are now participating in the Keysight EEsof EDA University Educational Support Programs, which provide several thousand students with EDA software licenses.

Материалы для прессы 2015-08-20

 
IMS 2015 Demos from Keysight EEsof EDA 
YouTube video playlist containing International Microwave Symposium (IMS) 2015 demo videos from Keysight EEsof EDA MicroApps.

Демонстрация 2015-06-19

 
How to Predict Package and Bondwire Effects on Your RF-Module Designs 
This short video shows how to predict package, board, and bond wire effects on your RF-module designs which subsequently enables you to fix the design prior going to fabrication. The video demonstrates the process of building modules that comprise different technologies and performing EM simulation on them.

Видеоролики, демонстрирующие решение прикладных задач 2015-02-19

 
Recommendations for Port Setup When Using ADS Momentum and Modelithics Models 
This application note is intended to help Advanced Design System (ADS) users using Modelithics models, simulate RF & Microwave circuits. The focus is on finding the optimum port setup for EM simulation of circuit layouts that include surface-mount technology (SMT) devices.

Руководство по применению 2015-02-05

PDF PDF 1.43 MB
How to Apply EM Port Calibration to Improve Simulation Accuracy (MoM) 
This video covers 5 different Momentum calibration methods and shows how the different types of calibration methods impact simulation results along with where and how to use them properly.

Видеоролики, демонстрирующие решение прикладных задач 2015-01-15

 
How to Optimize the Performance of Your RF Layout 
This video shows a practical and effective approach to optimize the performance of your RF layout by parameterizing it and performing EM optimization prior to going to fabrication – thus helping to achieve fist pass success.

Видеоролики, демонстрирующие решение прикладных задач 2015-01-14

 
Keysight Silicon RFIC Design Solutions 
In this video we show the Keysight Silicon RFIC design solutions that help you achieve your goals for designing today´s challenging RFICs and successfully going beyond the IC to verify its performance in higher levels of integration.

Демонстрация 2015-01-05

 
EDA Support Services - Flyer 
Keysight Support Services for EDA Products offers customers several benefits otherwise not available. This service is designed to help you get the most out of your software purchases.

Брошюра 2014-08-03

PDF PDF 454 KB
Keysight EEsof EDA Customer Support - Brochure 
Whether you are a novice or an experienced user, Keysight EEsof EDA’s customer support offerings are designed to help you every step of the way.

Брошюра 2014-08-03

PDF PDF 175 KB
Keysight EEsof EDA Software and Modular Solutions for Universities 
Keysight works in collaboration with universities to provide tools that enable education and research for the engineers of tomorrow. The brochure outlines available programs, software and hardware.

Брошюра 2014-08-03

PDF PDF 1.44 MB
RF and Microwave Industry-Ready Student Certification Program - Brochure 
This program confirms a student’s technical knowledge, design expertise, and hands-on measurement proficiency in the use of Keysight EEsof software design tools and Keysight instruments.

Брошюра 2014-08-03

PDF PDF 562 KB
Momentum 3D-Planar EM Simulation Overview 
In this video we show Keysight Momentum, the gold standard in 3D planar electromagnetic simulation that enables your design of optimum laminar structures.

Демонстрация 2014-08-01

 
Designing RFID Tags Using Direct Antenna Matching 
This Article by Cory Edelman and Murthy Upmaka describes the design challenges involved in RFID design and also focuses on the use of integrated EDA tools to optimally address the challenges.

Статья 2014-07-31

PDF PDF 1.09 MB

1 2 Следующие