이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

RF 및 마이크로웨이브

상세 분류

산업/기술

분야별 검색결과

제품 카테고리별

201-225 / 728

정렬방식:
How to Use Envelope Tracking to Improve Power Amplifier Efficiency 
This video introduces basic concepts regarding applying envelope tracking to improve power amplifier efficiency.

사용방법 동영상 2015-02-10

 
Recommendations for Port Setup When Using ADS Momentum and Modelithics Models 
This application note is intended to help Advanced Design System (ADS) users using Modelithics models, simulate RF & Microwave circuits. The focus is on finding the optimum port setup for EM simulation of circuit layouts that include surface-mount technology (SMT) devices.

어플리케이션 노트 2015-02-05

PDF PDF 1.43 MB
How to Make Accurate, Automated RF Wafer-level Measurements 
The video introduces automation as a way to increase productivity and efficiency. Keysight WaferPro Express measurement software is used to illustrate the various steps in combination with Cascade Microtech Velox software for prober control and Cascade WinCalXE software for automated calibration.

사용방법 동영상 2015-01-27

 
How to Design an RF Power Amplifier: Class F 
This short video will provide an introduction to Class F Power Amplifier Design by first building a nonlinear device model and then using this model in a circuit simulation environment to generate the idealized “square” Class F waveforms.

사용방법 동영상 2015-01-27

 
How to Setup and Run Load Pull Simulations: The Basics 
This video introduces basic concepts regarding running load pull simulations. It then uses load pull simulation to find a load impedance that enables you to obtain greater than 43 dBm output power and greater than 55% PAE from a Cree FET.

사용방법 동영상 2015-01-27

 
How to Design an RF Power Amplifier: The Basics  
This video provides a foundation for understanding how power amplifier circuits work. If you are new to High Frequency Power Amplifier Circuit Design, this is the place to start.

사용방법 동영상 2015-01-15

 
How to Apply EM Port Calibration to Improve Simulation Accuracy (MoM) 
This video covers 5 different Momentum calibration methods and shows how the different types of calibration methods impact simulation results along with where and how to use them properly.

사용방법 동영상 2015-01-15

 
How to Design an RF Power Amplifier: Class A, AB and B 
This video provides an introduction to the most basic modes of power amplifier operation by first building a nonlinear device model from scratch and then using this model in a circuit simulation environment to demonstrate various modes of power amplifier operation.

사용방법 동영상 2015-01-15

 
커넥터-보드 전이 설계를 특성 분석하고 최적화하는 방법  
이 동영상은 시뮬레이션된 결과와 측정된 결과 간의 일치를 확보하기 위해 SMA-PCB 전이를 정확하게 모델링하는 방법과 전이 성능을 개선하는 방법을 시연합니다.

사용방법 동영상 2015-01-15

 
How to Optimize the Performance of Your RF Layout 
This video shows a practical and effective approach to optimize the performance of your RF layout by parameterizing it and performing EM optimization prior to going to fabrication – thus helping to achieve fist pass success.

사용방법 동영상 2015-01-14

 
How to Design RF and Microwave Impedance Matching Networks 
This video describes how to design RF and Microwave impedance matching networks.

사용방법 동영상 2015-01-14

 
How to Use “Design of Experiments” to Create Robust Designs With High Yield 
This video explains how to use the DOE methodology to help you create and produce robust designs with first pass success and high yield.

사용방법 동영상 2015-01-14

 
Keysight Technologies’ GoldenGate Software Release Delivers New and Enhanced Capabilities 
Keysight announces the latest release of GoldenGate software, the industry's most trusted and proven simulation, analysis and verification solution for large-scale RFIC circuit design.

보도자료 2015-01-13

 
Power of Impedance Analyzer - Application Note 
This application note describes the necessity of real-characteristics evaluation, and shows that the impedance analyzers only have capabilities to achieve real-characteristics.

어플리케이션 노트 2015-01-07

University of Utah Goes to Extremes to Investigate the Characteristics of Polar Ice 
Read how Professors Ken Golden and Cynthia Furse and colleagues from the University of Utah used Keysight’s FieldFox handheld analyzer to measure the electromagnetic properties of polar ice

기사 2015-01-07

 
Keysight Unveils Silicon RFIC Interoperability in Latest Advanced Design System Software Release 
Keysight introduces the latest release of its powerful ADS software, ADS 2015. Featuring silicon RFIC interoperability with Cadence’s Virtuoso, GoldenGate-in-ADS, and a host of capabilities intended to increase design efficiency, the Keysight EEsof EDA software, ADS 2015, is changing how silicon RFIC and multi-technology module design is performed.

보도자료 2015-01-06

 
Keysight Silicon RFIC Design Solutions 
In this video we show the Keysight Silicon RFIC design solutions that help you achieve your goals for designing today´s challenging RFICs and successfully going beyond the IC to verify its performance in higher levels of integration.

기본 데모 2015-01-05

 
Keysight EEsof EDA Electronic System Level Design Flow with SystemVue 
In this video we show the Electronic System Level, or ESL, design flow from Keysight based on SystemVue -- the fastest way to design and validate challenging physical layer communications systems, where baseband and RF must work together.

기본 데모 2014-12-12

 
Keysight Donates $120 Mil. Gift of Software, Support and Training to Georgia Institute of Technology 
Keysight announces the largest in-kind software donation in its longstanding relationship with the Georgia Institute of Technology.

보도자료 2014-12-10

 
전력 흐름 및 지향성 커플러 – 어플리케이션 노트 (영어) 
교육 랩(Lab) #6: 전력 흐름 및 지향적 커플러에 관한 대학 엔지니어링 랩(Lab) 시리즈 – 랩(Lab) 6

어플리케이션 노트 2014-12-09

Keysight Technologies Joins NYU WIRELESS to Advance 5G Mobile Technology 
Keysight announces that they have joined the NYU WIRELESS university research center as a key sponsor of the fundamental groundwork that the research center is laying for a new generation of wireless technologies, also known as 5G.

보도자료 2014-12-08

 
Keysight Receives Global Frost & Sullivan Award for Market Leadership in Instrumentation Software 
Keysight Technologies announces that Frost & Sullivan has recognized Keysight with the 2014 Global Frost & Sullivan Award for Market Leadership in Instrumentation Software for excellence in capturing the highest market revenue within its industry. The award is based on Frost & Sullivan's recent analysis of the instrumentation software market.

보도자료 2014-12-08

 
Innovative Passive Intermodulation (PIM) and S-parameter Measurement Solution with the ENA 
This application note introduces the solution that combines PIM and S-parameter measurements by using the vector network analyzer.

어플리케이션 노트 2014-12-05

PDF PDF 690 KB
Keysight Technologies and Kwangwoon University Radio Research Center Co-host 5G and mmWave Workshop 
Keysight Technologies co-hosted a 5G and millimeter-Wave (mmWave) workshop with Kwangwoon University Radio Research Center, Seoul, South Korea. The 5G event, held in October, was the first co-hosted event in the region with over 190 in attendance.

보도자료 2014-12-04

 
Keysight Technologies Unveils Significant FEM Simulation Speed Increase in Latest 3-D EM Simulation  
Keysight announces the latest release of Electromagnetic Professional (EMPro) software, its 3-D electromagnetic simulation software.

보도자료 2014-12-02

 

이전 1 2 3 4 5 6 7 8 9 10 ... 다음