Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Fundamentals of Electronic Test & Measurement

  • Browse the application notes, seminars, and training classes here for measurement techniques.
  • Be sure to visit our forums for the latest discussions.
     

Уточнить список

убрать все фильтры

По типу содержания

По типу оборудования

1-15 из 15

Упорядочить:
Keysight PXIe Chassis Cooling Guidelines - White Paper 
Module temperatures in a PXI system can impact operating conditions. It’s important to actively manage the environment inside your chassis.

Руководство по применению 2018-08-27

PDF PDF 702 KB
Choosing the Test System Software Architecture - Application Note 
This application note is designed to help you quickly design a test system that produces reliable results and meets throughput requirements within budget. It explores the entire software development process, from gathering and documenting software requirements through design reuse considerations.

Руководство по применению 2017-12-05

Boosting PLL Design Efficiency From free-running VCO characterizations to closed-loop PLL evaluation 
This application note describes introduces practical solutions for VCO/PLL performance evaluation and gives actual examples of parameter measurements using the E5052B.

Руководство по применению 2008-11-21

Building Hybrid Test Systems. Ensuring success in two common development scenarios - Application Not 
Application Note 1465-33. When you migrate to a hybrid system that includes LXI along with GPIB, VXI, PXI, or any other architecture, two scenarios are most typical, minimum development time and maximum overall performance

Руководство по применению 2008-10-15

Best of 8 Hints for Making Better Oscilloscopes Measurements  
Keysight engineers sharing ideas of how to use the equipment they design

Руководство по применению 2008-03-17

PDF PDF 320 KB
Using LAN in Test Systems: Applications (1465-14) - Application Note and Example Programs 
Topics include balancing cost, convenience and security in three common LAN scenarios: sharing instruments, remote monitoring and data acquisition, and functional test systems. Includes downloadable example programs.

Руководство по применению 2005-04-01

 
Using LAN in Test Systems: Setting up System I/O (AN 1465-15) - Application Note 
This set of application notes shows you how to simplify test system integration by utilizing open connectivity standards such as local area networking (LAN). The collective goal of these notes is to help you produce reliable results, meet your throughput requirements and stay within your budget.

Руководство по применению 2005-03-29

PDF PDF 263 KB
Test-System Understanding Drivers and Direct I/O (AN 1465-3) - Application Note 
This application note answers common questions about the use of drivers and direct I/O to send commands from a PC application to the test instrument.

Руководство по применению 2004-12-21

PDF PDF 374 KB
Using SCPI and Direct I/O vs. Drivers (AN 1465-13) - Application Note 
Using SCPI and Direct I/O vs. Drivers, the fifth note in the series, outlines the relationship between input/output (I/O) software, application software and the ability to maximize instrument interchange and software reuse in present and future systems

Руководство по применению 2004-12-13

PDF PDF 408 KB
Test-System Computer I/O Considerations (AN 1465-2) - Application Note 
The first application note in the series, Introduction to Test-System Design, covers test-system philosophy and planning and discusses how test is used in three sectors: R&D, design validation and manufacturing

Руководство по применению 2004-12-09

PDF PDF 189 KB
Using USB in the Test and Measurement Environment (AN 1465-12) - Application Note 
Simplify test integration with USB interface. Whether you’re setting up an ad hoc system on a lab bench or designing a permanent solution for a manufacturing line, the three best choices today for connecting modern instrumentation to computers are GPIB, LAN, and USB.

Руководство по применению 2004-11-19

PDF PDF 194 KB
System Developer Guide Using LAN in Test Systems - PC Configuration (AN 1465-11) - Application Note 
Using LAN in Test Systems: PC Configuration,the third note in the series, describes the additional capabilities required to enable communication between a PC and LAN-enabled instrumentation. This note is a companion to Application Notes 1465-9 and 1465-10.

Руководство по применению 2004-10-19

PDF PDF 204 KB
Using LAN in Test Systems - Network Configuration (AN 1465-10) - Application Note 
The decision to use LAN in a test system delivers important benefits to your company and your team. From a business perspective, intense competition among equipment vendors has produced a wide selection of high quality, low-cost solutions for local area networking

Руководство по применению 2004-09-14

Using LAN in Test Systems - The Basics (AN 1465-9) - Application Note 
The basic purpose of any test system is to characterize and validate the performance of electronic components, assemblies or products. The complexity of this task depends on variables such as the physical nature of the device under test (DUT), the number of tests to be performed, the number of signals to be measured and the desired time per test.

Руководство по применению 2004-07-29

PDF PDF 270 KB
8 More Hints for Making Better Scopes Measurements 
This Application Note contains a variety of hints to help you understand and improve your use of oscilloscopes. It includes the following 8 hints: 1. Don't forget to check that probe 2. A quick, easy way to troubleshoot mixed hardware/software prototypes 3. Using scopes to measure noisy signals 4...

Руководство по применению 1999-12-01

PDF PDF 840 KB