Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

Basics & Measurement Fundamentals

1-3 sur 3

Tri:
RF & Microwave Measurement Fundamentals 
This 4-day class studies the principles of microwaves on transmission lines and power measurements, signal sources, mixers and modulation techniques, and the use of signal types in test applications.

Formation en classe

 
Transmission Line Fundamentals 
Accelerated Education Curriculum:Understand the need for transmission line

Formation en classe

 
Bluetooth Technology Fundamentals 
This 1-day course covers the applications for this new technology, the structure of the Bluetooth system architecture and the setup of so called short-range ad hoc networks will be introduced.

Formation en classe