検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

RF&マイクロ波

1-25 / 302

並べ替え
RF and Microwave Industry-Ready Student Certification Program 
This program confirms a student’s technical knowledge, design expertise, and hands-on measurement proficiency in the use of Keysight EEsof EDA software design tools and Keysight instruments.

ブローシャ 2019-10-04

PDF PDF 1.07 MB
Keysight EEsof EDAユーザ向けメールマガジン -- しみゅレター 
キーサイトEDAソリューションの技術情報やアプリケーション情報を定期的にお知らせするEメールニュースレターです。

ニュースレター 2019-06-26

 
Ericsson and Freiburg U. Design High-Q Power Harvesting Circuit Using ADS 
ADS HB was used to explore the design space around the innovative impedance transformation using a high Q quartz crystal resonator to transform the low voltage from the low impedance antenna.

事例紹介 2019-03-14

PDF PDF 2.37 MB
Making Better Models with User Data 
This paper details the process of combining MATLAB and the RF System analysis to improve the accuracy of simulations via personalized models.

アプリケーション・ノート 2019-03-05

PDF PDF 4.64 MB
How to Solve Signal Integrity Problems: The Basics 
How to Solve Signal Integrity Problems: The Basics shows you how to use basic signal integrity (SI) analysis techniques such as eye diagrams, S-parameters, time-domain reflectometry (TDR) and single pulse response to solve signal integrity problems.

使用法の説明ビデオ 2018-09-18

 
YouTubeのADSビデオライブラリ 
YouTubeのKeysight EEsof EDAのチャネルのAdvanced Design System(ADS)のビデオライブラリのプレイリスト

デモ 2018-07-26

 
Modelithics® COMPLETE Library and NEW mmWave & 5G Library Released for ADS 
The newest version of the Modelithics® COMPLETE Library for Keysight Advanced Design System (ADS) has just been released, adding 19 new models plus new dynamic layouts for active device models.

プレス資料 2018-04-02

 
GLOBALFOUNDRIES Launches RF Ecosystem Program to Accelerate Time-to-Market 
GLOBALFOUNDRIES Launches RF Ecosystem Program to Accelerate Time-to-Market for Wireless Connectivity, Radar and 5G Applications.

プレス資料 2018-03-20

 
Simulation and Verification of Pulse Doppler Radar Systems - Application Note 
Keysight SystemVue illustrates key algorithms in modern Pulsed Doppler radar system design, and also connects to Keysight sources and signal analyzers to verify hardware performance.

アプリケーション・ノート 2017-12-01

PDF PDF 10.43 MB
Keysight SystemVueを使用したアンテナ/MIMOチャネル効果の評価 
。このアプリケーションノートでは、キーサイトのW1715 MIMOチャネルビルダーを使用することによって実現した2つのMIMOチャネルモデル(すなわち、ジオメトリーベースのモデルと相関ベースのモデル)について説明し、アンテナ効果とチャネル特性がチャネルモデルの中でどのように組み合わされているかを示します。

アプリケーション・ノート 2017-07-31

How to Estimate Voltage Spikes from Layout Parasitic Inductance in Switched-Mode Power Supplies 
We showed you how to deal with layout parasitic inductance in our previous video entitled “How to design DC-to-DC power converters”, but a frequently asked question was “When should I start to worry about layout parasitics inductance? Is there a quick rule of thumb that says kind of ‘Caution: Further investigation’s needed?’” The answer is yes and this follow up video is about how to make these estimates.

使用法の説明ビデオ 2017-07-17

 
EDAcafé - DAC 2017 Interview: Michel Azarian, Silicon RFIC EDA Program Manager 
Sanjay Gangal from EDAcafé interviews Michel Azarian (Keysight Technologies' Silicon RFIC EDA Program Manager) at Design Automation Conference (DAC) 2017.

デモ 2017-06-22

 
Keysight Demonstrates Latest Design, Simulation, Verification Solutions at DAC 
Keysight Technologies will showcase the newest releases of its EDA software for RF-microwave circuit and system, high-speed digital, electronic system level, 3-D electromagnetic, and device-modeling applications at the 54th annual Design Automation Conference (www.dac.com), the premier conference for design and automation of electronic systems.

プレス資料 2017-06-14

 
Video Clips from the "Four Ways to Boost Simulation Data Processing using Python" Webcast 
Watch these powerful video clips from the Keysight webcast, "Four Ways to Boost Simulation Data Processing using Python".

デモ 2017-06-12

 
Electrothermal Simulation using the Wolfspeed ADS PDK  
This is a short demonstration of how the Wolfspeed ADS PDK is configured to work with the ADS electrothermal simulator to co-simulate electrical and thermal performance. This allows designers to quickly understand the impact of thermal effects on their circuit designs, and account for those effects during the design process.

デモ 2017-06-02

 
Keysight Technologies to Present a Vision for 5G Evolution at WAMICON 2017  
Keysight experts will be at WAMICON 2017, an annual IEEE Wireless and Microwave Conference, to discuss everything from circuit-level modeling to system verification for general RF, microwave, millimeter wave for 4G, emerging 5G communications, and aerospace & defense.

プレス資料 2017-04-10

 
New Modelithics COMPLETE Library Release v17.0 for ADS Represents over 15,000 Components 
Modelithics announces the latest release of the Modelithics COMPLETE Library version 17.0 for use with Advanced Design System (ADS) simulation software.

プレス資料 2017-02-15

 
Synthesis Made Easy With Keysight Genesys  
Learn how to quickly design many different RF circuits with various topologies in these short tutorial videos. These step-by-step tutorials walk you through the steps to accelerate your routine design tasks from hours to minutes with automatic RF circuit and system synthesis tools.

デモ 2016-12-01

 
Integrating Multiple Technology Devices onto Laminate-Based Multi-Chip-Modules 
Microwave Product Digest (MPD) featured article on "Integrating Multiple Technology Devices onto Laminate-Based Multi-Chip-Modules Using an Integrated Design Flow", written by Keefe Bohanan, Applications Engineer District Manager for Keysight EEsof EDA.

記事 2016-11-29

PDF PDF 3.90 MB
Direct-Synthesis Software Approach Facilitates Filter Design 
This Microwaves & RF article discusses how Genesys software can be used to design filters with the direct-synthesis technique. A lowpass filter example is presented to illustrate the software’s capabilities.

記事 2016-11-28

 
Using DSP and RF circuit co-design to reduce risk and cost 
For modern design organizations, it’s now more imperative than ever that they simulate both Digital Signal Processor (DSP) and RF circuits together at the system level using mixed signals.

記事 2016-10-11

 
The High-Frequency, High Speed Design Revolution: Why Your Design & Test Flow Will Soon Be Obsolete 
In this keynote from EDI CON USA 2016, Todd Cutler, vice president and general manager of Keysight Design & Test Software, discusses these trends and explains how, when coupled with market pressures, they are driving a revolution in the design and measurement industry.

デモ 2016-10-11

 
Software plus signal generators and analyzers support IEEE 802.11p design and test 
Jungik Suh, marketing program manager, Automotive & Energy Solutions, Keysight Technologies, provides input on several Keysight solutions for the connected-car arena for Evaluation Engineering's October print special report on automotive test.

記事 2016-10-05

 
Unlocking Millimeter Wave Insights 
It is easy to underestimate the challenges at millimeter-wave frequencies, and this amplifies the importance of integrated tools for design, simulation, measurement, and analysis. Learn more about how Keysight is taking the mystique out of millimeter waves and unlocking new insights.

デモ 2016-09-30

 
Genesys S/FilterソフトウェアによるカスタムRF/マイクロ波/アナログフィルターのシンセシス 
RF/マイクロ波/アナログフィルターの従来のデザイン手法は、テンプレートを使用するもので、応答の形状とフィルターのトポロジーは、ButterworthやChebyshevなどの標準フォーマットに固定されています。これに対して、この技術記事では、これより汎用的なデザイン手法であるダイレクトシンセシスと回路変換を用いる手法を紹介します

アプリケーション・ノート 2016-09-23

1 2 3 4 5 6 7 8 9 10 ... 次へ