您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

元件與特定裝置

縮小範圍

移除所有細分

依產業/技術

依內容類型

1-25 / 28

排序:
Validating Automotive Ethernet Conformance and Performance - Case Study 
This case study explores how the BMW Group was successful in validating their automotive Ethernet toolchain, getting visibility into the performance and robustness of the switches integrated in ECUs.

案例研究 2017-11-03

PDF PDF 536 KB
University Uses ADS to Create an Impedance Matching Method for Wireless Battery Charging  
Learn how NCKU created an impedance matching method for wireless battery charging using Keysight ADS.

案例研究 2017-10-07

PDF PDF 683 KB
STMicroelectronics & ESEO Use ADS To Design a 2.45 GHz Wireless Power Scavenging Circuit 
Learn how STMicroelectronics and ESEO designed a 2.45 GHz wireless scavenging circuit using Advanced Design System (ADS).

案例研究 2017-06-07

PDF PDF 539 KB
Early Design Review or Boundary Scan in Enhancing Testability and Optimazation of Test Strategy 
With complexities of PCB design scaling and manufacturing processes adopting to environmentally friendly practices raise challenges in ensuring structural quality of PCBs.

專文 2017-05-08

PDF PDF 624 KB
STMicroelectronics and University of Lyon Predict EMI Using ADS - Case Study 
Learn how STMicroelectronics and University of Lyon designers used ADS to develop a network parameter block technique to satisfy their need for accurate and general EMI modeling.

案例研究 2017-03-17

PDF PDF 509 KB
Software plus signal generators and analyzers support IEEE 802.11p design and test 
Jungik Suh, marketing program manager, Automotive & Energy Solutions, Keysight Technologies, provides input on several Keysight solutions for the connected-car arena for Evaluation Engineering's October print special report on automotive test.

專文 2016-10-05

 
Testing a Network Communication PCBA from Prototype to Manufacturing - Article Reprint 
Early implementation of BST can cut test costs and time.

專文 2016-02-17

PDF PDF 178 KB
The Boundary Scan Toolbox - Article Reprint 
Find out how boundary scan can enable embedded and other value-added test in your toolbox.

專文 2016-02-16

PDF PDF 409 KB
New IEEE Standards for Board and System Tests - Article Reprint 
This article highlights of changes to IEEE Std 1149.1, IEEE Std 1149.6, IEEE P1149.10 and IEEE P1838.

專文 2016-02-16

PDF PDF 190 KB
I'm a Board Test Engineer and I'm Loving It! - Article Reprint 
Life on the road can be relentless, but it’s never boring. Find out why from this personal story of a test engineer.

專文 2016-02-12

PDF PDF 178 KB
Emulating Analog Input Sensors in Automotive Electronics Functional Test - Article Reprint 
This article discusses guidelines for evaluating the digital-analog converters for your automotive electronics functional test needs.

專文 2016-02-09

PDF PDF 318 KB
Manufacturing Test Solutions for SSDS - Article Reprint 
A new system performs both ICT and boundary scan in high-volume settings.

專文 2016-02-09

PDF PDF 222 KB
Testing the Internet of Things - Article Reprint 
Connectivity is embedded in the electronics ecosystem. And test should be embedded in the devices that support it.

專文 2016-02-09

PDF PDF 79 KB
Tester for Hire - Article Reprint 
This article explores the possibility of renting test equipment to help electronics manufacturers juggle capacity according to production demand and available resources.

專文 2016-02-09

PDF PDF 381 KB
Finding Fault - Article Reprint 
testing mission-critical functions in automotive electronics.

專文 2016-02-05

PDF PDF 452 KB
Making Boundary Scan Easy - Article Reprint 
Testing boundary scan devices no longer need be a laborious task.

專文 2016-02-03

PDF PDF 217 KB
Testing of Small Form-Factor Products - Article Reprint 
Boundary scan and embedded test will need to make up for ICT gaps.

專文 2016-02-03

PDF PDF 546 KB
Testing New Grounds in Automotive Electronics - Article Reprint 
Manufacturers are increasingly designing products for ease of test.

專文 2016-02-02

PDF PDF 279 KB
Automating In-Circuit Test - Article Reprint 
Inline ICT is not as cumbersome as it used to be, and in the longer run, will help manufacturers save costs.

專文 2016-02-02

PDF PDF 87 KB
Principal Component Analysis-Based Compensation for Measurement Errors 
This paper examines some issues and trends that justify adding features to IEEE 1149.1 that will facilitate safe, fast and effective initialization of a board or system, to get it ready for testing. Published with kind permission of the IEEE

專文 2015-06-08

PDF PDF 1.86 MB
Comparing Boundary Scan Methods White Paper 
The need for reusable tests is driving standalone boundary scan-ICT integration. This article first appeared in the September 2009 issue of Circuits Assembly and is reprinted with kind permission.

專文 2014-07-31

PDF PDF 2.75 MB
Realization and Analysis of Electronically Steerable Phased Array using Scripting & Parameterization 
With the advent of multi-core, high speed processors and abundant memory availability, complex designs using 3-D full-wave electromagnetic (EM) tools have become common choice for microwave and antenna engineers.

專文 2013-07-09

 
Testing DDR Memory; How On-Chip DFT Helps 
This paper discusses DDR memory testing challenges we see today, and how the adoption of DFT capabilities pays off in higher test coverage, better diagnostics and reduced programming/support time.

專文 2012-04-17

PDF PDF 530 KB
Boundary-Scan Advanced Diagnostic Methods 
This paper illustrates how usage of boundary scan circuit information and predictive analysis of potential assembly faults will provide more precise and accurate diagnostic information.

專文 2012-04-17

PDF PDF 1.20 MB
Solutions for Undetected Shorts on IEEE 1149.1 Self-Monitoring Pins 
This paper presents the problem of undetected shorts on IEEE 1149.1 compliant self-monitoring pins, and potential mitigating solutions.

專文 2010-12-10

PDF PDF 789 KB

1 2 下一頁