这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

航空航天与国防

此内容需要使用支持JavaScript的浏览器和Adobe Flash Player

获得Flash 

集中精力完成重要任务

航空航天与国防行业的任务正在不断发展和变化,但是有一点始终未变,那就是必须要保证那些从事危险工作的人员的人身安全。这项任务能否成功,取决于人员和技术如何适应变化,实现完美融合。随着系统技术日趋复杂,达到这一目标也变得越来越困难。

是德是您成功完成任务的保证。借助是德在测量科学和测试流程中的专业技术,您可以腾出更多时间来处理更重要的问题:执行当前任务并按计划转向未来任务。有是德保证您的系统就绪,您完全可以高枕无忧,从而集中精力完成更重要的任务。

有关是德在航空航天/国防领域的作用的更多信息,请下载免费手册 《是德在航空航天与国防领域的作用》。

查看测量解决方案实例有源天线测试多发射机环境测试信号

1-16 / 16

排序:
Introducing SystemVue 2016 
See a live demo of SystemVue 2016. The new capabilities enable researchers and system architects working on platforms using beamforming algorithms for 5G, satellite, NewSpace, radar and EW applications, to reduce interference and power consumption, while increasing physical range.

基本演示 2016-06-27

 
NewSpace and Traditional Space panel session– recorded at the NewSpace 2015 conference 
Streamed live on July 16, 2015, this video is a panel discussion of important key players in the NewSpace arena.

基本演示 2016-02-02

 
Precision Validation of Radar System Performance in the Field Using FieldFox 

基本演示 2014-03-21

 
Realistic Ultra Wideband Radar Signal - Demo 
Testing of radar systems can be extremely time-consuming and expensive. Radar transceivers must be designed and tested with realistic environment and jamming scenarios, which often involve costly outdoor ranges, chambers, and real-time hardware simulators.

基本演示 2013-11-25

 
EVM measurement with the new M8190A Arbitrary Waveform Generator - video  
To meet the high demands of aerospace/ defense application tests, it is indispensable to simulate real-life scenarios with precision arbitrary waveforms. In a test setup with a high error vector magnitude (EVM), problems within your device under test may not be discovered. With signals close to reality, the Keysight M8190A is the perfect solution.

基本演示 2012-08-20

 
Reconfigurable Radar Design: Debug and Validation - video 
This video demonstrates how to debug and validate reconfigurable radar design with Keysight test and measurement instruments and software.

基本演示 2012-07-30

 
Microwave Switch Repeatability Demonstration - video 
This video compares the repeatability performance of a Keysight microwave switch with a competitor’s offering. Performance is compared by measuring the insertion loss across a frequency range, then comparing the relative difference of each insertion loss measurement.

基本演示 2012-06-11

WMF WMF 17.78 MB
OFDMA Concepts Demonstration - channel training sequence - video 
This video describes one of the key concepts of Orthogonal Frequency Division Multiple Access (OFDMA) modulation. This video illustrates how a channel training sequence can be used to discern two distinct transmission streams in a MIMO (Multiple In Multiple Out) Antenna configuration.

基本演示 2012-06-11

WMF WMF 20.57 MB
Interference Mitigation Through the Use of Wideband Signal Recording and Analysis - video  
This video describes the process to find and analyze the cause of a radio signal that is interfering with a wireless LAN transmitter. This requires the continuous capture of wireless spectrum, tools to search and find possible interferers as well as tools to determine how an interferer may affect the LAN signal.

基本演示 2012-06-11

WMF WMF 33.25 MB
OFDMA Concepts Demonstration - channel training sequence - video  
This video describes one of the key concepts of Orthogonal Frequency Division Multiple Access (OFDMA) modulation. This video illustrates how a channel training sequence can be used to discern two distinct transmission streams in a MIMO (Multiple In Multiple Out) Antenna configuration.

基本演示 2012-05-10

 
Reproducing DC Power Transients, Using an N6705B DC Power Analyzer to Create Transients - video 
DC power transients can easily be reproduced with N6705B DC Power Analyzer. Power transients can be used to test a DUT resilience to a change in voltage. Two examples are provided an automobile's voltage during engine turn-on and a PS interrupt specified in the DO-160F avionics test manual. Transients can also occur when the load on a PS changes.

基本演示 2012-05-10

 
Measuring Performance of Wide Bandwidth Radar Transmitters 
Short videos on measuring performance of wide bandwidth radar transmitters.

基本演示 2011-04-21

 
Self-diagnosing Switch Matrix 
Self-diagnosing Switch Matrix

基本演示 2011-02-16

 
Signal Studio for Global Navigation Satellite Systems N7609B Video Demonstrations 
View this series of three videos which will provide an introduction to the N7609B Signal Studio for Global Navigation Satellite Systems (GNSS) software and demonstrates some of the key features of the software.

基本演示 2010-03-30

 
P-Series Power Meter Radar Video Demonstrations 

基本演示 2009-04-01

 
E3238S / 35688E Product Tour DVD 

基本演示 2006-11-28

PDF PDF 185 Bytes