検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

航空宇宙/防衛

ご覧になるためには、ブラウザのJavascriptを有効にしてください。また、Adobe Flash Player が必要です。

Flash ダウンロード 

重要な場所に集中可能

ミッションは進化しますが、常に変わらないことが1つあります。すなわち、危険な状況にいる人々を保護する必要性です。成功は、作業に果たす人とテクノロジーに依存します。テクノロジーが複雑化しているため、用意ができたことを確認する作業はますます困難になっています。

Keysightは、ミッションの成功をサポートします。Keysightの測定やテスト・プロセスにおける専門知識を活用することで、お客様に、現在のミッションの達成、次に起こるイベントへの対処といったより大きな課題に取り組む時間的な余裕が生まれます。Keysightがシステムの準備作業を支援することにより、リソースを最も重要な場所に集中することが可能になります。

測定ソリューション例をご覧ください。アクティブ・アンテナ・テスト,マルチエミッタ・テスト信号

絞込み

絞込みのリセット

業種/テクノロジー

コンテンツのタイプ

製品カテゴリ

1-12 / 12

並べ替え
ハイブリッド・テスト・システムの構築、パート2 
ハイブリッド・テスト・システムの構築、パート2

アプリケーション・ノート 2008-10-15

GPIBからLXIへの移行(システム・ソフトウェア編) 
本書は、相対的な性能の向上と、それを実現するための移行方法を説明します。相対的な違いを比較するために、サンプルを作成し、その性能を4種類のI/O手法で測定し、GPIBからLANへの移行後の性能レベルを予想しました。

アプリケーション・ノート 2007-03-07

Using LAN in Test Systems: Applications (1465-14) - Application Note and Example Programs 
Topics include balancing cost, convenience and security in three common LAN scenarios: sharing instruments, remote monitoring and data acquisition, and functional test systems. Includes downloadable example programs.

アプリケーション・ノート 2005-04-01

 
Using LAN in Test Systems: Setting up System I/O (AN 1465-15) - Application Note 
This set of application notes shows you how to simplify test system integration by utilizing open connectivity standards such as local area networking (LAN). The collective goal of these notes is to help you produce reliable results, meet your throughput requirements and stay within your budget.

アプリケーション・ノート 2005-03-29

PDF PDF 263 KB
Test-System Understanding Drivers and Direct I/O (AN 1465-3) - Application Note 
This application note answers common questions about the use of drivers and direct I/O to send commands from a PC application to the test instrument.

アプリケーション・ノート 2004-12-21

PDF PDF 374 KB
Using SCPI and Direct I/O vs. Drivers (AN 1465-13) - Application Note 
Using SCPI and Direct I/O vs. Drivers, the fifth note in the series, outlines the relationship between input/output (I/O) software, application software and the ability to maximize instrument interchange and software reuse in present and future systems

アプリケーション・ノート 2004-12-13

PDF PDF 408 KB
Test-System Computer I/O Considerations (AN 1465-2) - Application Note 
The first application note in the series, Introduction to Test-System Design, covers test-system philosophy and planning and discusses how test is used in three sectors: R&D, design validation and manufacturing

アプリケーション・ノート 2004-12-09

PDF PDF 189 KB
Using USB in the Test and Measurement Environment (AN 1465-12) - Application Note 
Simplify test integration with USB interface. Whether you’re setting up an ad hoc system on a lab bench or designing a permanent solution for a manufacturing line, the three best choices today for connecting modern instrumentation to computers are GPIB, LAN, and USB.

アプリケーション・ノート 2004-11-19

PDF PDF 194 KB
System Developer Guide Using LAN in Test Systems - PC Configuration (AN 1465-11) - Application Note 
Using LAN in Test Systems: PC Configuration,the third note in the series, describes the additional capabilities required to enable communication between a PC and LAN-enabled instrumentation. This note is a companion to Application Notes 1465-9 and 1465-10.

アプリケーション・ノート 2004-10-19

PDF PDF 204 KB
Using LAN in Test Systems - Network Configuration (AN 1465-10) - Application Note 
The decision to use LAN in a test system delivers important benefits to your company and your team. From a business perspective, intense competition among equipment vendors has produced a wide selection of high quality, low-cost solutions for local area networking

アプリケーション・ノート 2004-09-14

Using LAN in Test Systems - The Basics (AN 1465-9) - Application Note 
The basic purpose of any test system is to characterize and validate the performance of electronic components, assemblies or products. The complexity of this task depends on variables such as the physical nature of the device under test (DUT), the number of tests to be performed, the number of signals to be measured and the desired time per test.

アプリケーション・ノート 2004-07-29

PDF PDF 270 KB
テスト・システムのソフトウェア・アーキテクチャ 
このアプリケーション・ノートでは、ソフトウェア・コンポーネントの設計、開発に必要な情報を提供しています。

アプリケーション・ノート 2004-07-14