这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

多标准无线(MSR)测试和设计

随着蜂窝网络持续向 3.9G 和 4G 过渡,基站收发信机(BTS)发射机也将全面地过渡到新的阶段。下一代基站发射机和接收机将会支持更宽的带宽,不仅包括采用单一无线制式的多载波(MC),还包括在单一发射机路径中的多种制式。多标准无线(MSR)基站能够同时传输单个单元内不同的无线接入技术(RAT)。例如,它能够同时传输单个 MSR 基站单元中的 GSM、W-CDMA、HSPA 和 LTE MC。MSR 网络可以支持多种制式,这对于降低基站规模和成本而言十分重要。鉴于此,预计 MSR 基站将会从已广泛部署的 2/3G 无线制式顺利而稳定地过渡到 3.9G(例如 LTE)、甚至是 4G(例如 LTE-Advanced)技术。MSR 开发人员面临着单载波系统的所有常见设计问题,以及在单个单元中不同信号之间不良交互所引起的大量潜在问题。是德提供功能强大的 MSR 测试和设计解决方案,其中包括符合 3GPP 第 9 版标准的一键式嵌入测量应用软件和更灵活的、面向未来的产品,从而能够快速适应不断演进的技术和标准。
深入分析。

增强信心。加快下一代无线技术的发展。
 

查看相关视频(优酷) 

1-10 / 10

排序:
是德科技 N9083A 和 W9083A 多标准无线技术 (MSR) X 系列测量应用软件 
是德科技 N9083A 和 W9083A 多标准无线技术 (MSR) X 系列测量应用软件

技术总览 2017-11-27

Unlocking Cellular Measurement Insights - Solution Brochure 
This brochure covers the intricacies of evolving cellular standards to provide our customers with valuable insights into their innovations from design and development into manufacturing.

手册 2016-06-22

PDF PDF 7.93 MB
Solutions and Measurement Tools for Use in Average Power and Envelope Tracking Design - Application  
This app note provides an outline of the techniques involved and the solutions Agilent provides for RF, baseband and system developers.

应用说明 2014-08-02

免费下载最新的“Power of Wireless(强大的无线技术)”应用指南 
Learn about the Power of Wireless – Keysight’s suite of test products that help you get your innovative, higher-performing designs to market before your competition.

促销资料 2014-04-11

 
免费下载最新无线应用指南 
免费下载最新无线应用指南

促销资料 2014-04-11

 
Anticipate Multi-Standard Radio (MSR) Performance with Keysight SystemVue  
As mobility carriers embrace 4G LTE technology, new equipment must co-exist with older 2G/3G standards. Multi-Standard Radio (MSR) testing characterizes these interactions, and is supported by a variety of Keysight test products. Keysight SystemVue, a system-level modeling environment for communications physical layer, enables R&D engineers to anticipate these interactions, achieve more robust system designs, then connect to Test to validate simulated performance using real hardware.

基本演示 2012-02-18

 
Agilent Technologies Announces 42-Mbps DC-HSDPA IP Data Throughput Solution for the 8960 Wireless 
The Agilent E5515E delivers sustained, end-to-end IP data throughput at 42 Mbps, flexible and comprehensive RF measurements, and improved hardware capability for future requirements, making it easy and fast to stress wireless devices and verify their performance at full data rates.

新闻资料 2012-02-14

 
Agilent Technologies to Demonstrate Industry-First R&D and Manufacturing Test Solutions 
Agilent Technologies will demonstrate its industry-first communications test and measurement solutions for LTE-Advanced, LTE, HSPA+, dual-carrier HSDPA, MIMO, multi-standard radio and voice over LTE, along with 2G/3G solutions for R&D, manufacturing and deployment at the Mobile World Congress in Barcelona, Feb. 27- March 1.

新闻资料 2012-02-13

 
Agilent Technologies Introduces Innovative Multi-Measurement Signal Analyzer Capability for Wireless 
Agilent Technologies Inc. (NYSE:A) today announced that an innovative, new multi-measurement capability is being added to its 89600 VSA software, enabling simultaneous signal analysis of multiple carriers and signal formats for more efficient testing and deeper signal insight in wireless test.

新闻资料 2011-11-15

 
Agilent Technologies Introduces Industry's First 3GPP Release 9 Compliant MSR Signal 
Ideal for engineers manufacturing base stations and base-station components, the MSR measurement application enables one-button, standards-based testing per the RF requirements defined in the TR 37 series of the 3GPP Release 9 standard. It is the first and only 3GPP-compliant one-button measurement application on the market today to quickly and easily manufacture MSR base stations and base-station components.

新闻资料 2011-10-19