Show 


E6785A/B/C/D/E/F/G/H/I/J/T/U Fast Switching Lab Application Revision Information

E6785A/B/C/D/E/F/G/H/I/J/T/U Fast Switching Lab Application Revision Information

Last updated: October 30, 2013

This document describes features and functionality that are part of the Agilent Technologies GSM/GPRS_W-CDMA fast switching lab applications. This document contains the original features, as well as enhancements that have been added over time. For a description of the fast switching application (such as license information, etc.), see Fast Switching Description .

   
CAUTION
You may need to upgrade the hardware in your test set before installing the application firmware described here. If you install application firmware on a test set with incompatible hardware, the following may occur:

  • Your test set may lock up.
  • The application may not run.
  • Some features in the application may be inaccessible, or may not perform to specifications.

To determine if a hardware upgrade is required for your testing needs, please review the hardware requirement information at:

http://www.agilent.com/find/8960upgrades


   

Select the appropriate link below to view the required release:

J.00.05 Subscription Release - November 2013

This is a subscription release of the E6785J application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.

You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, CDMA2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this subscription release. Contact your Agilent Sales Representative for more information.

This release has the equivalent features of the following lab applications:

  • E6701K GSM/GPRS Lab Application Revision K.00.05 (E6704A provides a license for enabling EGPRS in the E6701K)
  • E6702G CDMA2000 Lab Application Revision G.00.05
  • E6703J W-CDMA Lab Application Revision J.00.05
  • E6706G 1xEV-DO Lab Application Revision G.00.05

This release of the fast switching lab application requires release A.07.50 or newer of the Wireless Protocol Advisor. This is available at:

http://www.agilent.com/find/wlcontract

Hardware Requirements

This release has specific hardware requirements. Test sets with serial number<MY5210 require a HW upgrade to run this release.

To determine if a hardware upgrade is required for this release, please review the hardware requirement information at:

http://www.agilent.com/find/8960upgrades

_____________________________________________________________________________________________________

I.01.09 Release - May 2013

This release updates the E6785I fast switching lab application. It includes new features and defect fixes. For more information on measurements and features, please refer to the specifications for the equivalent model of the lab application listed below.

This release has the equivalent features of the following lab applications:

  • E6701J GSM/GPRS Lab Application Revision J.01.09 (E6704A provides a license for enabling EGPRS in the E6701J)
  • E6702F CDMA2000 Lab Application Revision F.01.09
  • E6703I W-CDMA Lab Application Revision I.01.09
  • E6706F 1xEV-DO Lab Application Revision F.01.09

You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, CDMA2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this release. Contact your Agilent Sales Representative for more information.

This release of the fast switching lab application requires release A.07.50 or newer of the Wireless Protocol Advisor. This is available at:

http://www.agilent.com/find/wlcontract

Hardware Requirements

This release has specific hardware requirements. Test sets with serial number<MY5210 require a HW upgrade to run this release.

To determine if a hardware upgrade is required for this release, please review the hardware requirement information at:

http://www.agilent.com/find/8960upgrades

_____________________________________________________________________________________________________

I.00.09 Subscription Release - November 2012

This is a subscription release of the E6785I application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.

You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, CDMA2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this subscription release. Contact your Agilent Sales Representative for more information.

This release has the equivalent features of the following lab applications:

  • E6701J GSM/GPRS Lab Application Revision J.00.15 (E6704A provides a license for enabling EGPRS in the E6701J)
  • E6702F CDMA2000 Lab Application Revision F.00.08
  • E6703I W-CDMA Lab Application Revision I.00.08
  • E6706F 1xEV-DO Lab Application Revision F.00.13

This release of the fast switching lab application requires release A.07.50 or newer of the Wireless Protocol Advisor. This is available at:

http://www.agilent.com/find/wlcontract

Hardware Requirements

This release has specific hardware requirements. Test sets with serial number<MY5210 require a HW upgrade to run this release.

To determine if a hardware upgrade is required for this release, please review the hardware requirement information at:

http://www.agilent.com/find/8960upgrades

_____________________________________________________________________________________________________

H.01.15 Release - April 2012

This is a maintenance release. The features offered in this release are identical to those offered in the H.01.13 Release - March 2012

H.01.13 Release - March 2012

This release updates the E6785H fast switching lab application. It includes new features and defect fixes. For more information on measurements and features, please refer to the specifications for the equivalent model of the lab application listed below.

This release has the equivalent features of the following lab applications:

  • E6701I GSM/GPRS Lab Application Revision I.01.12 (E6704A provides a license for enabling EGPRS in the E6701I)
  • E6702E CDMA2000 Lab Application Revision E.01.12
  • E6703H W-CDMA Lab Application Revision H.01.12
  • E6706E 1xEV-DO Lab Application Revision E.01.12

You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, CDMA2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this release. Contact your Agilent Sales Representative for more information.

This release of the fast switching lab application requires release A.07.50 or newer of the Wireless Protocol Advisor. This is available at:

http://www.agilent.com/find/wlcontract

Hardware Requirements

This release has specific hardware requirements. Test sets with serial number<MY5210 require a HW upgrade to run this release.

To determine if a hardware upgrade is required for this release, please review the hardware requirement information at:

http://www.agilent.com/find/8960upgrades

_____________________________________________________________________________________________________

H.00.06 Subscription Release - May 2011

This is a subscription release of the E6785H application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.

You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, CDMA2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this subscription release. Contact your Agilent Sales Representative for more information.

This release has the equivalent features of the following lab applications:

  • E6701I GSM/GPRS Lab Application Revision I.00.05 (E6704A provides a license for enabling EGPRS in the E6701I)
  • E6702E CDMA2000 Lab Application Revision E.00.05
  • E6703H W-CDMA Lab Application Revision H.00.05
  • E6706E 1xEV-DO Lab Application Revision E.00.05

This release of the fast switching lab application requires release A.07.50 or newer of the Wireless Protocol Advisor. This is available at:

http://www.agilent.com/find/wlcontract

Hardware Requirement

http://www.agilent.com/find/8960upgrades

_____________________________________________________________________________________________________

G.01.13 Release - December 2010

This release updates the E6785G fast switching lab application. It includes new features and defect fixes. For more information on measurements and features, please refer to the specifications for the equivalent model of the lab application listed below.

This release has the equivalent features of the following lab applications:

  • E6701H GSM/GPRS Lab Application Revision H.01.12 (E6704A provides a license for enabling EGPRS in the E6701G)
  • E6702D CDMA2000 Lab Application Revision D.01.12
  • E6703G W-CDMA Lab Application Revision G.01.10
  • E6706D 1xEV-DO Lab Application Revision D.01.10

You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, CDMA2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this subscription release. Contact your Agilent Sales Representative for more information.

This release of the fast switching lab application requires release A.07.50 or newer of the Wireless Protocol Advisor. This is available at:

http://www.agilent.com/find/wlcontract

Hardware Requirement

http://www.agilent.com/find/8960upgrades

_____________________________________________________________________________________________________

G.00.15 Subscription Release - June 2010

This is a subscription release of the E6785G application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.

You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, CDMA2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this subscription release. Contact your Agilent Sales Representative for more information.

This release has the equivalent features of the following lab applications:

  • E6701H GSM/GPRS Lab Application Revision H.00.15 (E6704A provides a license for enabling EGPRS in the E6701G)
  • E6702D CDMA2000 Lab Application Revision D.00.14
  • E6703G W-CDMA Lab Application Revision G.00.14
  • E6706D 1xEV-DO Lab Application Revision D.00.14

This release of the fast switching lab application requires release A.07.50 or newer of the Wireless Protocol Advisor. This is available at:

http://www.agilent.com/find/wlcontract

Hardware Requirement

http://www.agilent.com/find/8960upgrades

_____________________________________________________________________________________________________

G.00.09 Subscription Release - January 2010

This is a subscription release of the E6785G application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.

You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, CDMA2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this subscription release. Contact your Agilent Sales Representative for more information.

This release has the equivalent features of the following lab applications:

  • E6701H GSM/GPRS Lab Application Revision H.00.09 (E6704A provides a license for enabling EGPRS in the E6701G)
  • E6702D CDMA2000 Lab Application Revision D.00.08
  • E6703G W-CDMA Lab Application Revision G.00.08
  • E6706D 1xEV-DO Lab Application Revision D.00.08

This release of the fast switching lab application requires release A.07.50 or newer of the Wireless Protocol Advisor. This is available at:

http://www.agilent.com/find/wlcontract

Hardware Requirement

http://www.agilent.com/find/8960upgrades

_____________________________________________________________________________________________________

F.01.12 Release - September 2009

This release updates the E6785F fast switching lab application. It includes new features and defect fixes. For more information on measurements and features, please refer to the specifications for the equivalent model of the lab application listed below.

This release has the equivalent features of the following lab applications:

  • E6701G GSM/GPRS Lab Application Revision G.01.12 (E6704A provides a license for enabling EGPRS in the E6701G)
  • E6702C CDMA2000 Lab Application Revision C.01.12
  • E6703F W-CDMA Lab Application Revision F.01.12
  • E6706C 1xEV-DO Lab Application Revision C.01.12

You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, CDMA2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this subscription release. Contact your Agilent Sales Representative for more information.

This release of the fast switching lab application requires release A.07.50 or newer of the Wireless Protocol Advisor. This is available at:

http://www.agilent.com/find/wlcontract

Hardware Requirement

http://www.agilent.com/find/8960upgrades

_____________________________________________________________________________________________________

F.00.21 Subscription Release - May 2009

This is a subscription release of the E6785F application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.

You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, CDMA2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this subscription release. Contact your Agilent Sales Representative for more information.

This release has the equivalent features of the following lab applications:

  • E6701G GSM/GPRS Lab Application Revision G.00.18 (E6704A provides a license for enabling EGPRS in the E6701G)
  • E6702C CDMA2000 Lab Application Revision C.00.18
  • E6703F W-CDMA Lab Application Revision F.00.19
  • E6706C 1xEV-DO Lab Application Revision C.00.17

This release of the fast switching lab application requires release A.07.50 or newer of the Wireless Protocol Advisor. This is available at:

http://www.agilent.com/find/wlcontract

Hardware Requirement

http://www.agilent.com/find/8960upgrades

_____________________________________________________________________________________________________

F.00.07 Subscription Release - December 2008

This is a subscription release of the E6785F application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.

You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, CDMA2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this subscription release. Contact your Agilent Sales Representative for more information.

This release has the equivalent features of the following lab applications:

  • E6701G GSM/GPRS Lab Application Revision G.00.07 (E6704A provides a license for enabling EGPRS in the E6701G)
  • E6702C CDMA2000 Lab Application Revision C.00.07
  • E6703F W-CDMA Lab Application Revision F.00.07
  • E6706C 1xEV-DO Lab Application Revision C.00.07

This release of the fast switching lab application requires release A.07.50 or newer of the Wireless Protocol Advisor. This is available at:

http://www.agilent.com/find/wlcontract

Hardware Requirement

http://www.agilent.com/find/8960upgrades

_____________________________________________________________________________________________________

U.01.04 Special Release (E6785U) - October 2008

This is a subscription release of the E6785U application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.

You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, cdma2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this subscription release. Contact your Agilent Sales Representative for more information.

The E6785U can only be loaded onto an E5515C with Special High Data Rate Hardware (or a test set with the equivalent hardware upgrades). Loading the E6785U onto an E5515B or E5515C without the appropriate hardware upgrades will cause the test set to lock up.

Note, the Special High Data Rate Hardware required to support the E6785U meets the E6785D measurement parametric specifications in a temperature range of 25 +/- 5 ° C, and has an operating temperature range of 0 to 35 ° C.

This release has the equivalent features of the following lab applications:

  • E6701U GSM/GPRS Lab Application Revision U.01.04 (E6704A provides a license for enabling EGPRS in the E6701T)
  • E6702T CDMA2000 Lab Application Revision T.04.04
  • E6703U W-CDMA Lab Application Revision U.01.04
  • E6706U 1xEV-DO Lab Application Revision U.01.04

_____________________________________________________________________________________________________

E.01.17 Release (E6785E) - October 2008

This is a maintenance release to resolve the known issues detailed in the previous release. The features offered in this release are otherwise identical to those offered in the E.01.14 Release - September 2008 , with the following exception:

  • The value for RLC SDU window size has been increased when on a 5.7Mbps HSUPA IP data to increase IP data throughput for some devices (from 1024 to UE reported max AM RLC Window size).

This release is available for download at the Lab Application Annual Contract site: www.agilent.com/find/wlcontract.

This release has the equivalent features of the following lab applications:

  • E6701F GSM/GPRS Lab Application Revision F.01.15
  • E6702B CDMA2000 Lab Application Revision B.07.14
  • E6703U W-CDMA Lab Application Revision E.01.16
  • E6706B 1xEV-DO Lab Application Revision B.01.13

_____________________________________________________________________________________________________

E.01.14 Release - September 2008

This release updates the E6785E fast switching lab application. It includes new features and defect fixes. For more information on measurements and features, please refer to the specifications for the equivalent model of the lab application listed below.

This release has the equivalent features of the following lab applications:

  • E6701F GSM/GPRS Lab Application Revision F.01 (E6704A provides a license for enabling EGPRS in the E6701E)
  • E6702B CDMA2000 Lab Application Revision B.07
  • E6703E W-CDMA Lab Application Revision E.01
  • E6706B 1xEV-DO Lab Application Revision B.01

Known Issues

  • A protocol processor timeout occurs during repeated packet switched data handover procedures between two test sets in E6701F.
  • The real time vocoder's Voice Activity Detection State parameter (CALL:RTVocoder:VADetection[:STATe) is not functioning in E6701F. It remains in the OFF state.
  • Results are erroneously high for USF BLER (Unassigned) when three or more uplinks are in use in E6701F (that is, when using extended dynamic allocation).
  • Cannot camp to band IX in E6703E.
  • An assert occurs when attempting a PCR handoff between bands (for example, 1 to 2, 2 to 5, 5 to 1) with a PDP context established using "Reported CQI" during an FTP in E6703E.
  • Using save/recall causes HSUPA 2ms settings to un-synchronize between host and protocol in E6703E.
  • Web pages are sometimes not properly displayed on the mobile when Web browsing with E6701F and E6703E.
  • The SYSTem:APPLication:CATalog:LICense:APPLication:ALL? command does not function in E6701F and E6703E.

http://www.agilent.com/find/8960upgrades

_____________________________________________________________________________________________________

Hardware Requirement

http://www.agilent.com/find/8960upgrades

U.00.39 Special Release - May 2008

This is a maintenance release to resolve known issues. The features offered in this release are identical to those offered in the U.00.37 Special Release - May 2008 Release.

This release has the equivalent features of the following lab applications:

  • E6701U GSM/GPRS Lab Application Revision U.00.34 (E6704A provides a license for enabling EGPRS in the E6701U)
  • E6702T CDMA2000 Lab Application Revision T.03.08
  • E6703U W-CDMA Lab Application Revision U.00.33
  • E6706U 1xEV-DO Lab Application Revision U.00.46

Hardware Requirements

http://www.agilent.com/find/8960upgrades

_____________________________________________________________________________________________________

E.00.41 Subscription Release - May 2008

This is a maintenance release to resolve known issues. The features offered in this release are identical to those offered in the E.00.39 Subscription Release - May 2008 Release.

This release has the equivalent features of the following lab applications:

  • E6701F GSM/GPRS Lab Application Revision F.00.39 (E6704A provides a license for enabling EGPRS in the E6701T)
  • E6702B CDMA2000 Lab Application Revision B.06.08
  • E6703E W-CDMA Lab Application Revision E.00.36
  • E6706B 1xEV-DO Lab Application Revision B.00.46

Hardware Requirements

http://www.agilent.com/find/8960upgrades

_____________________________________________________________________________________________________

U.00.37 Special Release - May 2008

This is a subscription release of the E6785U application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.

You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, cdma2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this subscription release. Contact your Agilent Sales Representative for more information.

The E6785U can only be loaded onto an E5515C with Special High Data Rate Hardware (or a test set with the equivalent hardware upgrades). Loading the E6785U onto an E5515B or E5515C without the appropriate hardware upgrades will cause the test set to lock up.

Note, the Special High Data Rate Hardware required to support the E6785U meets the E6785D measurement parametric specifications in a temperature range of 25 +/- 5 ° C, and has an operating temperature range of 0 to 35 ° C.

This release has the equivalent features of the following lab applications:

  • E6701U GSM/GPRS Lab Application Revision U.00.32 (E6704A provides a license for enabling EGPRS in the E6701U)
  • E6702T CDMA2000 Lab Application Revision T.03.08
  • E6703U W-CDMA Lab Application Revision U.00.31
  • E6706U 1xEV-DO Lab Application Revision U.00.44

This release of the fast switching lab application requires release A.07.50 or newer of the Wireless Protocol Advisor. This is available at:

http://www.agilent.com/find/wlcontract

Hardware Requirements

http://www.agilent.com/find/8960upgrades

E.00.39 Subscription Release - May 2008

This is a subscription release of the E6785E application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.

You must have current GSM/GPRS/EGPRS, W-CDMA/HSPA, cdma2000/IS-95/AMPS and 1xEV-DO Lab Application Annual Contracts to obtain this subscription release. Contact your Agilent Sales Representative for more information.

This release has the equivalent features of the following lab applications:

  • E6701F GSM/GPRS Lab Application Revision F.00.37 (E6704A provides a license for enabling EGPRS in the E6701F)
  • E6702B CDMA2000 Lab Application Revision B.06.08
  • E6703E W-CDMA Lab Application Revision E.00.34
  • E6706B 1xEV-DO Lab Application Revision B.00.44

This release of the fast switching lab application requires release A.07.50 or newer of the Wireless Protocol Advisor. This is available at:

http://www.agilent.com/find/wlcontract

Hardware Requirement

http://www.agilent.com/find/8960upgrades

U.00.23 Special Release - November 2007

This is a subscription release of the E6785U application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.

You must have current GSM/GPRS/EGPRS and W-CDMA/HSPA Lab Application Annual Contracts to obtain this subscription release. Contact your Agilent Sales Representative for more information.

The E6785U can only be loaded onto an E5515C with Special High Data Rate Hardware (or a test set with the equivalent hardware upgrades). Loading the E6785U onto an E5515B or E5515C without the appropriate hardware upgrades will cause the test set to lock up.

Note, the Special High Data Rate Hardware required to support the E6785U meets the E6785D measurement parametric specifications in a temperature range of 25 +/- 5 ° C, and has an operating temperature range of 0 to 35 ° C.

This release has the equivalent features of the following lab applications:

  • E6701U GSM/GPRS Lab Application Revision U.00.22 (E6704A provides a license for enabling EGPRS in the E6701U)
  • E6703U W-CDMA Lab Application Revision U.00.20

Hardware Requirements

http://www.agilent.com/find/8960upgrades

E.00.25 Subscription Release - November 2007

This is a subscription release of the E6785E application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.

You must have current GSM/GPRS/EGPRS and W-CDMA/HSPA Lab Application Annual Contracts to obtain this subscription release. Contact your Agilent Sales Representative for more information.

This release has the equivalent features of the following lab applications:

  • E6701F GSM/GPRS Lab Application Revision F.00.27 (E6704A provides a license for enabling EGPRS in the E6701E)
  • E6703E W-CDMA Lab Application Revision E.00.23

Hardware Requirements

http://www.agilent.com/find/8960upgrades

T.03.08 Special Release - July 2007

The E6785T can only be loaded onto an E5515C with Special High Data Rate Hardware (or a test set with the equivalent hardware upgrades). Loading the E6785T onto an E5515B or E5515C without the appropriate hardware upgrades will cause the test set to lock up.

Note, the Special High Data Rate Hardware required to support the E6785T meets the E6785D measurement parametric specifications in a temperature range of 25 +/- 5 ° C, and has an operating temperature range of 0 to 35 ° C.

This release has the equivalent features of the following lab applications:

  • E6701T GSM/GPRS Lab Application Revision T.03 (E6704A provides a license for enabling EGPRS in the E6701T)
  • E6703T W-CDMA Lab Application Revision T.03

Hardware Requirements

http://www.agilent.com/find/8960upgrades

D.02.08 Release - July 2007

This release updates the E6785D GSM/GPRS_W-CDMA fast switching lab application. It includes new features and defect fixes. For more information on measurements and features, please refer to the specifications for the equivalent model of the lab application listed below. This release has the equivalent features of the following lab applications:

  • E6701E GSM/GPRS Lab Application Revision E.02 (E6704A provides a license for enabling EGPRS in the E6701E)
  • E6703D W-CDMA Lab Application Revision D.02

Hardware Requirements

http://www.agilent.com/find/8960upgrades

E.00.16 Subscription Release - May 2007

This is a subscription release of the E6785E application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.

You must have current GSM/GPRS/EGPRS and W-CDMA/HSDPA Lab Application Annual Contracts to obtain this subscription release. Contact your Agilent Sales Representative for more information.

This is a maintenance release to resolve known issues. The features offered in this release are identical to those offered in the E.00.13 Subscription Release - April 2007 Release.

_____________________________________________________________________________________________________

U.00.13 Special Release - April 2007

This is a subscription release of the E6785U application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.

You must have current GSM/GPRS/EGPRS and W-CDMA/HSDPA Lab Application Annual Contracts to obtain this subscription release. Contact your Agilent Sales Representative for more information.

The E6785U can only be loaded onto an E5515C with Special High Data Rate Hardware (or a test set with the equivalent hardware upgrades). Loading the E6785U onto an E5515B or E5515C without the appropriate hardware upgrades will cause the test set to lock up.

Note, the Special High Data Rate Hardware required to support the E6785U meets the E6785D measurement parametric specifications in a temperature range of 25 +/- 5 ° C, and has an operating temperature range of 0 to 35 ° C.

This release has the equivalent features of the following lab applications:

  • E6701U GSM/GPRS Lab Application Revision U.00.13 (E6704A provides a license for enabling EGPRS in the E6701T)
  • E6703U W-CDMA Lab Application Revision U.00.12

Hardware Requirements

http://www.agilent.com/find/8960upgrades

E.00.13 Subscription Release - April 2007

This is a subscription release of the E6785E application. In order to provide early access to new features, this subscription release has been partially qualified. The new features present in this release have been bench-tested to verify their performance. The previously existing features in this release have undergone a shortened software qualification cycle to verify that they have not been negatively affected by the new features.

You must have current GSM/GPRS/EGPRS and W-CDMA/HSDPA Lab Application Annual Contracts to obtain this subscription release. Contact your Agilent Sales Representative for more information.

This release has the equivalent features of the following labapplications:

  • E6701F GSM/GPRS Lab Application Revision F.00.13 (E6704A provides a license for enabling EGPRS in the E6701E)
  • E6703E W-CDMA Lab Application Revision E.00.12

Hardware Requirements

http://www.agilent.com/find/8960upgrades

T.01.19 Special Release - March 2007

The E6785T can only be loaded onto an E5515C with Special High Data Rate Hardware (or a test set with the equivalent hardware upgrades). Loading the E6785T onto an E5515B or E5515C without the appropriate hardware upgrades will cause the test set to lock up.

Note, the Special High Data Rate Hardware required to support the E6785T meets the E6785D measurement parametric specifications in a temperature range of 25 +/- 5 ° C, and has an operating temperature range of 0 to 35 ° C.

This is a maintenance release to resolve known issues. The features offered in this release are identical to those offered in the T.01.12 Special Release - December 2006 .

Hardware Requirements

http://www.agilent.com/find/8960upgrades

Resolved Known Issues

  • GSM/GPRS Tx Power Measurement problem

D.01.20 Release - March 2007

This is a maintenance release to resolve known issues. The features offered in this release are identical to those offered in the D.01.13 Release - December 2006 .

Hardware Requirements

http://www.agilent.com/find/8960upgrades

Resolved Known Issues

  • GSM/GPRS Tx Power Measurement problem

T.01.12 Special Release - December 2006

The E6785T can only be loaded onto an E5515C with Special High Data Rate Hardware (or a test set with the equivalent hardware upgrades). Loading the E6785T onto an E5515B or E5515C without the appropriate hardware upgrades will cause the test set to lock up.

Note, the Special High Data Rate Hardware required to support the E6785T meets the E6785D measurement parametric specifications in a temperature range of 25 +/- 5 ° C, and has an operating temperature range of 0 to 35 ° C.

This release has the equivalent features of the following lab applications:

  • E6701T GSM/GPRS Lab Application Revision T.01 (E6704A provides a license for enabling EGPRS in the E6701T)
  • E6703T W-CDMA Lab Application Revision T.01

Hardware Requirements

http://www.agilent.com/find/8960upgrades

D.01.13 Release - December 2006

This release updates the E6785D GSM/GPRS_W-CDMA fast switching lab application. It includes new features and defect fixes. For more information on measurements and features, please refer to the specifications for the equivalent model of the lab application listed below. This release has the equivalent features of the following lab applications:

  • E6701E GSM/GPRS Lab Application Revision E.01 (E6704A provides a license for enabling EGPRS in the E6701E)
  • E6703D W-CDMA Lab Application Revision D.01

Hardware Requirements

http://www.agilent.com/find/8960upgrades

T.00.03 Special Release - August 2006

The E6785T can only be loaded onto an E5515C with Special High Data Rate Hardware (or a test set with the equivalent hardware upgrades). Loading the E6785T onto an E5515B or E5515C without the appropriate hardware upgrades will cause the test set to lock up.

Note, the Special High Data Rate Hardware required to support the E6785T meets the E6785D measurement parametric specifications in a temperature range of 25 +/- 5 ° C, and has an operating temperature range of 0 to 35 ° C.

This release has the equivalent features of the following lab applications:

  • E6701T GSM/GPRS Lab Application Revision T.00.08 (E6704A provides a license for enabling EGPRS in the E6701T)
  • E6703T W-CDMA Lab Application Revision T.00.08

D.00.03 Pre-Release (E6785D)- August 2006

This is a pre-release of the E6785D application. In order to provide early access to new features, this pre-release has not been fully qualified.

You must have current E6720A Option 001 and 003 Lab Application Annual Upgrade Contracts to obtain this pre-release. Contact your Agilent Sales Representative for more information.This release has the equivalent features of the following lab applications:

  • E6701E GSM/GPRS Lab Application Revision E.00.12 (E6704A provides a license for enabling EGPRS in the E6701E)
  • E6703D W-CDMA Lab Application Revision D.00.08

C.04.06 Release - July 2006

This release updates the E6785C GSM/GPRS_W-CDMA fast switching lab application. It includes new features and defect fixes. For more information on measurements and features, please refer to the specifications for the equivalent model of the lab application listed below. This release has the equivalent features of the following lab applications:

  • E6701D GSM/GPRS Lab Application Revision D.03.40 (E6704A provides a license for enabling EGPRS in the E6701D)
  • E6703C W-CDMA Lab Application Revision C.04

C.03.12 Release - December 2005

This release updates the E6785C GSM/GPRS_W-CDMA fast switching lab application. It includes new features and defect fixes. For more information on measurements and features, please refer to the specifications for the equivalent model of the lab application listed below. This release has the equivalent features of the following lab applications:

  • E6701D GSM/GPRS Lab Application Revision D.03.32 (E6704A provides a license for enabling EGPRS in the E6701D)
  • E6703C W-CDMA Lab Application Revision C.03.11

C.02.25 Release - May 2005

This release introduces the E6785C GSM/GPRS_W-CDMA fast switching lab application with the equivalent features of the following lab applications and application revisions:

  • E6701D GSM/GPRS Lab Application Revision D.02.10 (E6704A provides a license for enabling EGPRS in the E6701D)
  • E6703C W-CDMA Lab Application Revision C.02.25

For more information on measurements, specifications, and E5515 mainframe requirements, please refer to the specifications for the equivalent model of the lab application listed above.

C.01.18 Release - January 2005

This release introduces the E6785C GSM/GPRS_W-CDMA fast switching lab application with the equivalent features of the following lab applications and application revisions:

  • E6701D GSM/GPRS Lab Application Revision D.01.18 (E6704A provides a license for enabling EGPRS in the E6701D)
  • E6703C W-CDMA Lab Application Revision C.01.17

For more information on measurements, specifications, and E5515 mainframe requirements, please refer to the specifications for the equivalent model of the lab application listed above.

B.02.14 Release - January 2005

This release introduces the E6785C GSM/GPRS_W-CDMA fast switching lab application with the equivalent features of the following lab applications and application revisions:

  • E6701D GSM/GPRS Lab Application Revision C.04.14 (E6704A provides a license for enabling EGPRS in the E6701D)
  • E6703C W-CDMA Lab Application Revision B.02.14

For more information on measurements, specifications, and E5515 mainframe requirements, please refer to the specifications for the equivalent model of the lab application listed above.

B.01.33 Release - July 2004

This release updates the E6785B GSM/GPRS_W-CDMA fast switching lab application with the equivalent features of the following lab applications and application revisions:

  • E6701C GSM/GPRS Lab Application Revision C.03.54 (E6704A provides a license for enabling EGPRS in the E6701C)
  • E6703B W-CDMA Lab Application Revision B.01.34

For more information on measurements, specifications, and E5515 mainframe requirements, please refer to the specifications for the equivalent model of the lab application listed above.

B.01.28 Release - April 2004

This release updates the E6785B GSM/GPRS_W-CDMA fast switching lab application with the equivalent features of the following lab applications and application revisions:

  • E6701C GSM/GPRS Lab Application Revision C.03.48 (E6704A provides a license for enabling EGPRS in the E6701C)
  • E6703B W-CDMA Lab Application Revision B.01.29

For more information on measurements, specifications, and E5515 mainframe requirements, please refer to the specifications for the equivalent model of the lab application listed above.

B.01.16 Release - January 2004

This release updates the E6785B GSM/GPRS_W-CDMA fast switching lab application with the equivalent features of the following lab applications and application revisions:

  • E6701C GSM/GPRS Lab Application Revision C.03.32 (E6704A provides a license for enabling EGPRS in the E6701C)
  • E6703B W-CDMA Lab Application Revision B.01.16

For more information on measurements, specifications, and E5515 mainframe requirements, please refer to the specifications for the equivalent model of the lab application listed above.

A.02.10 Release - July 2003

This release updates the E6785A GSM/GPRS_W-CDMA fast switching lab application with the equivalent features of the following lab applications and application revisions:

  • E6701C GSM/GPRS Lab Application Revision C.02.10 (E6704A provides a license for enabling EGPRS in the E6701C)
  • E6703A W-CDMA Lab Application Revision A.02.10

For more information on measurements, specifications, and E5515 mainframe requirements, please refer to the specifications for the equivalent model of the lab application listed above.

A.01.25 Release - March 2003

This is the initial release of the E6785A GSM/GPRS_W-CDMA fast switching lab application. This release has the equivalent features of the following lab applications and application revisions:

  • E6701C GSM/GPRS Lab Application Revision C.01.24 (E6704A provides a license for enabling EGPRS in the E6701C)
  • E6703A W-CDMA Lab Application Revision A.01.23

For more information on measurements, specifications, and E5515 mainframe requirements, please refer to the specifications for the equivalent model of the lab application listed above.

A.01.20 Release - February 2003

This is the initial release of the E6785A GSM/GPRS_W-CDMA fast switching lab application. This release has the equivalent features of the following lab applications and application revisions:

  • E6701C GSM/GPRS Lab Application Revision C.01.20 (E6704A provides a license for enabling EGPRS in the E6701C)
  • E6703A W-CDMA Lab Application Revision A.01.20

For more information on measurements, specifications, and E5515 mainframe requirements, please refer to the specifications for the equivalent model of the lab application listed above.