무엇을 찾고 있습니까?

November 22 – 24, 2022
New Zealand, Australia, Southeast Asia
The largest annual technical conference to discover the latest technical challenges & solutions
3 Tracks. 3 Days.
At our virtual event, Keysight World Technical Week consists of 5G/6G, High Speed Digital, and Automotive tracks to provide the latest insight for engineers. Join us each day to hear from Keysight’s technology experts.

5G/6G
5G technology continues to evolve along with standard updates and contributes to wireless and other vertical industries. The 5G/6G track consists of two different sub-tracks for Device and Network/Infrastructure, and the industry’s hot topics, trends, and solution discussions are included to ensure your success in 5G and beyond.

High Speed Digital
The strong consumer demand for faster internet speed is pushing the high speed digital interface technology to evolve at a faster rate than ever. Design and development engineers are now facing challenges that are far more complex than before. We will discuss these changes, challenges, and how you may tackle them.

Automotive
We will cover the technical essentials for EV development such as EV charging, battery, grid evaluation, and power electronics device tests like GaN/SiC. In addition, the program includes a wide range of AV core technologies such as C-V2X communication, high-speed in-vehicle network, cyber security, and ADAS/sensor testing to realize autonomous driving/connected cars into the market.
Agenda
Nov. 22: 5G/6G
Device | Network/Infrastructure | |
---|---|---|
10:00 | 6G: Technology Revolutions Needed Roger Nichols, Keysight |
|
11:00 |
Accelerating Innovations in 5G Non-Terrestrial Networks Raymond Shen, PhD, Keysight |
|
13:30 | Addressing the 5G Device Test Challenges Posed by Release 16 and 17 Manuel Blanco, Keysight |
O-RAN Radio Unit Conformance Testing Parisa Akhshi, Keysight |
14:30 | 5G RF/RRM Conformance and Regulatory Test Ashley Chan, Keysight |
Distributed Cloud Testing and Visibility Bharath Sathyanarayan, Keysight Kelvin Heng, Keysight |
15:30 | Understanding Regulatory Testing for Wi-Fi 6E Devices Bill Koerner, Keysight |
5G Field Test Automation and Analytics Jun-Yian Lean, Keysight |
Nov. 23: High Speed Digital
Interface | Fundamental | |
---|---|---|
10:00 | Data Center Technologies That Are Shaping the Future of Communication Joachim Peerlings, Keysight Masahito Tomizawa, Nippon Telegraph and Telephone Corporation Gerald Pasdast, Intel Corporation Vladimir Kozlov, Lightcounting |
|
11:30 |
Signal Integrity Simulation Flow for High Speed Interconnects Li Wern Chew, Intel Microelectronics (M) Sdn. Bhd. |
|
13:30 | DDR5/LPDDR5 - Challenges on Memory Device/System Validation & Solutions Kar Hooi Kuan, Keysight |
Ready for PAM4? - The Basic of PAM4 Brian Yeo, Keysight |
14:30 | Solid PCIe® Protocol Test Strategy Enables Datacenter Transformation David Woolf, Keysight |
Debugging Techniques with Infiniium Oscilloscopes Wai Cheong Ng, Keysight |
15:30 | Testing USB4® and Beyond Jit Lim, Keysight |
- PCI-SIG®, PCIe® and PCI Express® are US registered trademarks and/or service marks of PCI-SIG.
- USB Type-C®, USB-C®, and USB4® are trademarks of USB Implementers Forum.
Nov. 24: Automotive
EV/ Power Electronics/Cyber Security | Autonomous Drive/Connected Car | |
---|---|---|
10:00 | UL Vehicle to Grid Standards Development Timothy Zgonena, Underwriters Laboratories |
Experiments Helps the Design of Vehicular Wireless Communication Technology Tai Huang, National Innovation Center of Intelligent and Connected Vehicle |
11:00 |
Grid-Edge Frontier – Implications and Opportunities for the e-mobility Industry Panel discussion : Andrew Cifala / Jens Schmutzler / Wolfgang Kalthoff, Keysight Moderator : Kevin Cavel, Keysight |
Comparing C-V2X Day 1 and Day 2 Use Case Application KPI‘s in SiL vs HiL Bill McKinley, Keysight |
13:30 | EV Battery Test: Improve Design and Operation of Your Lab Stefan Dreifke, Keysight |
Emerging Needs of High Speed and Signal Integrity in In-Vehicle Networks Junichiro Azami, Sony Semiconductor Solutions Corporation |
14:30 | Dynamic Characterization of WBG Power Modules, Device Modeling, and Circuit Simulation Takamasa Arai, Keysight |
Keysight High Speed Test Solutions for Automotive SerDes In-Vehicle Network Carrie Browen, Keysight Demo : Kevin Kershner / Jae Yong Chang, Keysight |
15:30 | Keysight Automotive Cybersecurity Tools to Stay Compliant With UNECE WP.29 UN-R 155 and ISO/SAE 21434 Seung-Taek Chang, Keysight |
From the Road to the Lab: Validation of ADAS / AD Functions With Real Sensors Silviu-Sorin Tuca, Keysight |
Guest Speakers
Want help or have questions?