Choose a country or area to see content specific to your location
무엇을 찾고 있습니까?
Salute to Smart Bench Essentials Challenge Winners

A Retrospective of the SBE Challenge
The Smart Bench Essentials (SBE) Challenge celebrates innovators from around the world by showcasing their inventions and workbench. The creativity, passion, persistence, and altruistic spirit demonstrated by the entrants impressed the SBE judges. Indeed, you are the rays of hope for the future of the world — be it an advancement in solving the coronavirus pandemic, saving energy, reducing carbon emissions, robotic systems to improve the quality of life, exploring space science, and much more.
Keysight dedicates this web page to all SBE Challenge innovators to showcase some of the entries from the top five fields of interests, as well as testimonials and photos from the six winners.
- Consumer Electronics / IoT
- Automotive and Energy
- Aerospace and Defense
- IC / Semiconductor and Manufacturing
- Education
Consumer Electronics / IoT
Consumer electronics and the Internet of Things (IoT) are products of interest that are very close to our everyday activities. This technology represents the largest field of interest based on the number of entrants in the SBE Challenge. Many innovative and life-enhancing engineering ideas emerged from the entries, such as:
Automotive and Energy
Automotive, energy, and communication technologies have come together to enable the electrification of transport vehicles with features that reduce the driver's cognitive burden, improve connectivity, and increase safety. Judging by the number of SBE Challenge entrants in this area, there are an increasing number of innovators in this fast-growing industry, such as the following:
Aerospace and Defense
In recent years, space science and exploration have become more accessible to commercial and small-scale developers as many countries and private companies are investing in the aerospace and defense industry. Here are some of the entrants who are either working in the aerospace and defense industry or contributing to space science and exploration:
IC/Semiconductor and Manufacturing
IC / semiconductor and manufacturing is the foundation of many industries. Integrated circuit (IC) technologies rapidly advance and will continue to do so in the coming years. Many of the SBE Challenge entrants play important roles in this area, such as the following:
Education
The Smart Bench Essentials instruments garnered much interest from university educators and students alike. The Keysight PathWave BenchVue software included with SBE instruments and the optional PathWave Remote Lab Access software enable multiuser access so students, educators, and lab administrators can access the lab to test, analyze, and share collaboratively — anytime and anywhere.
Here are some entries with a touch of passion, altruistic spirit, and humor for learning and teaching:
SBE Challenge Winners
Congratulations to the six winners of the SBE Challenge. Here are their winning stories:
Smart Software for a Smart Bench
With PathWave BenchVue software applications, you can configure your test instruments quickly and operate all of them together on the same PC. BenchVue stores all your data on your PC and exports data in standard formats for analysis and reporting.

Explore Keysight Smart Bench Essentials Family

EDU33212A Waveform Function Generator
Up to 20 MHz Frequency Range
Dual-channel function generators offer six built-in modulation types, 17 popular waveforms to simulate typical applications for testing, and 16-bit arbitrary waveform capability
구성/견적
구성 옵션
이메일 취소
EDU36311A Triple-Output DC Power Supply
2 Channels of 30V / 1A and 1 Channel of 6V / 5A
With three electrically isolated channels with a total of 90 W clean and reliable power, this power supply includes over-voltage protection, over-current protection, and over-temperature protection to prevent damage
구성/견적
구성 옵션
이메일 취소
EDU34450A Digital Multimeter
5.5-Digits Resolution
A dual display 5.5-digit digital multimeter with up to 110 readings/s for speed-critical tests, plus generous internal memory for logging up to 5,000 data points
구성/견적
구성 옵션
이메일 취소
EDUX1052G InfiniiVision Oscilloscope
50 MHz Bandwidth
Proven InfiniiVision technology that gives you professional-level measurements you can trust. It comes with a built-in 20-MHz function generator
구성/견적
구성 옵션
이메일 취소Explore Keysight Smart Bench Essentials Family
Want help or have questions?