Choose a country or area to see content specific to your location
백서
As 5G New Radio (NR) moves from the definition and specification phase into development, enabling technologies such as multiple input, multiple output (MIMO), and beamforming are critical. Engineers will use active phased array antennas to implement MIMO and beamforming in base stations and devices. In fact, these active antennas are critical to overcome signal propagation issues, such as higher path loss at millimeter wave frequencies. They also provide the ability to dynamically shape and steer beams to specific users. Active antennas offer more flexibility and improve the performance of 5G communications, especially at millimeter-wave (mmWave) frequencies.
콘텐츠 잠금 해제
무료 가입
*Indicates required field
감사합니다!
귀하의 양식이 성공적으로 제출되었습니다.
Note: Clearing your browser cache will reset your access. To regain access to the content, simply sign up again.
×
판매 문의 부탁드립니다.
*Indicates required field
감사합니다!
A sales representative will contact you soon.