Choose a country or area to see content specific to your location
백서
The 3rd Generation Partnership Project (3GPP) published its very first 5G specification in December 2017. It includes non-standalone (NSA) mode using the LTE core and radio networks, while preparing a full-scale rollout of NR stand-alone deployments. The main scenario for NSA mode is the widely considered LTE-NR Dual Connectivity (DC), in which user data can be exchanged between a mobile device and a NR base station along with LTE connectivity.
The first 5G standard non-standalone deployment configuration offers throughput and latency advantages that can be achieved with the existing 4G network coverage. However, it requires more complex hardware implementations to allow simultaneous connections with both LTE and NR networks, which will increase costs, especially for user equipment (UE).
콘텐츠 잠금 해제
무료 가입
*Indicates required field
감사합니다!
귀하의 양식이 성공적으로 제출되었습니다.
Note: Clearing your browser cache will reset your access. To regain access to the content, simply sign up again.
×
판매 문의 부탁드립니다.
*Indicates required field
감사합니다!
A sales representative will contact you soon.