Column Control DTX

3–Electrode Electrochemical Measurement Techniques

애플리케이션 노트

The Keysight B2900A Precision Source/Measure Unit (SMU) is used for electrochemical measurements including two widely applied workflows known as cyclic voltammetry (C-V) and chrono-amperometry. Both measurements are based on three-electrode systems including working electrode, reference electrode, and counter electrode. In C-V the potential is scanned and the corresponding current of the electrochemical redox reaction is measured. The voltages and the current of the oxidation and reduction peaks are measured with the values depending on the analyte concentration (Nernst equation) and the kinetic diffusion properties (Fick’s law). In chrono-amperometry the current of the redox reaction is measured with respect to time at a given constant potential. Two different electrochemical systems are measured including a Li-ion cell with TiO2 as the reference electrode and a glucose sensor with a polymer modified electrode. In comparison to the conventional potentiostat-based setup the SMU has very sensitive current and voltage measurement resolution allowing for instance also small electrode systems with low electrochemical currents to be accurately measured. The process control can be done either from the front panel of the SMU or by the PC-based Keysight B2900A Quick I/V Measurement Software.

×

판매 문의 부탁드립니다.

*Indicates required field

선호하는 연락방법을 선택해 주십시오. *필수입력항목
Preferred method of communication? 이메일 변경하기
Preferred method of communication?

[키사이트 개인정보 수집 및 이용]
 1. 개인정보 수집 및 이용 동의
 2. 키사이트 파트너 업무 위탁 동의
 3. 키사이트 해외 본사 및 지사 제공 동의

"제출"을 클릭하시면 개인정보 수집 및 이용에 동의한 것으로 간주합니다. 보다 자세한 내용은 홈페이지 하단의 개인정보보호정책 을 참조하시기 바랍니다.

감사합니다!

A sales representative will contact you soon.

Column Control DTX