Choose a country or area to see content specific to your location
애플리케이션 노트
A significant and understandable concern with new test system setup is becoming familiar with and programming the instruments. Learning the steps needed to control an instrument can be time consuming if not difficult. Many hours can be spent reading through syntax manuals and performing trial and error tests. When a test system is updated only occasionally, it may be hard to remember the instrument commands and steps required to make changes.
This document includes examples with the few steps needed to make measurements using the 34980A’s 1) front panel, 2) built-in web interface, and 3) Command Expert software. In a matter of minutes the 34980A will be making measurements, recording the commands sent to the 34980A and creating executable code for your choice of application software.
콘텐츠 잠금 해제
무료 가입
*Indicates required field
감사합니다!
귀하의 양식이 성공적으로 제출되었습니다.
Note: Clearing your browser cache will reset your access. To regain access to the content, simply sign up again.
×
판매 문의 부탁드립니다.
*Indicates required field
감사합니다!
A sales representative will contact you soon.