무엇을 찾고 있습니까?
Keysight Introduces First PCI Express® 6.0 Protocol Validation Tools
- Expands PCI Express 6.0 architecture solution portfolio with new Protocol Analyzer and Exerciser to enable advanced PCI Express 6.0 protocol and Compute Express Link validation
- Provides high-speed analysis up to 64 GT/s (PAM4) reducing the risk, cost, and time of PCI Express 6.0 technology silicon, endpoint, and root port prototyping and verification
- Offers cable-free protocol analysis in a streamlined form factor that speeds testing and accelerates time-to-market
SANTA ROSA, Calif. June 13, 2023
Keysight Technologies, Inc. (NYSE: KEYS) introduces the first PCI Express® (PCIe®) 6.0 protocol validation tools. The cable-free Protocol Analyzer and Protocol Exerciser enable semiconductor, computer, and peripheral makers to perform complete silicon chip, root complex, and endpoint system verification in a real-time development environment.
The PCIe 6.0 specification is a new high-speed serial interface standard released by the PCI-SIG® supporting the higher data traffic and bandwidth requirements of data centers. With the standard enabling new designs for servers, endpoint devices, switches, storage devices, and compute engines at speeds up to 64 gigatransfers per second (GT/s), equipment and device companies need protocol test solutions to validate PCIe 6.0 technology designs and ensure interoperability with other PCIe 6.0 specification compliant designs.
Keysight meets the need of design engineers with the first PCIe 6.0 Protocol Analyzer and PCIe 6.0 Protocol Exerciser. These cable-free solutions provide testing versatility and enable faster, more confident testing of PCIe 6.0 technology designs.
The new Keysight protocol PCIe 6.0 architecture solutions offer:
- Analysis of the data link / transaction layer of PCIe 6.0 technology designs
- Support for all PCIe technology speeds – 2.5 GT/s, 5.0 GT/s, 8 GT/s, 16 GT/s, 32GT/s, and 64GT/s (PAM4) – and lane widths from x1 to x16
- Emulation of root complex and endpoint devices when validating PCIe and Compute Express Link (CXL) technology designs
- Debugging support with PCIe 6.0 technology and CXL 1.1 / 2.0 protocol visualization and analysis tools
- Cable-free protocol analysis in a streamlined Card Electromechanical (CEM) form factor
- Complete PCIe 6.0 standard test solution for the entire design cycle
Jim Pappas, Director of Technology Initiatives Intel, said: "PCI Express 6.0-based I/O technology is expected to deliver a breakthrough performance in high-performance I/O interfaces. It also enables additional innovations including accelerator interconnects like Compute Express Link and on-chip communications such as Universal Chiplet Interconnect Express. PCIe 6.0 capable protocol analyzer and exerciser test equipment from companies including Keysight Technologies are critical to accelerating the development, deployment, and dissemination of high-performance I/O technologies on future Intel platforms and throughout the industry."
Al Yanes, Chairman of the PCI-SIG®, said: "The PCI-SIG is pleased to see PCIe 6.0 technology test tools start to become available to its members from member companies such as Keysight Technologies. We appreciate Keysight's continued efforts to support PCIe technology and the time, effort and expense Keysight along with other test vendors put into new tool development to allow our members to support the new advances in the PCI Express specification."
Dr. Joachim Peerlings, Vice President of Network and Data Center Solutions at Keysight said: "In the race to advance artificial intelligence applications, physical layer and protocol validation of devices including networking interface cards, graphics processing units, and accelerators is key. With the revolutionary PCI Express 6.0 Protocol Analyzer and Exerciser, Keysight complements the portfolio of physical layer high-speed I/O and Ethernet physical and protocol solutions to enable the industry to test designs end-to-end."
Keysight's new PCIe 6.0 standard protocol solutions will be exhibited at the PCI-SIG Developers Conference 2023 in Santa Clara on June 13-14, 2023.
Resources
PCI-SIG®, PCIe® and the PCI Express® are US registered trademarks and/or service marks of PCI-SIG
About Keysight Technologies
At Keysight (NYSE: KEYS), we inspire and empower innovators to bring world-changing technologies to life. As an S&P 500 company, we're delivering market-leading design, emulation, and test solutions to help engineers develop and deploy faster, with less risk, throughout the entire product lifecycle. We're a global innovation partner enabling customers in communications, industrial automation, aerospace and defense, automotive, semiconductor, and general electronics markets to accelerate innovation to connect and secure the world. Learn more at Keysight Newsroom and www.keysight.com.
Keysight Contact:
Geri Lynne LaCombe, Americas/Europe
+1 303 662–4748
[email protected]
Fusako Dohi, Asia
+81 42 660–2162
[email protected]
The Keysight P5570A Analyzer and P5573A Exerciser enable advanced PCI Express 6.0 standard protocol validation at 64 GT/s with lane widths of x4, x8, and x16.
Need to contact Media Relations at Keysight?