무엇을 찾고 있습니까?
Keysight Accelerates RF System Design and Digital Mission Engineering Workflows for 5G Non-Terrestrial Networks
New PathWave System Design 2023 software offers channel modeling, simulation, and digital twins
SANTA ROSA, Calif., October 12, 2022
Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that delivers advanced design and validation solutions to help accelerate innovation to connect and secure the world, announces PathWave System Design (SystemVue) 2023 software to speed the design process for 5G non-terrestrial networks (NTN) and other wireless systems. The latest improvements to PathWave System Design empower radio frequency (RF) system designers to create digital twins of their architectures and transform from a hardware-centric to a simulation-centric design flow.
New 5G NTN systems have challenging complexity, which is stressing development lifecycles. Engineers are looking to commercial software solutions that connect with their existing environments and drive virtual prototyping of their systems in application-specific environments. Simulations that use measurement-derived models deliver higher fidelity in mission-critical applications such as satellite communications and aerospace defense. System architects want to explore real-world “what if” scenarios prior to building hardware to reduce technical risk and minimize time-to-market.
PathWave System Design 2023 software supports engineers working in radio frequency integrated circuit (RFIC), sub-assembly, and mission or system-of-systems applications by connecting system, baseband, and hardware verification tools in a complete RF system modeling workflow. Engineers can perform industry-leading phased array analysis that captures all non-ideal effects across channels and between amplifiers and antennas. New tool capabilities also enable frequency domain nonlinear system modeling to predict application-specific system behavior.
“5G applications are evolving towards 6G, requiring the need for tools that address the entire digital engineering design and validation workflow,” said Peter Blood, Director of Product Management for PathWave System Design at Keysight. “Organizations are demanding that systems are virtually prototyped in their target scenario, so system and mission engineers are turning to simulation, virtual prototyping, and digital twins. These techniques shift the development process left in time and remove the need for multiple physical prototypes. PathWave System Design blends simulation with measurement-derived models and offers a complete RF system workflow to rapidly architect, design, and verify these complex NTN systems with updated 5G libraries.”
PathWave System Design 2023 software key features and benefits include:
- An updated 5G transceiver to support NTN in conjunction with PathWave Vector Signal Analysis (89600 VSA) 2023. Enhancements include a full-featured channel model, which natively supports all the propagation characteristics for low, medium, and geostationary earth orbits, including large path delay and large-frequency Doppler Shift with trajectory visualization.
- Two new simulation user interfaces: the Digital Pre-distortion (DPD) Explorer for circuit level designers in PathWave Advanced Design System (ADS) and the DPD Designer for architects in PathWave System Design. These enhancements deliver unprecedented efficiency, flexibility, speed, and fidelity enabled by Keysight’s compact waveforms and new graphical user interfaces. The new Dynamic Gain model delivers unrivaled power amplifier modeling with memory effects and supports workflow with other Keysight software and instrumentation for extraction.
- New Load Pull modeling that creates the ultimate phased array digital twin with power amplifier models derived from Keysight instrumentation or circuit-level simulation. Phased array architects can be confident that their system simulation delivers the highest accuracy due to Keysight’s expertise in RF measurement science.
- Connectivity with Keysight’s EXata software and PROPSIM Channel Studio software that enables mission engineers to create a 5G network-level digital twin. High-fidelity physical layer analysis from PathWave System Design and PROPSIM channel models enhance a unique blend of statistical simulation from EXata. Designers can evaluate network-level performance of NTN communications systems without compromising on fidelity, complexity, or simulation speed.
Find more information about PathWave System Design 2023 here.
Find more information about PathWave Vector Signal Analysis 2023 here.
About Keysight Technologies
Keysight delivers advanced design and validation solutions that help accelerate innovation to connect and secure the world. Keysight's dedication to speed and precision extends to software-driven insights and analytics that bring tomorrow's technology products to market faster across the development lifecycle, in design simulation, prototype validation, automated software testing, manufacturing analysis, and network performance optimization and visibility in enterprise, service provider and cloud environments. Our customers span the worldwide communications and industrial ecosystems, aerospace and defense, automotive, energy, semiconductor and general electronics markets. Keysight generated revenues of $4.9B in fiscal year 2021. For more information about Keysight Technologies (NYSE: KEYS), visit us at www.keysight.com.
# # #
Additional information about Keysight Technologies is available in the newsroom at https://www.keysight.com/go/news and on Facebook, LinkedIn, Twitter, and YouTube.
Keysight Contact:
Geri Lynne LaCombe, Americas/Europe
+1 303 662–4748
[email protected]
Fusako Dohi, Asia
+81 42 660–2162
[email protected]
5G system designers realize the full breadth of Non-Terrestrial Networks with PathWave System Design’s new 3GPP release 17-compliant channel model.
Need to contact Media Relations at Keysight?