이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

자동화 X-레이 검사

키사이트는 자동화 광학 및 자동화 X-레이 검사 사업을 철회할 예정입니다. 2009년 3월 1일부터 시작하여 지원이 종료될 때까지(제품 생산이 중단되는 때부터 7년간) 키사이트는 기존의 보증 및 지원 계약 의무를 충실하게 이행할 것이며 예비 부품, 시간 및 재료 서비스 및 자체 지원 옵션을 제공할 예정입니다.

이번 사업 철회 발표에 관한 FAQ 목록을 보려면 www.keysight.com/find/inspection을 방문하십시오.

키사이트는 PCB 어셈블리 테스트 시장에서 인서킷 테스트(ICT)기능 테스트 제품 제품군을 확장하기 위해 모든 기업적 노력을 기울이고 있습니다.

1-25 / 118

정렬방식:
5DX Windows 7 Controller Upgrade - Flyer
Upgrade your 5DX AXI PC controller to enjoy better inspection performance.

브로셔 2017-12-01

PDF PDF 547 KB
Automated X-Ray Inspection System Keysight Technologies - Technical Overview
This is a technical datasheet. Keysight has developed a sealed ultra-high vacumn X-ray tube that provides stable output throughout a significantly long life.

기술 개요 2015-03-24

PDF PDF 644 KB
Maximize Your Keysight AXI Coverage with Flexible Pricing - Brochure
This flyer describes the different support options Keysight AXI users can select from to ensure peace of mind for covering the support needs of their 5DX and x6000 investments.

브로셔 2014-07-31

PDF PDF 141 KB
Problem with Subtype Learning When Used with the Connector Algorithm in R7.0
5DX Technical Paper - Problem with Subtype Learning When Used with the Connector Algorithm in R7.0

어플리케이션 노트 2013-10-29

PDF PDF 16 KB
Ball Grid Array Joint Inspection Using X-ray as it relates to voids and the IPC-7095A specification
With the introduction of Lead-free solder, voiding within Ball Grid Array (BGA) joints is potentially a major issue. This article discusses the relationship to voiding, the IPC standard and Automated X-ray Inspection.

특집 기사 2012-12-06

PDF PDF 105 KB
Diagnostic Testing and the Medalist 5DX Automated X-ray Inspection System
Users of the Medalist 5DX automated x-ray inspection system can benefit from running diagnostic tests on a regular basis. This application note provides some guidelines.

어플리케이션 노트 2009-01-14

PDF PDF 188 KB
Successful Implementation of the Keysight Medalist x6000 AXI Solution – The Pyramid Concept
This aplication note provides a pyramid concept that outlines how users can successfully leverage the powerful defects detection capabilities of the Keysight Medalist x6000 automated x-ray inspection system to reduce their production and life cycle costs and improve product quality.

어플리케이션 노트 2008-11-19

PDF PDF 55 KB
Exposed Pad Algorithm for the Medalist x6000 AXI System
This application note describes how to use the exposed pad algorithm in the Medalist x6000 AXI software to test all varieties of QFN and FET package types for defects such as Open and Voiding.

어플리케이션 노트 2008-10-21

PDF PDF 1.83 MB
Setting Up HotKeys for AXI products on the Keysight Medalist Repair Tool
Users of the Keysight Medalist Repair Tool, also known as the Keysight Repair Tool (ART), can setup hot keys to increase the efficiency of image viewing in RT4.0 for their X-ray inspection products.

어플리케이션 노트 2008-09-26

PDF PDF 629 KB
codeNexus - Defect Reporter
Defect Reporter enchancement for the Medalist 5DX Automated X-ray Inspection System

어플리케이션 노트 2008-09-26

PDF PDF 764 KB
Build Operator Menu: Multiple Menu Configuration Control for 5DX Auto User Interface
The "Build Operator Menu" software replaces and extends the functionality found in the BLDOPMNU DOS command. This application note provides useful user information about this menu.

어플리케이션 노트 2008-09-04

PDF PDF 849 KB
Adjusting the X-ray Surface Map parameters on the Medalist 5DX Automated X-ray System
Tips on obtaining the best images using the 5DX surface map parameters.

어플리케이션 노트 2008-08-27

Quad Flat No Lead (QFN) Best Practices
The purpose of this application note and best practices guide is to describer the QFN-type component and provide testing methods to ensure robust testing on the Medalist 5DX Automated X-ray Inspection (AXI) System.

어플리케이션 노트 2008-08-26

PDF PDF 492 KB
Keysight 5DX 8.50 Software Release
The Keysight Technologies Automated X-ray Inspection System 8.50 software release for the 5DX is available.

릴리스 노트 2008-08-21

Using the FET Algorithm on the Medalist 5DX AXI to Analyze Non-Standard Joints
A new algorithm family called FET for the Keysight Medalist 5DX automated X-ray inspection (AXI) system helps users to effectively analyze non-standard joints for insufficient or no solder, non-reflowed or cold solder, and excessive voiding.

어플리케이션 노트 2008-07-01

PDF PDF 553 KB
Adjusting the Defect Analyzer detection parameters on the Medalist 5DX Automated X-ray System
Defect Analyzer operates by making a small change in the ‘z’ height of the board and re-testing suspect joints.

어플리케이션 노트 2008-06-12

Keysight 5DX operation manual
This is a operation manual that describes the safety and operation for 5DX

작동 매뉴얼 2008-06-01

Results from 2007 Industry Defect Level and Test Effectiveness Studies
To select an optimal test strategy, good knowledge of defect levels and test effectiveness are two very important factors to include. This paper presents data from a 2007 study of 3.7 billion solder joints. Reprinted with permission from IPC.

기사 2008-05-21

PDF PDF 118 KB
Article reprint: Impact of Quad Flat No Lead Package (QFN) on Automated X-ray Inspection (AXI)
This paper discusses lack of industry specification for QFN inspection, how AXI methodology was improved to detect QFN solder joint defect, design for inspection and future work.

기사 2008-03-06

PDF PDF 1.63 MB
How CAD Data and Threshold Settings Affect Pin Length on the Keysight Medalist 5DX
This application note describes the effects of CAD data and threshold settings on pin lengths while working on the Medalist 5DX Automated X-Ray Inspection system.

어플리케이션 노트 2008-02-22

PDF PDF 124 KB
Comparing CAD and BOM data for 5DX Use
Instructions for comparing CAD and BOM data to quickly deal with no load components.

어플리케이션 노트 2008-01-04

PDF PDF 1.16 MB
Keysight x6000 operation manual
This is a operation manual that describes the safety and operation for x6000.

작동 매뉴얼 2007-12-01

Xray Choices for SMT Manufacturing
In many cases, there is a complementary choice of automated 3D X-ray and off-axis 2D X-ray inspection. This article explores this concept. Published with kind permission from SMT

기사 2007-11-01

PDF PDF 188 KB
Tips for X-ray Users On Exporting NDF’s With No Loads Set To False
Navigating CAD can be a time consuming process. Small tips can be extremely helpful in creating quality programs in a short amount of time.

어플리케이션 노트 2007-10-18

X-ray Test Users Utilize BOM Explorer to Change
Automated X-ray Inspection 5DX Users can save time by implementing these quick and easy steps to use BOM explorer to change "no pops" to "untested".

어플리케이션 노트 2007-10-12

1 2 3 4 5 다음