Highlights of PathWave Test Automation Deployment 9.23:

  • Use PluginTypeSelectorAttribute for Mixin selector
  • Add MacOS to Nuget Package
  • Make IMixinBuilder an ITapPlugin 
  • Various bug fixes and performance improvements

Full Release Notes:

OpenTAP Release Highlights

ダウンロード方法

  1. Click the Download Button
  2. Save the installer

インストール方法

  1. Click the Download button
  2. Edit the file properties to make .Deployment file executable 
  3. Double-click the .exe file to launch the installer
 

ライセンス

  • Requires a License

Installs on: PC

OS

  • Ubuntu 20.04
  • Ubuntu 22.04

前提知識

  • Information Not Available