技術概要
Introduction
Digital Audio Broadcasting (DAB) is the most widely adopted technology for digital radio broadcasting. DAB-based standards, including the recently developed DAB+ and DMB, support video and data services in addition to audio service.
The British standard, BS EN 50248 “Characteristics of DAB Receivers”, describes DAB receiver characteristics for commercial equipment intended for terrestrial and cable reception in band III and L- band and for satellite reception in L-band.
This document discusses the measurement configurations and procedures for DAB receiver RF performance test using Keysight Technologies, Inc. instruments, according to BS EN 50248.
DAB Receiver Test Demonstrations
Overview of requirements for DAB receiver test
BS EN 50248 includes both basic and functional performance requirements for DAB receivers, as well as the minimum performance levels and measuring methods. The RF performance tests stipulated in the standard are as follows.
Sensitivity in a Gaussian channel
Maximum input power in a Gaussian channel
Selectivity, including two parts:Adjacent channel selectivity
Rejection of unwanted signals (far-off selectivity)
Performance in a Rayleigh channelSensitivity
Acquisition time after synchronization loss
All the measurements listed above need to be performed in both the VHF band and the L-Band as below:
VHF Band III: 174 MHz ~ 240 MHz
L-Band: 1452 MHz ~ 1492 MHz
The BER result of 10-4 is used as the criteria in all tests. The BER should be measured at the convolutional decoder output of the receiver and performed in the MSC (Main Service Channel) using an EEP (equal error protection) sub-channel with code rate ½. Note that while some receivers can provide BER results, if they cannot, an extra BER meter is required to measure the BER results. Any known digital pattern with a length of more than 1 symbol can be used as the test sequence – for example, all zero sequence.
Sensitivity and maximum input power in a Gaussian channel
Sensitivity and maximum input power are the minimum and maximum input signal levels of the DAB receiver at which the BER result meets the criteria as stipulated in BS EN 50248.
For the sensitivity test, the minimum requirement in EN 50248 is –81 dBm for both VHF band and L-band. If the measured power is lower than this value, it means the receiver passes the sensitivity test.
×
営業担当者からご連絡させていただきます。
*Indicates required field
ありがとうございました。
A sales representative will contact you soon.