Benchmarking PXB and Channel Emulator RF Fading Performance

アプリケーションノート

RF faders (channel emulators) allow engineers to comprehensively evaluate wireless communication systems by predicting their performance in response to real-world conditions. The Keysight Technologies, Inc. N5106A PXB baseband generator and channel emulator is a comprehensive diagnostic toolset for designing and verifying wireless signal processing devices. Unlike dedicated faders, the PXB combines real-time fading with multichannel baseband generation and signal capture in a single, multipurpose instrument.

While the benefits of such a combination are numerous, it is reasonable to question if the fading provided by the PXB rivals that of a dedicated RF fader. This application note is intended to specifically address that question by benchmarking the fading performance of the Keysight PXB against two well-known RF fading solutions: the Spirent SR5500 Wireless Channel Emulator and the Elektrobit Propsim C8 multichannel emulator. Test results will show that the PXB has fading performance comparable to that of the Spirent SR5500 and Elektrobit C8, moreover, it fully satisfies the performance specification in 3GPP TS 34.121-1 v8.6.0.

×

営業担当者からご連絡させていただきます。

*Indicates required field

ご希望の連絡手段を選択してください。*必須項目です。
Preferred method of communication? ご登録のEメールアドレスの変更
Preferred method of communication?

続行することにより、プライバシーポリシーにご同意頂いたものとみなします。 こちらのデータの利用方法については、キーサイトのプライバシーステートメントをご確認ください。キーサイトプライバシーステートメント にご同意頂いたものとみなします。また、弊社及び弊社販売店からご連絡を差し上げる場合がございます。

ありがとうございました。

A sales representative will contact you soon.