Measurement Wizard Assistant (MWA) Software for Network Analyzers

アプリケーションノート

In today’s fast-paced testing environments, with increasing functionality supported in devices under test (DUTs), network analysis is becoming more and more complicated. Many components have multiple RF input and/or output ports making multiport measurement a requirement for total device characterization. Complex multiport devices also have more parameters that need to be measured requiring engineers to spend a lot of time setting up the measurement system, an expenditure that leads to a loss of efficiency in product development and manufacturing test. To accelerate time to market, device manufacturers need easy-to-use software that guides them through whole measurement procedure and minimizes the time spent on setup and measurements. The Keysight Technologies, Inc. Measurement Wizard Assistant (MWA) software for the Keysight ENA network analyzer simplifies measurement procedures. MWA software supports multiport measurement on the 4-port ENA using the E5092A configurable multiport test set(s).

 

This application note explains how using MWA software on the ENA simplifies measurements and reduces the setup time of complicated measurements. It provides you with a step-by-step guide to the MWA and useful measurement tips for using the software.

×

営業担当者からご連絡させていただきます。

*Indicates required field

ご希望の連絡手段を選択してください。*必須項目です。
Preferred method of communication? ご登録のEメールアドレスの変更
Preferred method of communication?

続行することにより、プライバシーポリシーにご同意頂いたものとみなします。 こちらのデータの利用方法については、キーサイトのプライバシーステートメントをご確認ください。キーサイトプライバシーステートメント にご同意頂いたものとみなします。また、弊社及び弊社販売店からご連絡を差し上げる場合がございます。

ありがとうございました。

A sales representative will contact you soon.