Column Control DTX

Designing an Advanced MMIC Amplifier

Applikationsberichte

There are many design steps required for the development and manufacture of MMIC circuits, as illustrated in the MMIC Design Flow. Advanced Design System (ADS) is a central part of the complete MMIC design flow, and is used throughout this process. This application note illustrates, through the design of an MMIC amplifier, several of the common problems faced in designing, simulating, and producing a physical layout of an MMIC circuit, as well as the validation steps that are needed to verify that the physical layout still produces the desired result. It is beyond the scope of this note to describe all possible design specifications for an MMIC circuit, but it does include enough specification and design steps to address many common design challenges.

×

*Indicates required field

*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By clicking the button, you are providing Keysight with your personal data. See the Keysight -Datenschutzaussage Informationen darüber, wie wir diese Daten verwenden.

Thank you.

A sales representative will contact you soon.

Column Control DTX