Replicate RF Environments

小冊子

Keysight Understands Your Challenges

 

As the electromagnetic spectrum becomes progressively crowded, it is increasingly challenging to define and simulate test environments that represent real-world scenarios. Field testing can be both time-consuming and costly, with little probability of reproducing specific vulnerabilities and less chance of investigating the root cause of the problem.

 

Solving your test challenges

 

Keysight gives you the ability to test your designs and early prototypes in realworld environments before field deployment. 

You now can repeatedly test different scenarios in the laboratory as part of your performance test suite. Our solutions can help you test using the following environment scenarios

• Replicating ISM signals on a busy station platform

• Testing radar signals around a proposed 5G cell site

• Checking for adjacent interference at a satellite ground station

 

Services

 

Our general-purpose hardware and software have the capabilities for capturing wideband signals, post-capture analysis, creating custom signals, and generating wideband signals.

 

Keysight has cost-effective test solutions for replicating signals from actual locations using a graphical user interface.

 

Using our platforms, you can now

• Initiate recordings

• Preview spectrum and spectrogram create and access a signals library 

• Replay signal environments

 

Compact, commercial off-the-shelf hardware

• wideband signal capture

• streaming signal storage

• wideband signal generation

• comprehensive signal analysis

 

Scalability for additional functionality

• preselection / filtering

• up- and down-conversion

• multiple channels

• extra memory depth

 

The Keysight Z2082E-42x provides RF record / playback using Keysight M9203A digitizer and the Keysight M9336A arbitrary waveform generator in a compact PXI mainframe.

 

Our Experts

 

The crowded spectrum represents a challenge for radio coexistence and systems performance. Design validation benefits from both the simulation of the RF environment and exposure to real-world signals. The ability to perform this in the lab, in a controlled and repeatable way, gives measurement confidence in the early stages of the design cycle.

 

Keysight’s application experts will help you achieve your goals and keep a step ahead of your competition.

×

営業担当者からご連絡させていただきます。

*Indicates required field

ご希望の連絡手段を選択してください。*必須項目です。
Preferred method of communication? ご登録のEメールアドレスの変更
Preferred method of communication?

続行することにより、プライバシーポリシーにご同意頂いたものとみなします。 こちらのデータの利用方法については、キーサイトのプライバシーステートメントをご確認ください。キーサイトプライバシーステートメント にご同意頂いたものとみなします。また、弊社及び弊社販売店からご連絡を差し上げる場合がございます。

ありがとうございました。

A sales representative will contact you soon.