何をお探しですか?
Keysight Maintains Support for Leading Number of 5G Conformance Test Cases Mandated by GCF
5G device test platform used to achieve first validation of 5G RF demodulation test cases
SANTA ROSA, Calif., February 9, 2021
Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that helps enterprises, service providers and governments accelerate innovation to connect and secure the world, announced that the company maintains support for leading number of 5G new radio (NR) radio frequency (RF) and protocol conformance test cases mandated by the Global Certification Forum (GCF).
Keysight's support of GCF mandated conformance test cases, through the company's 5G network emulation platform solutions, enables one hundred and eight vendors to validate 5G devices across twenty different form factors. At the most recent Conformance Agreement Group (CAG) meeting, organized by GCF from 26 to 29 of January, it was also confirmed that Keysight's 5G device test platforms enabled the certification organization to validate the industry's first 5G RF demodulation test cases.
"Early access to 5G RF demodulation test cases speeds validation of the baseband chip within a 5G device, enabling the delivery of always-on connected experiences," said Muthu Kumaran, senior director of Keysight's wireless test group. "By supporting a leading number of GCF-validated test cases, 5G device vendors can quickly ramp up market introduction of new 5G products across any 3GPP-specified frequency band, in both non-standalone (NSA) and standalone (SA) mode."
Keysight's 5G network emulation solutions offer the industry's most comprehensive support for 5G RF and protocol test cases validated by either GCF or PTCRB, a certification forum led by representatives from leading U.S. mobile operators. Access to a wide range of 5G NR test cases, on common platforms, accelerates and simplifies device testing across 4G and 5G. By connecting data sets across the workflow, users can effectively streamline their validation processes, leading to shorter time to a market.
RF demodulation testing is critical to performance verification of a 5G device at baseband level. Compliance to the latest GCF-specified RF demodulation test cases ensures any improvements in connectivity, reliability and bandwidth introduced by 3GPP are correctly implemented by the 5G device vendor. The first demodulation test cases in mmWave spectrum, also referred to as frequency range 2 (FR2), support 5G device validation in NSA mode, which uses an evolved packet core (EPC) as an anchor for mobility management and coverage to support 5G carriers. The first demodulation test cases in FR1 (sub-7GHz spectrum) enable users to verify that a 5G device accurately reports the desired precoding matrix indicator (PMI), resulting in optimized system data throughput.
Keysight has maintained continuous support for a leading number of GCF-validated test cases specific to FR2 since July of 2019. Keysight's 5G device test solutions for FR2, which leverage the company's UXM 5G Wireless Test Platform and 5G over-the-air (OTA) compact antenna test (CATR) range chambers, enabled GCF to activate certification of 5G FR2 devices in October 2020. These solutions also enabled PTCRB to validate multicarrier 5G NR test cases in NSA mode for FR2 at the PTCRB validation group (PVG) meeting in November 2020.
About Keysight Technologies
Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps enterprises, service providers and governments accelerate innovation to connect and secure the world. Keysight's solutions optimize networks and bring electronic products to market faster and at a lower cost with offerings from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $4.2B in fiscal year 2020. More information is available at www.keysight.com.
# # #
Additional information about Keysight Technologies is available in the newsroom at https://www.keysight.com/go/news and on Facebook, LinkedIn, Twitter, and YouTube.
Keysight Contact:
Geri Lynne LaCombe, Americas/Europe
+1 303 662–4748
[email protected]
Fusako Dohi, Asia
+81 42 660–2162
[email protected]
Need to contact Media Relations at Keysight?