何をお探しですか?
Keysight’s New Regenerative Power Supplies Reduce Cooling and Electricity Costs with an Eco-friendly Design
Two new models - 20 kW and up to 2,000 V - provide high power and voltage for battery and electronics testing in hybrid-electric/electric vehicles (HEV/EV)
SANTA ROSA, Calif., June 16, 2020
Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that helps enterprises, service providers and governments accelerate innovation to connect and secure the world, today announced it is expanding the company's RP7900 Series with two new bidirectional, regenerative DC power supplies providing integrated safety features that protect people and devices under test (DUT). The unique regenerative design of the new models enables the energy normally consumed to be returned to the grid cleanly, saving costs associated with energy consumption and cooling.
The automotive industry is using larger batteries to extend the range of electric vehicles (EV) and higher voltage electronics to reduce charging time. In fact, MarketsandMarkets estimates nearly 39 percent CAGR growth by 2025 for high voltage batteries to support longer range cars and larger electric vehicles including buses and trucks. As the demand for high power grows, so does the need for high power test equipment. However, high power applications in aerospace defense and infrastructure, as well as automotive and energy, present unique challenges spanning site preparation necessities and safety requirements when transitioning from low power to high power.
Keysight's RP7900 is a part of the company's HEV/EV Power Converter Test Solutions which enable customers to deploy high-voltage, high-power solutions that meet the fast paced, high-growth demands of the hybrid-electric/electric vehicle (HEV/EV) market.
By combining the seamless source and load functionality into a compact 3U-high package, Keysight's RP7900 Series of regenerative power supplies minimizes high-power test costs by shrinking floor space usage, reducing heat dissipation and maintaining uptime.
These new power supplies, available in two models - 20 kW and up to 2,000 V - offer the following key features and benefits:
- Two-quadrant, bidirectional sourcing and sinking capability allows for seamless, uninterrupted transitions between sourcing and sinking current without changing the power supply's output characteristics or introducing any disruptive behavior.
- Autoranging output characteristic improves flexibility over rectangular, or traditional, output characteristic power supplies due to expanded power curve, which delivers more voltage and current combinations in one power supply.
- Provides fast output speed, sub-millisecond command-processing time (≤ 1 ms), and output list that help achieve significant throughput gains in testing.
- Offers simultaneous voltage and current measurement capabilities delivering high accuracy and resolution.
- Reduces rack space requirements due to superior power density in the power range of 20 kW in 3U height.
"The next generation of hybrid-electric and electric vehicle power electronics developed and manufactured by our customers require higher voltage, increased bandwidth and exceptional control capability in design qualification and manufacturing test," said Christopher Cain, vice president and general manager of Keysight's Electronic Industrial Products. "Keysight's RP7900 series power supply capabilities enable automated testing to accelerate time to market and lower operational costs, while the unique regenerative capability delivers substantial operational savings as load-current is converted into AC grid power, instead of simply dissipating as heat that must be further managed in the test environment."
Pricing and Availability
Keysight's RP7900 Series of regenerative power systems are available now, starting at USD $27,335.
Additional information is available at www.keysight.com/find/RP7900.
About Keysight Technologies
Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps enterprises, service providers and governments accelerate innovation to connect and secure the world. Keysight's solutions optimize networks and bring electronic products to market faster and at a lower cost with offerings from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $4.3B in fiscal year 2019. More information is available at www.keysight.com.
# # #
Additional information about Keysight Technologies is available in the newsroom at https://www.keysight.com/go/news and on Facebook, LinkedIn, Twitter, and YouTube.
Keysight Contact:
Geri Lynne LaCombe, Americas/Europe
+1 303 662–4748
geri_lacombe@keysight.com
Fusako Dohi, Asia
+81 42 660–2162
fusako_dohi@keysight.com
Need to contact Media Relations at Keysight?