何をお探しですか?
Keysight Introduces New Performance Test Solution for Benchmarking 5G Devices and Base Stations
Enables mobile operators to automate performance evaluation as new features and versions are available
SANTA ROSA, Calif., November 17, 2020
Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that helps enterprises, service providers and governments accelerate innovation to connect and secure the world, has introduced a new performance test solution that enables mobile operators to automatically benchmark and evaluate performance of 5G new radio (NR) devices and base stations in a laboratory environment.
Keysight's Performance Benchmarking Solution for Lab Networks enables mobile operators to flexibly, confidently and cost-effectively evaluate how 5G devices and 5G bases stations will perform in a live 5G NR network environment as new models, features and versions become available. The versatile test solution combines Keysight's Nemo Outdoor 5G NR Drive Test Solution, Nemo 5G Device Analytics software, and PathWave Test Automation, a test sequencer built on OpenTAP, an open source test automation engine, and complemented with a wide range of test cases to create an automated test environment.
"We're pleased to support mobile operators with an automated performance test solution that reduces time to market, while maintaining high quality standards, compared to manual processes," said Petri Toljamo, vice president and general manager for Nemo wireless solutions at Keysight. "Frequent updates to devices and base stations, as well as the introduction of new models and versions, require a simple, workflow-connected solution that generates a single performance score for each device or base station under test."
Keysight's 5G Performance Benchmarking Solution for Lab Networks enables mobile operators to:
- Evaluate multiple devices in a single test campaign using live base stations
- Evaluate a 5G base station (gNodeB) using a reference 5G device
- Compile key performance indicators (KPIs) across multiple test cases to generate a single score, reinforcing objective comparisons between the different models or versions under test
- Access a single user interface for test plan execution, analysis, report generation and access to historical records
- Expand test campaigns and evaluate advanced scenarios such as mobility by using OpenTAP and attenuators
"Keysight's integrated solutions improve test automation and accelerate performance evaluation in a test laboratory environment prior to deployment enables Erillisverkot to provide secure and reliable information and communications technology (ICT) services to public authorities," said Antti Kauppinen, head of department, mobile technology development and strategy, Erillisverkot Group. "Thorough and continuous testing of devices and network elements with new features and updates guarantees a smooth roll-out."
Users can combine Keysight's Performance Benchmarking Solution for Lab Networks with the company's 5G Device Benchmarking Toolset, a first-to-market solution launched in March 2020, to verify devices using Keysight's UXM 5G wireless test platform, a network emulator.
About Keysight Technologies
Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps enterprises, service providers and governments accelerate innovation to connect and secure the world. Keysight's solutions optimize networks and bring electronic products to market faster and at a lower cost with offerings from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $4.3B in fiscal year 2019. More information is available at www.keysight.com.
# # #
Additional information about Keysight Technologies is available in the newsroom at https://www.keysight.com/go/news and on Facebook, LinkedIn, Twitter, and YouTube.
Keysight Contact:
Geri Lynne LaCombe, Americas/Europe
+1 303 662–4748
geri_lacombe@keysight.com
Fusako Dohi, Asia
+81 42 660–2162
fusako_dohi@keysight.com
Need to contact Media Relations at Keysight?