検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

モジュラ・ネットワーク・テスタ

The introduction of the Keysight Modular Network Tester sets a new class of test equipment for installation & maintenance of state-of-the-art communications networks. The Modular Network Tester consists of a platform sporting all test engines required on today's and tomorrow's high-speed core and access networks, featuring innovative solutions to make the life of the outside-plant technicians easier. But it is not just another OTDR, not just another optical spectrum analyzer, not just a dispersion tester, or video microscope...it can be any or all of these instruments. It's all up to the end-user to decide which test engines and accessories he will need for his actual OSP tasks.

How is that possible? One simple word: "MODULAR". The Keysight Modular Network Tester is a testing platform that actually grows with the customer, an instrument that easily adapts as his needs change. Snap-On test engines allow the customer to choose the functionality of his instrument to fit the way that he works.

Hence, the Modular Network Tester is positioned as "The Perfect Fit" for the way OSP' technicians work, as well as for their I&M testing tools' budget.