検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

自動X線検査

Keysightは、自動光検査および自動X線検査事業から撤退することになりました。Keysightは、撤退後も保証およびサポートのすべての契約を遵守し、スペア部品、材料サービス、セルフ・サポート・オプションをサポート期間終了まで提供します。サポート期間は、2009年3月1日の販売終了日より7年間となります。

撤退のお知らせに関するFAQの一覧は、次のページを参照してください。 www.keysight.com/find/inspection

プリント回路基板アセンブリ(PCBA)テスト市場のインサーキット・テスト(ICT)およびファンクション・テスト製品については、今後も製品提供を拡張していきます。

1-25 / 62

並べ替え
Problem with Subtype Learning When Used with the Connector Algorithm in R7.0
5DX Technical Paper - Problem with Subtype Learning When Used with the Connector Algorithm in R7.0

アプリケーション・ノート 2013-10-29

PDF PDF 16 KB
Diagnostic Testing and the Medalist 5DX Automated X-ray Inspection System
Users of the Medalist 5DX automated x-ray inspection system can benefit from running diagnostic tests on a regular basis. This application note provides some guidelines.

アプリケーション・ノート 2009-01-14

PDF PDF 188 KB
Successful Implementation of the Keysight Medalist x6000 AXI Solution – The Pyramid Concept
This aplication note provides a pyramid concept that outlines how users can successfully leverage the powerful defects detection capabilities of the Keysight Medalist x6000 automated x-ray inspection system to reduce their production and life cycle costs and improve product quality.

アプリケーション・ノート 2008-11-19

PDF PDF 55 KB
Exposed Pad Algorithm for the Medalist x6000 AXI System
This application note describes how to use the exposed pad algorithm in the Medalist x6000 AXI software to test all varieties of QFN and FET package types for defects such as Open and Voiding.

アプリケーション・ノート 2008-10-21

PDF PDF 1.83 MB
Medalist 5DX自動X線システムでの製造不良アナライザの検出パラメータの調整
製造不良アナライザは、ボードのZ高さをわずかに変更し、疑わしい接合を再検査することによって動作します。

アプリケーション・ノート 2008-09-30

Setting Up HotKeys for AXI products on the Keysight Medalist Repair Tool
Users of the Keysight Medalist Repair Tool, also known as the Keysight Repair Tool (ART), can setup hot keys to increase the efficiency of image viewing in RT4.0 for their X-ray inspection products.

アプリケーション・ノート 2008-09-26

PDF PDF 629 KB
codeNexus - Defect Reporter
Defect Reporter enchancement for the Medalist 5DX Automated X-ray Inspection System

アプリケーション・ノート 2008-09-26

PDF PDF 764 KB
Build Operator Menu: Multiple Menu Configuration Control for 5DX Auto User Interface
The "Build Operator Menu" software replaces and extends the functionality found in the BLDOPMNU DOS command. This application note provides useful user information about this menu.

アプリケーション・ノート 2008-09-04

PDF PDF 849 KB
Medalist 5DX自動X線検査システムの表面マップ・パラメータの調整
Medalist 5DX自動X線検査システムの表面マップ・パラメータの調整

アプリケーション・ノート 2008-08-27

Quad Flat No Lead (QFN) Best Practices
The purpose of this application note and best practices guide is to describer the QFN-type component and provide testing methods to ensure robust testing on the Medalist 5DX Automated X-ray Inspection (AXI) System.

アプリケーション・ノート 2008-08-26

PDF PDF 492 KB
Using the FET Algorithm on the Medalist 5DX AXI to Analyze Non-Standard Joints
A new algorithm family called FET for the Keysight Medalist 5DX automated X-ray inspection (AXI) system helps users to effectively analyze non-standard joints for insufficient or no solder, non-reflowed or cold solder, and excessive voiding.

アプリケーション・ノート 2008-07-01

PDF PDF 553 KB
How CAD Data and Threshold Settings Affect Pin Length on the Keysight Medalist 5DX
This application note describes the effects of CAD data and threshold settings on pin lengths while working on the Medalist 5DX Automated X-Ray Inspection system.

アプリケーション・ノート 2008-02-22

PDF PDF 124 KB
Comparing CAD and BOM data for 5DX Use
Instructions for comparing CAD and BOM data to quickly deal with no load components.

アプリケーション・ノート 2008-01-04

PDF PDF 1.16 MB
X-線検査システム・ユーザへのヒント
X-線検査システム・ユーザへのヒント: "no loads" を "false" に設定して NDF でエクスポート

アプリケーション・ノート 2007-12-26

X線テストでBOMエクスプローラを使ってNo PopsをUntestedに変更
自動X線検査システム5DXをお使いの方は、以下の簡単な手順でBOMエクスプローラを使って"no pops"を"untested"に変更することにより、時間を節約できます。

アプリケーション・ノート 2007-11-21

x6000自動X線検査システムでのキャリアの使用法
x6000自動X線検査システムでは、いくつかの理由により基板を検査する際にキャリアの使用が必要となることがあります。

アプリケーション・ノート 2007-10-29

5DX users benefit from configuring Automatic Reporter
Keysight Medalist 5DX Automated X-ray Inspection users can avoid the hassle of stopping Automatic Reporter and deleting those .res files and image folders every time a fine tune of a program is done.

アプリケーション・ノート 2007-06-20

5DX Automated X-ray Inspection Software Internal Error Notification Tool AN
This application note describes the Initial installation, Configuration changes, and Operation of the 5DX Automated X-ray Inspection Software Internal Error Notification Tool.

アプリケーション・ノート 2007-04-23

PDF PDF 371 KB
DirectFET Algorithm Recommendations on the Keysight 5DX Automated X-ray Inspection System
This application note helps users understand how to optimize the 5DX Automated X-Ray Inspection system for the best performance on a DirectFET.

アプリケーション・ノート 2007-03-23

PDF PDF 22 KB
Save Time – Create a Defect Log on Each Board Tested with the 5DX Automated X-ray Inspection System
This App Note shows you how to create a defect log for 5DX AXI System

アプリケーション・ノート 2007-03-16

PDF PDF 205 KB
Quad Flat No-Lead (QFN) Application Note and Best Practices
This document provides details on QFN component test methodology and best practices to ensure robust testing and quality results. The QFN algorithm was introduced in 5DX software version 8.4, and enhanced and simplified in patch version 8.4.1.

アプリケーション・ノート 2007-01-31

PDF PDF 1.05 MB
X線/インサーキット・テスト環境での不良検出率の改善
X線/インサーキット・テスト環境[Keysight AwareTest xiソフトウェアを使用]でのケース・スタディから、ファンクション・テストの不良を半分に減らし、プロセス・テストで2倍の不良を発見できるという結果が得られました。

アプリケーション・ノート 2007-01-10

PDF PDF 748 KB
プリント回路基板におけるX線検査の経済性
Keysightは、米国の製造業者と協力して、現実の製造環境でのPCBAテスト・コストのモデリングと定量化に取り組みました。この研究では、テスト、不良解析、修理、再テストに関わるすべてを対象として、総テスト・コストに対するX 線の影響を評価しました。

アプリケーション・ノート 2006-12-26

PDF PDF 367 KB
Understanding the Corrected Gray Level Measurement in the PTH2 Algorithm for the 5DX Automated X-ray
The PTH2 Algorithm family has enabled many customers to dramatically reduce false calls and increase test effectiveness on plated through-hole joints. This note assists with understanding the key questions associated with this algorithm family.

アプリケーション・ノート 2006-12-12

Tips for Getting the Best Results On Fine Pitch Gullwing Components with Keysight’s 5DX AXI Systems
5DX Automated X-ray Inspection systems using post version 8.x software should use default values for FPGullwing. They are suitable without modification for the majority of FPGullwing subtypes.

アプリケーション・ノート 2006-11-14

1 2 3 次へ