検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

自動X線検査

Keysightは、自動光検査および自動X線検査事業から撤退することになりました。Keysightは、撤退後も保証およびサポートのすべての契約を遵守し、スペア部品、材料サービス、セルフ・サポート・オプションをサポート期間終了まで提供します。サポート期間は、2009年3月1日の販売終了日より7年間となります。

撤退のお知らせに関するFAQの一覧は、次のページを参照してください。 www.keysight.com/find/inspection

プリント回路基板アセンブリ(PCBA)テスト市場のインサーキット・テスト(ICT)およびファンクション・テスト製品については、今後も製品提供を拡張していきます。

1-25 / 122

並べ替え
5DX Windows 7 Controller Upgrade - Flyer
Upgrade your 5DX AXI PC controller to enjoy better inspection performance.

ブローシャ 2017-12-01

PDF PDF 547 KB
Automated X-Ray Inspection System Keysight Technologies - Technical Overview
This is a technical datasheet. Keysight has developed a sealed ultra-high vacumn X-ray tube that provides stable output throughout a significantly long life.

技術概要 2015-03-24

PDF PDF 644 KB
Maximize Your Keysight AXI Coverage with Flexible Pricing - Brochure
This flyer describes the different support options Keysight AXI users can select from to ensure peace of mind for covering the support needs of their 5DX and x6000 investments.

ブローシャ 2014-07-31

PDF PDF 141 KB
Problem with Subtype Learning When Used with the Connector Algorithm in R7.0
5DX Technical Paper - Problem with Subtype Learning When Used with the Connector Algorithm in R7.0

アプリケーション・ノート 2013-10-29

PDF PDF 16 KB
Ball Grid Array Joint Inspection Using X-ray as it relates to voids and the IPC-7095A specification
With the introduction of Lead-free solder, voiding within Ball Grid Array (BGA) joints is potentially a major issue. This article discusses the relationship to voiding, the IPC standard and Automated X-ray Inspection.

特集記事 2012-12-06

PDF PDF 105 KB
5DX 用 8.50 ソフトウェア・リリース
Keysight Medalist 5DX 自動 X線検査システム 8.50 ソフトウェア・リリース

リリース・ノート 2010-09-20

Diagnostic Testing and the Medalist 5DX Automated X-ray Inspection System
Users of the Medalist 5DX automated x-ray inspection system can benefit from running diagnostic tests on a regular basis. This application note provides some guidelines.

アプリケーション・ノート 2009-01-14

PDF PDF 188 KB
Successful Implementation of the Keysight Medalist x6000 AXI Solution – The Pyramid Concept
This aplication note provides a pyramid concept that outlines how users can successfully leverage the powerful defects detection capabilities of the Keysight Medalist x6000 automated x-ray inspection system to reduce their production and life cycle costs and improve product quality.

アプリケーション・ノート 2008-11-19

PDF PDF 55 KB
Exposed Pad Algorithm for the Medalist x6000 AXI System
This application note describes how to use the exposed pad algorithm in the Medalist x6000 AXI software to test all varieties of QFN and FET package types for defects such as Open and Voiding.

アプリケーション・ノート 2008-10-21

PDF PDF 1.83 MB
Medalist 5DX自動X線システムでの製造不良アナライザの検出パラメータの調整
製造不良アナライザは、ボードのZ高さをわずかに変更し、疑わしい接合を再検査することによって動作します。

アプリケーション・ノート 2008-09-30

Setting Up HotKeys for AXI products on the Keysight Medalist Repair Tool
Users of the Keysight Medalist Repair Tool, also known as the Keysight Repair Tool (ART), can setup hot keys to increase the efficiency of image viewing in RT4.0 for their X-ray inspection products.

アプリケーション・ノート 2008-09-26

PDF PDF 629 KB
codeNexus - Defect Reporter
Defect Reporter enchancement for the Medalist 5DX Automated X-ray Inspection System

アプリケーション・ノート 2008-09-26

PDF PDF 764 KB
Build Operator Menu: Multiple Menu Configuration Control for 5DX Auto User Interface
The "Build Operator Menu" software replaces and extends the functionality found in the BLDOPMNU DOS command. This application note provides useful user information about this menu.

アプリケーション・ノート 2008-09-04

PDF PDF 849 KB
Medalist 5DX自動X線検査システムの表面マップ・パラメータの調整
Medalist 5DX自動X線検査システムの表面マップ・パラメータの調整

アプリケーション・ノート 2008-08-27

Quad Flat No Lead (QFN) Best Practices
The purpose of this application note and best practices guide is to describer the QFN-type component and provide testing methods to ensure robust testing on the Medalist 5DX Automated X-ray Inspection (AXI) System.

アプリケーション・ノート 2008-08-26

PDF PDF 492 KB
Using the FET Algorithm on the Medalist 5DX AXI to Analyze Non-Standard Joints
A new algorithm family called FET for the Keysight Medalist 5DX automated X-ray inspection (AXI) system helps users to effectively analyze non-standard joints for insufficient or no solder, non-reflowed or cold solder, and excessive voiding.

アプリケーション・ノート 2008-07-01

PDF PDF 553 KB
Keysight 5DX operation manual
This is a operation manual that describes the safety and operation for 5DX

操作マニュアル 2008-06-01

Results from 2007 Industry Defect Level and Test Effectiveness Studies
To select an optimal test strategy, good knowledge of defect levels and test effectiveness are two very important factors to include. This paper presents data from a 2007 study of 3.7 billion solder joints. Reprinted with permission from IPC.

記事 2008-05-21

PDF PDF 118 KB
Article reprint: Impact of Quad Flat No Lead Package (QFN) on Automated X-ray Inspection (AXI)
This paper discusses lack of industry specification for QFN inspection, how AXI methodology was improved to detect QFN solder joint defect, design for inspection and future work.

記事 2008-03-06

PDF PDF 1.63 MB
How CAD Data and Threshold Settings Affect Pin Length on the Keysight Medalist 5DX
This application note describes the effects of CAD data and threshold settings on pin lengths while working on the Medalist 5DX Automated X-Ray Inspection system.

アプリケーション・ノート 2008-02-22

PDF PDF 124 KB
Comparing CAD and BOM data for 5DX Use
Instructions for comparing CAD and BOM data to quickly deal with no load components.

アプリケーション・ノート 2008-01-04

PDF PDF 1.16 MB
X-線検査システム・ユーザへのヒント
X-線検査システム・ユーザへのヒント: "no loads" を "false" に設定して NDF でエクスポート

アプリケーション・ノート 2007-12-26

Keysight x6000 operation manual
This is a operation manual that describes the safety and operation for x6000.

操作マニュアル 2007-12-01

X線テストでBOMエクスプローラを使ってNo PopsをUntestedに変更
自動X線検査システム5DXをお使いの方は、以下の簡単な手順でBOMエクスプローラを使って"no pops"を"untested"に変更することにより、時間を節約できます。

アプリケーション・ノート 2007-11-21

Xray Choices for SMT Manufacturing
In many cases, there is a complementary choice of automated 3D X-ray and off-axis 2D X-ray inspection. This article explores this concept. Published with kind permission from SMT

記事 2007-11-01

PDF PDF 188 KB

1 2 3 4 5 次へ