Why visit the Keysight booth at productronica?

Keysight enables innovators to push the boundaries of engineering by quickly solving design, emulation, and test challenges to create the best electronic manufacturing experiences. Whether you’re looking to empower IIoT networks for Industry 4.0, e-mobility or autonomous driving, or test RF components or digital compliance, Keysight accelerates innovation with intelligent insights that reduce risk and speed time to market.

Date and Location

November 14 – 17, 2023
Messegelände/ICM,
Am Messesee,
81829 München,
Germany

Hall A1.576

Demonstrations

Inline high-density ICT

The Keysight i3070 Series 7i E9988GL inline, high-density in-circuit test (ICT) system has Quad-Density pin cards that can provide up to 5760 test nodes in a slim footprint. This enables manufacturers to economically meet increasing test demands for large printed circuit board assembly (PCBA). It also protects manufacturers’ existing investments by maintaining backward compatibility with Keysight i3070 Series 5i E9988E / E9988EL test programs, including fixtures.

MFT 19” i3070 test handler

IPTE MFT 19 test handler

The MFT 19” Keysight i3070 test handler is a 19” rack-type handler for parallel in-circuit tests on PCBs that are routed through the handler on transport belts. The handler’s multi-functionality lies in the fact that the modular MFT 19 provides single lane, dual lane, single segment, dual segment, single well, and dual well configurations, enabling up to four times an increase in throughput compared to a standard single lane tester.

Combined ICT and FCT

A scalable combined in-circuit test (ICT) and functional component/circuit test (FCT) system breaks the traditional split of systems. Ultimately, this offers customers the flexibility to combine and streamline test coverage of both ICT and FCT, providing a more efficient balance between throughput and test coverage, which helps customers achieve improvements in cost-of-test.

End-to-end testing for PLM

PLM ecosystems are the backbone of product development with many interconnected systems that make comprehensive testing a challenge. The Eggplant Test Automation software excels in adapting to diverse CAD/PLM environments, comprehensively automating rich and thin client testing with customizations, and enabling unrestricted testing of 3D moving images and PLM functionality evaluation. From the demo, customers will see Eggplant’s ability to facilitate end-to-end testing in different PLM environments.

Cross-instrument automation

Keysight will demonstrate the PathWave Test Automation suite to show the open-source environment, test sequencer, and system management tools available in this powerful software. PathWave Test Automation delivers significant cost- and time-saving benefits over traditional test automation and analysis tools. It offers graphical user interfaces for test plan development, optimization, and management so you can easily visualize, compare, and share test results across teams.

Big data analytics

Combining test and measurement expertise with data science and big data engineering, the PathWave Manufacturing Analytics platform provides actionable insights for every level in your organization in the smart factory of the future. Improve yield, lower retest, and handling, and lower the cost of poor quality with big data advanced analytics that really works. Accelerate your Return on Investment and business outcomes with unique, innovative analytics.

Next-gen compliance test

Experience a new level of speed with the most advanced oscilloscopes on the market – the new Infiniium UXR-B and MXR-B Series. With the highest performance, lowest noise, and fastest speed, these oscilloscopes help you take your compliance testing to the next level. The new B-Series offers up to two times faster testing for multi-gigabit automotive ethernet, PCIe, and USB – dramatically reducing your device validation time. The Infiniium oscilloscope line also has industry-leading signal integrity and provides fully upgradeable channels and bandwidth. Visit the Keysight booth to experience the new B-Series and discuss your measurement challenges with our test experts.

Infiniium UXR-B

One-stop RF device testing

E5081A ENA-X Vector Network Analyzer

The importance of distortion measurement using the actual modulated signal is increasing for active RF components such as power amplifiers. Join us to learn how to cover multiple measurement parameters with a single connection, including noise figure, EVM, adjacent channel power ratio (ACPR), and standard S-parameters. Our spectral correlation technique directly analyzes the modulated input and output signals in the frequency domain while applying full vector correction at the device under test (DUT) plane.

1U multi-channel SMU

New at the Keysight stand this year is the latest SMU solution that addresses your growing footprint challenges. Solve your design, test, and validation challenges with the PZ2100 SMU solution, providing multiple SMU module options. This solution integrates 20 SMU channels into a valuable 1U height, with multiple capabilities such as pulser and digitizer, as well as precise voltage/current source measures to adapt to a wide range of application requirements. Also speed time-to-market with flexible software options, simplified system integration and synchronization, and application-specific measurement capabilities. 

Industrial IoT devices test

Keysight NB-IoT & LTE-M signaling tester

Keysight NB-IoT & LTE-M signaling tester can help you to solve manufacturing test challenges, for instance, ensuring there is proper communication with SIM card of the device by retrieving certain information such as the IMSI number. In addition, the solution will check that the device is able to connect to the base station emulator (X8801A), which requires a stable and healthy SIM card operation. Next, the solution emulates a challenging but realistic network connection, where the signal perceived by the device is at a very sensitive level (example: -120 dBm/180 kHz). The device will be tested to ensure it is able to initiate the attach procedure with the base station emulator at this sensitive level.

Next-generation bench solutions

Next-generation bench solutions enable engineers to address today’s increasingly complex range of measurement challenges. Keysight’s bench solutions are designed to provide the broadest range of power and measurement solutions – from dependable and compact multi-channel power supplies to versatile data acquisition systems with digitizer and solid-state multiplexer modules. Experience again our solutions trusted for decades such as the 6.5-digit Truevolt DMM and MegaZoom technology in InfiniiVision Scopes, or discover Keysight’s latest battery test, profiler, and emulation solution. 

Keysight online store

shopping cart

Benefit from free 2-day delivery for many products

The Keysight online store is more than just an electronic order portal, including access to Keysight Technical Experts and Easy Online Purchase using Credit Cards.

Ask for a special offer available at the booth!

KeysightCare

KeysightCare

Discover KeysightCare. Talk to us to see how KeysightCare offers dedicated, proactive support through a single point of contact for instruments, software, and solutions. Get faster response times, faster access to specialized experts, and faster time to resolution. Beyond KeysightCare, get more from your test instruments with broad services offerings, including calibration and repair, technology refresh, consulting, and training.

Want help or have a question?