Column Control DTX

Massive MIMO Testing with PROPSIM 5G Channel Emulation Solution

Application Notes

The Building Blocks of a Massive MIMO Test Environment

The cornerstone of a massive MIMO test setup is a channel emulator. The test solution connects a base station with 32 antenna ports to four user equipment (UE) devices, each having two antenna ports. This process requires a PROPSIM F64 channel emulator equipped with 64 RF channels and 512 logical links between the base station and the UE devices when connected bidirectionally.

With a PROPSIM F64-based setup, it is possible to test with commercial devices for both base stations and UEs. The test setup uses test and measurement equipment, such as signal and spectrum analyzers, to monitor system behavior and performance. Combining multiple channels into a single port enhances the capacity of the channel emulator. (See “Introducing Partial Sampling in a Massive MIMO Test Environment,” which describes how to set up a test with combiners.)

×

Please have a salesperson contact me.

*Indicates required field

Preferred method of communication? *Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By clicking the button, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you.

A sales representative will contact you soon.

Column Control DTX