Column Control DTX

Automating the Lightwave Component Analyzer with SCPI

应用文章

The Keysight N437x Series Lightwave Component Analyzer (LCA) is a solution which integrates a vector network analyzer (VNA) along with a calibrated lightwave test set to measure the transfer function of electrical to electrical (EE), electrical to optical (EO), optical to electrical (OE), and optical to optical (OO) components. Similar to a vector network analyzer both the magnitude and phase response of a component are characterized as a function of frequency. Typical measurements performed by the LCA include: gain, bandwidth, frequency response, flatness, and electrical return loss. A key value of the LCA is that the calibrated response of the lightwave test set is automatically de-embedded from the measurement and the reported results are isolated to the optical component under test. Additional information on the measurement fundamentals for the LCA can be found in the Keysight application note, High Speed Lightwave Component Analysis. [1] In this paper, we will review the steps required to automate the N437xA LCA and provide suggestions to help a new user quickly integrate the LCA into their automated test environment.

×

请销售人员联系我。

*Indicates required field

您希望以何种方式进行联系? *必填项
Preferred method of communication? 更改电子邮件地址?
Preferred method of communication?

请通过单击按钮,提供给是德科技您的个人数据。请在Keysight隐私声明 中,参阅有关我们如何使用此数据的信息,謝謝。

感谢您!

A sales representative will contact you soon.

Column Control DTX