Choose a country or area to see content specific to your location
애플리케이션 노트
The Keysight N437x Series Lightwave Component Analyzer (LCA) is a solution which integrates a vector network analyzer (VNA) along with a calibrated lightwave test set to measure the transfer function of electrical to electrical (EE), electrical to optical (EO), optical to electrical (OE), and optical to optical (OO) components. Similar to a vector network analyzer both the magnitude and phase response of a component are characterized as a function of frequency. Typical measurements performed by the LCA include: gain, bandwidth, frequency response, flatness, and electrical return loss. A key value of the LCA is that the calibrated response of the lightwave test set is automatically de-embedded from the measurement and the reported results are isolated to the optical component under test. Additional information on the measurement fundamentals for the LCA can be found in the Keysight application note, High Speed Lightwave Component Analysis. [1] In this paper, we will review the steps required to automate the N437xA LCA and provide suggestions to help a new user quickly integrate the LCA into their automated test environment.
콘텐츠 잠금 해제
무료 가입
*Indicates required field
감사합니다!
귀하의 양식이 성공적으로 제출되었습니다.
Note: Clearing your browser cache will reset your access. To regain access to the content, simply sign up again.
×
판매 문의 부탁드립니다.
*Indicates required field
감사합니다!
A sales representative will contact you soon.