Automotive Ethernet provides the new backbone for faster networks to serve autonomous vehicles and advanced driver assistance systems (ADAS). These technologies require higher bandwidth and lower latency. Keysight offers full scale solutions for in-vehicle network standard conformance, functional and performance testing from physical Layer 1 though higher-layer protocols up to Layer 7.

Visit the Keysight booth to view a demonstration and speak with the experts.

Who should attend?
Engineers and technicians seeking to learn about Automotive Ethernet technology and testing in automotive applications.

Dates and Times
12–13 February, 2020
9:00am-5:00pm

Location
The Westin Grand Munich
Arabellastrasse 6
81925
Munich, Germany

Register Here

Demonstrations

Agenda

Presenters

Agenda

Keysight experts will contribute to the following program topics.

Date and Time
13 February, 2020
9:30am

Session 4: Validation and Test
Ensuring Security of Data Communication in an IVN and Comparing the Choice of Encryption Techniques

Connected car security is one of the biggest concerns in the automotive world. With automotive Ethernet, in-vehicle networks are adopting a shared network design. The number of Electronic Control Units (ECU), sensors, and interconnects in cars is growing. ECUs in different car domains will interconnect with Ethernet backbones. Encryption is an established technique in the networking world for securing data communications in a shared network. There are different methods of encryption at different layers of an Ethernet stack. Though the traditional networking world uses encryption techniques, adoption in an automotive environment with time-critical applications and a new automotive physical layer is not proven. Proper adoption requires sophisticated validation methods in the network test cycle. This presentation will focus on the effectiveness of different encryption methods (for example, IPSec or MACsec) in the car network and validation methodologies.

Date and Time
13 February, 2020
11:00am

Session 5: Layer 2
When Gates Misbehave for IEEE 802.1Qbv Implementation

IEEE 802.1Qbv provides scheduling across bridges for time-critical application traffic. This ensures predictable and low-latency end-to-end paths for industrial and in-vehicle applications that require precise communication. Accuracy is essential when implementing 802.1Qbv in production devices. Metrics for accuracy measurement include the phase jitter of the opening and closing of time gate queues. A positive phase jitter, in which a gate fails to close within a specified time frame, can allow unwanted bandwidth into the network. For an automotive network, this can cause havoc in terms of the protocol’s data unit (pdu) signal not reaching their destination on time. The applications that typically run inside a car are time-sensitive in nature which needs bounded latency and guaranteed delivery. Requirements of a time sensitive network can only be met by ensuring traffic-shaping paradigms such as time-aware shaper function properly in an automotive network. This presentation will focus on the automotive scenarios where time-sensitive networking paradigms play a major role. We will dive into time-aware shaper implementations, cases where they go wrong, and the impact on an in-vehicle network. This presentation will also cover how to characterize misalignment of time-gated queues in the validation phase and the unique testing challenges.

Presenters

Avik Bhattacharya, Product manager for automotive and industrial Ethernet validation solutions

Avik Bhattacharya is the product manager for automotive and industrial Ethernet validation solutions in Keysight’s Ixia Solutions Group. Since 2007, he has worked on cutting-edge networking technologies, including routing, switching, multiprotocol label switching, software-defined networking, and time-sensitive networking (TSN). During that time, his roles have included research and development engineer, engineering manager, and now product manager. As an expert in automotive and industrial network testing, he is a frequent presenter at technical events and a contributor to technical blogs and articles. Avik holds a bachelor of technology degree in computer science and completed his MBA in international business.

Tanuman Bhaduri, Network communications engineer

Tanuman Bhaduri is a network communications engineer. He has worked in the communication industry for more than nine years. Tanuman is an audio video bridging (AVB)/ TSN expert in the Ixia Solutions Group at Keysight Technologies and has been the key designer for the AVB conformance and functional solution. He has co-authored a book on advanced programming. Tanuman holds a master’s degree in computer science from the University of Calcutta.

Have questions or need help?