Keysight Enables Advanced Pre-Tapeout Silicon Prototyping Using Digital Twin Signaling

  • Platform provides a unique real-time development environment that reduces the risk, cost, and time associated with silicon chip prototyping and verification
  • Integration with Keysight’s complete library of full-speed digital twin signals for full system verification in pre-tapeout environment
  • Supports development applications for 6G and other emerging high-speed communication technologies

SANTA ROSA, Calif. May 10, 2023 

Keysight Technologies, Inc. (NYSE: KEYS) released a new Universal Signal Processing Architecture (USPA) prototyping platform, enabling semiconductor companies to conduct complete chip prototyping and verification, pre-tapeout, in a real-time development environment integrating digital twins of fully-compliant, standards-based signals. 

The final step of the chip design process, known as the silicon tapeout, is an increasingly expensive procedure that leaves little room for design failure. If a design fails following the tapeout, chip makers must start over again with a new "re-spin" that can take 12 months or longer to complete. In addition to tying up valuable research and development resources, these chip redesigns can potentially cause the chip maker to miss a narrow time-to-market window.

To reduce the risks of design failures and expensive re-spins, the Keysight USPA platform provides chip designers and engineers with complete digital twin signaling to verify designs before they are committed to silicon. The USPA platform offers designers an alternative to proprietary custom prototyping systems by integrating ultrafast signal converters with a high performance, completely modular field-programmable gate array (FPGA) prototyping system.

The unique USPA prototyping platform offers the following benefits:

  • Supports the highest performance optoelectronic development projects with digital-to-analog converter (DAC) and analog-to-digital converter (ADC) interfaces that emulate signals at full speed, up to 68 GS/s (ADC) and 72 GS/s (DAC).
  • Provides a broad range of input / output interfaces that are suitable for applications including 6G wireless development, digital radio frequency memory, advanced physics research, and high-speed data acquisition applications, such as radar and radio astronomy.
  • Offers flexibility with two configurations, including a pre-configured system for single channel transceiver applications and a fully configurable set of modular components that can be combined to support a wide range of single and multi-channel applications. In addition, the pre-configured system can be expanded with additional components that leverage the modularity, scalability, and cost-effective reusability of the platform architecture.

 

Hong Jiang, CEO Avance Semi, Inc. said: "When we began work on our first ASIC for the coherent fiber communication market, we understood that we might only have one chance to get it right and that a second tapeout would be both prohibitively expensive and so time- consuming that we could miss our narrow time-to-market window. With Keysight's USPA platform and our system integration effort, we can optimize and verify our design in real-time as it progresses. This is like a "free soft tapeout" we can run as many times as needed. This approach saves development time and money while dramatically increasing confidence in our design and product release timeline."

Dr. Joachim Peerlings, Vice President and General Manager of Keysight's Network and Data Center Solutions Group, said: "By accelerating and de-risking chip development, Keysight USPA delivers a new end-to-end solution that meets the challenges of leading-edge designs in a very high-cost environment. This powerful platform gives chip developers a digital twin of their future silicon device, allowing them to fully validate their designs and algorithms before incurring the expense and risk of a tapeout."

Resources

About Keysight Technologies

At Keysight (NYSE: KEYS), we inspire and empower innovators to bring world-changing technologies to life. As an S&P 500 company, we’re delivering market-leading design, emulation, and test solutions to help engineers develop and deploy faster, with less risk, throughout the entire product lifecycle. We’re a global innovation partner enabling customers in communications, industrial automation, aerospace and defense, automotive, semiconductor, and general electronics markets to accelerate innovation to connect and secure the world. Learn more at Keysight Newsroom and www.keysight.com..

Keysight Contact:

Geri Lynne LaCombe, Americas/Europe
+1 303 662–4748
geri_lacombe@keysight.com

Fusako Dohi, Asia
+81 42 660–2162
fusako_dohi@keysight.com

The Keysight M8135A is a pre-configured USPA system for single channel transceiver applications.