What are you looking for?
Keysight Delivers Single Vendor Validation Solution for Seamless Support of PCIe® 5.0 and 6.0
Enables complete design cycle deployments in peripheral component interconnect express (PCIe)
SANTA ROSA, Calif. April 5, 2022
Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that delivers advanced design and validation solutions to help accelerate innovation to connect and secure the world, announced an end-to-end PCIe test solution for digital development and senior engineers that enable the simulation, pathfinding, characterization, validation and compliance testing of PCIe designs.
The rapid increase of AI (artificial intelligence) related workloads in data centers and edge computing demand new compute designs. Data center system designers are challenged to provide new higher speed devices within reduced design cycles. New PCIe devices will need to keep up with Ethernet network interfaces in data centers and the emergence of CXL (compute express link).
To maintain performance goals and prepare for the PCIe 6.0 move to pulse amplitude modulation 4-level (PAM4), customers need a smooth transition from PCIe 5.0 to 6.0, where the integrity of PCIe measurements are backed by leading-edge tools and comply with PCIe specifications. With shrinking design cycles, end-to-end solutions from simulation to validation through the layers of the stack are required.
Keysight provides a comprehensive physical layer test solution, approved by the Peripheral Component Interconnect Special Interest Group (PCI-SIG) to test transmitters and receivers for all generations of the PCIe specification, which is currently supported by the PCI-SIG integrators list. To reflect the increasing time to market pressure for design engineers, Keysight extends the portfolio to cover PCIe protocol, making it the first end-to-end solution from simulation to full stack validation.
"Keysight has been a member of the PCI-SIG since its founding in 1992 and has been on the PCI-SIG Board of Directors starting in 2007. Keysight participates in many working groups to enable testability and early availability of various standards to the industry," said Dr. Joachim Peerlings, vice president of network and data center solutions at Keysight Technologies. "Today, Keysight is launching a complete PCIe testing solution from simulation to protocol, enabling customers to evaluate and validate the true performance margins of their designs."
Keysight's new PCIe test solution leverages the company's physical layer-system simulation; physical layer interconnect, transmitter (Tx) and receiver (Rx) test; and shown for the first time at DesignCon – a new protocol layer test solution consisting of hardware and software products.
Key customer benefits include:
- Interoperability and support across the entire design cycle from a single-vendor.
- A Keysight Infiniium UXR-Series real-time oscilloscope for accurate PAM4 PCIe 6.0 Tx measurements and Rx calibrations to enable low intrinsic noise with 110 GHz bandwidth to provide future proof capabilities.
- Investment protection with the Keysight M8040A Bit Error Ratio Tester (BERT), which utilizes the same hardware for non-return to zero (NRZ) and PAM-4 measurements.
- Superior signal integrity that enables engineers to focus on protocol bugs rather than interposer signaling issues.
- Fast transmitter phased locked loop (PLL) bandwidth measurements to reduce the measurement time from hours to seconds.
- End-to-end verification of components and sub-systems across the product workflow with common software platforms and built-in test automation capabilities.
More information on Keysight's complete PCIe solution is available at www.keysight.com/find/PCIe.
PCI-SIG®, PCIe® and the PCI Express® are US registered trademarks and/or service marks of PCI-SIG.
About Keysight Technologies
Keysight delivers advanced design and validation solutions that help accelerate innovation to connect and secure the world. Keysight's dedication to speed and precision extends to software-driven insights and analytics that bring tomorrow's technology products to market faster across the development lifecycle, in design simulation, prototype validation, automated software testing, manufacturing analysis, and network performance optimization and visibility in enterprise, service provider and cloud environments. Our customers span the worldwide communications and industrial ecosystems, aerospace and defense, automotive, energy, semiconductor and general electronics markets. Keysight generated revenues of $4.9B in fiscal year 2021. For more information about Keysight Technologies (NYSE: KEYS), visit us at www.keysight.com.
# # #
Additional information about Keysight Technologies is available in the newsroom at https://www.keysight.com/go/news and on Facebook, LinkedIn, Twitter, and YouTube.
Keysight Contact:
Geri Lynne LaCombe, Americas/Europe
+1 303 662–4748
geri_lacombe@keysight.com
Fusako Dohi, Asia
+81 42 660–2162
fusako_dohi@keysight.com
Need to contact Media Relations at Keysight?