Filler panel kit for use with the E4360A Modular Solar Array Simulator Mainframe.

HIGHLIGHTS

Filler panel kit for use with the E4360A Modular Solar Array Simulator Mainframe. For proper operation of the E4360 Modular Solar Array Simulator, any empty slots must be filled with a filler panel. This filler panel kit provides one filler panel to fill one empty slot. Required when you have only one module installed in an E4360A mainframe.

The E4369A filler panel kit is also orderable as option FLR on the E4360A Modular Solar Array Simulator Mainframe.

Extend the Capabilities of Your Product

Want help or have questions?