Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Wireless Device Test Sets & Wireless Solutions

Keysight products provide mobile phone designers and manufacturers with increased measurement speeds, improved accuracy, and exceptional flexibility for testing mobile devices. Our one box test sets cover all the major technology formats: LTE-Advanced, LTE (FDD and TDD), GSM/GPRS/EGPRS/E-EDGE, W-CDMA/HSPA/HSPA+/DC-HSDPA, cdma2000®/1xEV-DO/eHRPD, TD-SCDMA/TD-HSDPA/TD-HSUPA, IS-95, TIA/EIA-136, AMPS, Bluetooth®, Bluetooth Enhanced Data Rate (EDR), Bluetooth Low Energy, ZigBee™, Wireless LAN (WLAN), 802.11a/b/g, 802.11n, NFC/EMV, MIMO, and WiMAX™.

Extend Keysight wireless test set capabilities with software products designed to streamline wireless measurements and automate testing for time consuming and complex measurement and analysis tasks. Software products are available for all wireless communications test set platforms-automating test for cellular mobile devices, WiMAX, LTE, and Bluetooth/WLAN devices.

Keysight systems integrate the instruments, cabling, and system hardware into a rack carefully designed to provide cooling, power, ergonomics, safety, and mechanical stability. Let Keysight help you ease the transition from design into high volume production quickly while reducing your cost of test, enabling you to reach profitability faster.

Related solutions from Anite

Anite is now part of Keysight Technologies. Anite’s Device & Infrastructure Testing business now conducts business as Keysight Technologies. Please see below information about Anite Conformance Toolset, Anite SAS Interoperability Testing, Propsim Channel Emulation Solutions, Anite Virtual Drive Testing Toolset and Anite Development Toolset. Please visit www.anite.com  for information related to Anite’s Network Testing business with its Nemo branded solutions.

51-75 of 879

Sort:
5G RF DVT Toolset - Solution Brief
This flyer introduces the Keysight 5G RF/RRM Design Verification toolset which is a comprehensive solution to address diverse global spectrum requirements and efficiently prototype advanced 5G RF/RRM features, including beamforming at mm-Wave frequencies and standalone/non-standalone use cases.

Solution Brief 2017-09-15

E7515A UXM Wireless Test Set - Brochure
The UXM is a highly integrated signaling test set created for functional & RF design validation in the 4G era & beyond. It delivers LTE-A cat 6 now & will handle increasingly complex cases later.

Brochure 2017-09-13

PDF PDF 1.29 MB
Keysight Technologies Selected by China Mobile Terminals for Cellular-IoT RF,RRM Conformance Testing
Collaboration enables chipset, module and device makers to optimize their designs and verify RF and RRM performance to China Mobile’s Cellular-IoT test plan

Press Materials 2017-09-04

Keysight Technologies Selected by Qualcomm for 5G Test Solutions
Keysight will provide the scalability and capability required to support 5G design and test–from initial requirements to final standards

Press Materials 2017-08-19

Narrowband IoT (NB-IoT): Cellular Technology for the Hyperconnected IoT - Application Note
This paper explains the underlying reasons why this technology is shaped as it is today and explore the challenges in adopting this new application and explains the new ways of securely roll out NB-IoT application quickly to market.

Application Note 2017-08-08

Keysight and Ixia Solutions Group Announce Integrated Cellular + WiFi Protocol Verification Solution
New test platform illustrates the impact Keysight's acquisition of Ixia is having in the wireless industry

Press Materials 2017-08-03

Collaboration with Sequans to Provide NB-IoT, LTE Cat-M1 Test Solutions

Press Materials 2017-08-03

E7760A Wideband Transceiver User's Guide
A guide to the screen interface and SCPI programming interface for the E7760A. Also: test scenarios, port usage, and information on the IEEE 802.11ad-2012 PHY radio standard.

User Manual 2017-07-01

PDF PDF 12.44 MB
Critical Test Parameters of NB-IoT, Test Challenges and Keysight Solution - Application Note
This application note describes some of the most relevant features of NB-IoT, which make it a strong candidate among the different Low Power Wide Area Network (LPWAN) options through use of Internet of Things.

Application Note 2017-06-05

X-Series Multi-touch Test Set User Documentation (webhelp)
Online documentation that includes programming information, SCPI commands, and more.

Help File 2017-06-05

802.11ad Integrated RF Test Solution - Data Sheet
The E7760A and M1650A provide IF (6-17GHz) and RF (55-68GHz) physical-layer signals for 802.11ad WiGig device testing. This document describes their performance and physical characteristics.

Data Sheet 2017-06-02

PDF PDF 1.44 MB
Keysight Technologies to Help RDA Microelectronics Accelerate NB-IoT Chipset Tests

Press Materials 2017-06-01

Keysight Technologies Enables Prototyping of Next-Generation 5G Mobile Devices
5G Protocol R&D Toolset is the first in a series of Keysight 5G Network Emulation Solutions to help you streamline your current and future 5G device workflow.

Press Materials 2017-05-23

Keysight Technologies Announces First Test Platform to Validate GCF RF NB-IoT and CAT-M Test Cases

Press Materials 2017-05-02

E7760A Wideband Transceiver Getting Started Guide
Safety information, basic instructions for use, operating tasks, and an introduction to the user interface and operating system.

User Manual 2017-05-01

PDF PDF 4.67 MB
E7760A Wideband Transceiver and M1650A mmWave Transceiver - Configuration Guide
This document guides the user through selecting the appropriate options for the E7760A and M1650A based on their intended use cases. It is applicable to both new purchases and upgrades.

Configuration Guide 2017-04-25

PDF PDF 1.16 MB
Keysight Technologies to Help China Telecom Accelerate NB-IoT Device Test

Press Materials 2017-04-18

Keysight Helps Accelerate Deployment of IoT Technology Using Qualcomm™ Technologies' LTE IoT Modems

Press Materials 2017-03-22

E6650A EXF Wireless Test Set for Femtocell You Tube
E6650A EXF Wireless Test Set for Femtocell You Tube

Demo 2017-03-15

E7521A GSM/GPRS/EGPRS Test Application Online Documentation (.chm)
This help describes how to use the E7521A GSM/GPRS/EGPRS Test Application for software revision 1.6.1.x. You must copy this file to your PC (or the UXM) in order to view its contents.

Help File 2017-03-01

CHM CHM
E7515A UXM Firmware Update Tool Installation and User Guide
Instructions and user information on how to use the E7515A firmware update tool.

User Manual 2017-03-01

PDF PDF 672 KB
E7523A W-CDMA Test Application Help (.chm file)
This Help file describes the settings and remote programming commands (SCPI) for the E7523A W-CDMA software applications. Refer to the topic: Using Help > Updating the Help File in this chm for instructions for replacing the context-sensitive help in your UXM. You must copy this file to your PC (or the UXM) in order to view its contents. system functions, and measurement functions.

Help File 2017-03-01

Eye on 802.11ax:What It Is and How to Overcome the Design & Test Challenges It Creates - White Paper
This white paper introduces key technologies of 802.11ax and presents some unique challenges for the engineers designing and testing 802.11ax devices.

Application Note 2017-02-28

PDF PDF 2.52 MB
Integrated 802.11ad RF Test Solution - Brochure
Design your 802.11ad device with confidence. Frequencies are 10 times higher, modulation bandwidths are 100 times wider, and modulation is now a mixture of modes.

Brochure 2017-02-03

PDF PDF 622 KB
T4010S Conformance Test System - Technical Overview
The T4010S LTE RF test systems are automated solutions for conformance test and design verification of LTE UE. This document covers key benefits, features, technical specifications and ordering info.

Technical Overview 2017-01-24

Previous 1 2 3 4 5 6 7 8 9 10 ... Next

Related Industries & Technologies