Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

Discontinued Automated X-ray Inspection

Keysight is exiting the automated optical and automated x-ray inspection business. Keysight will honor all existing warranty and support contracts and offer spare parts, time and materials services, and self support options until end-of-support, which is seven years from product discontinuance, starting March 1st, 2009.

For the list of frequently asked questions on this exit announcement, please visit www.keysight.com/find/inspection.

Keysight remains fully committed to expand the product offerings in its In-Circuit Test (ICT) and Functional Test product families in the printed circuit board assembly test market.

26-50 sur 60

Tri:
Carrier Usage with the 5DX Automated X-ray Inspection System
Carriers can be used successfully in the 5DX Automated X-ray Inspection system. Several factors need to be considered when designing a carrier. This document outline the factors that should be considered in the carrier design.

Notes d’application 2006-09-21

Considerations for Surface Map Setup
The concept of delta-Zs is perhaps the most difficult thing to understand about the surface map process.

Notes d’application 2006-08-08

Gauge Repeatability on 5DX X-ray System
Summary of 5DX repeatability capability, factors that influence the repeatability capabilities of the 5DX, impacts to gauge repeatability and reproducibility (GR&R) results.

Notes d’application 2005-03-09

PDF PDF 102 KB
Test and Inspection as Part of the Lead-free Manufacturing Process
The paper addresses issues that will impact defect levels and defect spectrum during the transition to lead-free manufacturing. It also addresses different test and inspection systems’ readiness to test lead-free printed circuit board assemblies.

Notes d’application 2005-02-22

PDF PDF 421 KB
Testing FPGullwing Misalignment Across the Pad
A technique is described which enables detection of misalignment of gullwing joints across the joint using duplicate components and FPGullwing Misalignment.

Notes d’application 2004-12-08

PDF PDF 1.58 MB
Understanding the PCAP Polarity Reject Signal
This paper describes the algorithm used to determine if polarized capacitors are properly oriented.

Notes d’application 2004-12-02

PDF PDF 1.09 MB
Handling Surface Mapping with Varying Board Construction
This paper describes a method for dealing with lot-to-lot or supplier-to-supplier variations in board construction. Often the variations in board construction result in different color boards which otherwise cause problems with surface mapping.

Notes d’application 2004-12-02

PDF PDF 1.02 MB
Understanding and Configuring the 5DX Selftest and Black/White Level Tests
This paper discusses the theory and practice of 5DX automatic compensation tools, Selftest and gray level correction.

Notes d’application 2004-12-01

PDF PDF 158 KB
How and Why: Confirmation and Adjustments
This paper describes the process of and reason for periodic adjustment of a 5DX system using the confirmation and adjustment panel.

Notes d’application 2004-12-01

PDF PDF 636 KB
Instructions for Using One Confirmation and Adjustment Panel with Multiple Systems
Readjusting the thickness table setting for one machine, using the Confirmation and Adjustment Panel, and adjustment data for a second machine, improves the portability of applications between the two machines.

Notes d’application 2004-08-26

The Importance of Test and Inspection When Implementing Lead-Free Manufacturing
Many papers, articles, and studies have been written about process issues, reliability issues, repair issues, and the merits of different alloys. This paper addresses the impacts on test and inspection when going lead-free.

Notes d’application 2004-08-20

PDF PDF 260 KB
PLR and 5DX Customized Defect Names Implementation
You can use customized defect names on both the 5DX and on the PLR. This is particularly valuable when you want to display defect names in a local language.

Notes d’application 2003-03-01

What to Consider When Selecting the Optimal Test Strategy
This paper addresses several issues for selecting the optimal inspection strategy, presenting data from many studies that Keysight has performed in the quest to find the optimal test / inspection strategy.

Notes d’application 2003-03-01

PDF PDF 175 KB
When to Use AOI, When to Use AXI, and When to Use Both
by Stig Oresjo, senior test strategy consultant at Keysight Technologies.

Notes d’application 2002-12-01

PDF PDF 70 KB
Interactive Board Complexity Calculator
Calculate Your Board's Complexity Index.

Notes d’application 2002-11-01

Preparing a .cc File for Export to Test Link
This procedure describes the process of converting ECAD data into a form that can be used by Test Link.

Notes d’application 2002-10-16

PDF PDF 70 KB
Remote Network Connections Creation for the Operator Logon
Operator logon on the Keysight 5DX Series II System is limited, in that it does not allow Operator to make network connections that are required for sending images and res files to the PLR workstation.

Notes d’application 2002-06-30

Using NDFCOL.EXE, the NDF "Line Up the Columns" Utility
NDFCOL.EXE is a handy little utility that will form neat columns of data in NDF files.

Notes d’application 2002-06-06

Obtaining a Listing of Applications on Series II Systems
There is currently no easy way to obtain a list of all resident applications on a 5DX System or TDW. It is difficult to match panel name with hash name and see when the application was last updated.

Notes d’application 2002-06-01

Sampling on the Keysight 5DX
Sampling Mode allows test coverage to be optimized with line speed. This document explore the setup procedure for the Keysight 5DX for sampling.

Notes d’application 2002-05-08

The Life of a 5DX Inspection C# File
The {Hashed Panel Name}.C# file is basically cad information about a panel program. It is used in conjunction with various utilities to overlay cad data on images or provide cad data for filters.

Notes d’application 2001-10-16

PDF PDF 97 KB
Version 7.x ASAP Best Practices
In an effort to standardize programming practices for the Keysight 5DX, Keysight has created a set of procedures representing 5DX "best practices" that address various aspects of the programming process.

Notes d’application 2001-07-25

Comparing AOI and AXI
Choosing the right technology requires looking at board mix, capital budget and other business considerations. But most of all, you need to understand the typical characteristics of each technology.

Notes d’application 2001-07-25

PDF PDF 42 KB
Rotating Boards on a Panel
Rotating Boards on a Panel if often necessary. In addition to the software revisions named within, the explained technique in the document is utilized for for 4.x, 5.x, 6.x and 7.x. For 8.x Test Link deals with this automatically.

Notes d’application 2001-05-17

PDF PDF 40 KB
Series II Compliance with the Machinery Directive (in Europe) - specific installation procedures
Series II will meet requirements of Machinery Directive in European Community member countries, if the following steps, which are described in the document, are taken during installation of equipment.

Notes d’application 2001-05-17

Précédente 1 2 3 Page suivante