Here’s the page we think you wanted. See search results instead:

 

Sprechen Sie mit einem Experten

Wireless Network Emulators

Keysight’s industry leading wireless network emulators enable the entire mobile device ecosystem to accelerate delivery of 5G new radio (NR) products to market by streamlining the workflow from early prototyping, development, and design verification to conformance, carrier acceptance, and high volume manufacturing.

Leading chipset and device makers, as well as mobile operators, use Keysight’s first-to-market end-to-end wireless network emulator solutions for comprehensive protocol, RF, functional, and performance testing of 5G chipsets and devices. Common development tools allow users to efficiently develop by eliminating siloed data sets and sharing design insights gained across each stage of the wireless device lifecycle. And to address diverse global spectrum requirements, Keysight’s 5G test solutions seamlessly scale in a simple, compact form factor to support FR1 (sub-6GHz) and FR2 (mmWave) frequencies.

Proven in collaborations with the 5G market leaders, Keysight wireless network emulators are uniquely positioned to address new 5G NR challenges related to more bands and bandwidth, mmWave frequencies, higher order MIMO, and beamforming. The solution software continues to evolve rapidly to stay current with the latest 5G and 4G standards. Keysight combines its network emulation solutions with a wide range of purpose-built chambers to deliver comprehensive mobile device performance validation capabilities in over-the-air (OTA) test environments.

Related solutions from Anite

Anite is now part of Keysight Technologies. Anite’s Device & Infrastructure Testing business now conducts business as Keysight Technologies. Please see below information about Anite Conformance Toolset, Anite SAS Interoperability Testing, Propsim Channel Emulation Solutions, Anite Virtual Drive Testing Toolset and Anite Development Toolset. Please visit www.anite.com  for information related to Anite’s Network Testing business with its Nemo branded solutions.

251-275 of 412

Sort:
N4010A Bluetooth Online User's Guide
Keysight N4010A Wireless Connectivity Test Set online, interactive help. Bluetooth.

User Manual 2006-09-06

Add Fast Switch Capability and Speed Improvement - E5515-90089
Install note for adding Fast Switch capability and speed improvement

Installation Manual 2006-08-31

PDF PDF 46 KB
E1962B/E6702B/T GPIB Syntax Guide for Rev. B.11/B.04/T.00
Printable GPIB command Syntax Guide for the cdma2000/IS-95/AMPS applications.

User Manual 2006-06-28

PDF PDF 966 KB
E1961A GPIB Syntax Guide for Rev. A.11.20
Printable GPIB command syntax guide for the AMPS/136 application.

User Manual 2006-06-28

PDF PDF 12.49 MB
E6569C Release Notes
Software release information for the E6569C wireless test manager suite.

Release Notes 2006-06-08

Add additional capability to the E5515B or E5515C - E5515-90323
Installation note for adding additional capability to the E5515B or E5515C

Installation Manual 2006-04-26

PDF PDF 58 KB
Installing the Digital Link Sub System - E5515-90286
Install note for installing the Digital Link Sub System

Installation Manual 2006-04-25

PDF PDF 43 KB
Install the Host Processor Assembly - E5515-90292
Install note for installing the Host Processor Assembly

Installation Manual 2006-04-25

PDF PDF 45 KB
Installing the ADC Board - E5515-90290
Install note for installing the ADC Board

Installation Manual 2006-04-24

PDF PDF 42 KB
Component Level Information Packet

Service Manual 2006-04-03

PDF PDF 20.06 MB
E1968A,E6701D/E,E6704A GPIB Syntax Guide for Rev. A.06/D.03/E.00
Printable GPIB Syntax Guide for the GSM/GPRS/EGPRS applications.

User Manual 2006-03-20

PDF PDF 1.17 MB
Add Option 002 Second Source to E5515B and E5515C - E5515-90308
Installation note for adding Option 002 Second Source to E5515B and E5515C

Installation Manual 2006-03-20

PDF PDF 566 KB
E6701E/E6704A GSM/GPRS/EGPRS CHM Help File for Rev E.00.08
Downloadable version of the Online User's Guide for the GSM/GPRS/EGPRS applications. (Windows Only)IMPORTANT: Save the file to your desktop. For Windows XP, right-click on the file and select Properties>>Unblock.

User Manual 2006-03-12

FILE FILE 6.45 MB
N4010A Bluetooth Tx/Rx EDR dll User's Guide
Downloadable version of the Online User's Guide for the EDR application. (Windows Only) IMPORTANT: Save the file to your desktop. For Windows XP, right-click on the file and select Properties>>Unblock.

User Manual 2005-11-28

FILE FILE 237 KB
Add Option 003 to the E5515C - E5515-90294
Install note for adding option 003 to the E5515C

Installation Manual 2005-11-16

PDF PDF 134 KB
Transitioning from an E1985 to an E1987A
Recommendations for going from an E1985 to an E1987A

User Manual 2005-11-02

PDF PDF 38 KB
Add Option 002 Second Source and EDGE Hardware - E5515-90309
Installation note for adding Option 002 Second Source and EDGE Hardware

Installation Manual 2005-03-20

PDF PDF 647 KB
Adds EGPRS capability to the E5515B and E5515C - E5515-90310
Installation note for adding EGPRS capability to the E5515B and E5515C

Installation Manual 2005-03-20

PDF PDF 203 KB
RF Interface Kit Removal/Installation for single or two port RF Interface Setups - E5515-90056
Installation instructions for the RF Interface Kit Removal/Installation for single or two port RF Interface Setups

Installation Manual 2005-03-07

PDF PDF 282 KB
Upgrade Instructions for Option 006 upgrade kit for E5515C - E5515-90212
Upgrade Instructions for Option 006 upgrade kit for E5515C

Installation Manual 2005-03-07

PDF PDF 351 KB
E1968A/E6701D/E6704A CHM Help File for Rev. A.04/D.01
Downloadable version of the Online User's Guide for the GSM/GPRS/EGPRS applications. (Windows Only) IMPORTANT: Save the file to your desktop. For Windows XP, right click on the file and select Properties>>Unblock.

User Manual 2005-01-18

HTML HTML 6.01 MB
E1987A/E1985B/C/E and E6785B/C CHM Help File
Alternative to our online User's Guide, allows you to download entire documentation to your PC. Windows only.

User Manual 2005-01-18

HTML HTML 329 KB
E6719B Release Notes
Software revision history for the E6719B lab application suite.

Release Notes 2004-12-23

HTML HTML 4 KB
E6564A Release Notes
The latest software revision information for the E6564A 1xEV-DO Wireless Test Manager.

Release Notes 2004-11-12

E6563A AMPS/136 Wireless Test Manager Release Notes
Describes the features in the E6563A AMPS/136 Wireless Test Manager releases. This document contains the original features, as well as enhancements that have been added over time.

Release Notes 2004-11-12

Previous ... 11 12 13 14 15 16 17 Next

Industriebereiche & Technologien