PXI/USB VNA HTML Help (.CHM)

Download and install the simulator from www.keysight.com/find/pxiusbvna-firmware. The CHM file is located under C:\Program Files\Keysight\Network Analyzer\Help. The help file does not show if it is saved in remote directory. You can copy it on different place in the local HDD. If you encounter a problem to view, right-click on the file, click Properties, then click Unblock