WEBVTT

1
00:00:04.120 --> 00:00:06.640
<b>Smart electrification of cars and laboratories</b>

2
00:00:06.640 --> 00:00:09.200
<b>is key for the cost-effective decarbonization</b>

3
00:00:09.200 --> 00:00:10.840
<b>pathways for e-mobility.</b>

4
00:00:12.240 --> 00:00:14.600
<b>The electrification of cars in a mass scale</b>

5
00:00:14.600 --> 00:00:17.880
<b>starts in the first steps in huge smart laboratories.</b>

6
00:00:19.640 --> 00:00:22.080
<b>Just like for the vehicles, the principle applies</b>

7
00:00:22.080 --> 00:00:24.480
<b>to the laboratories that they must be designed</b>

8
00:00:24.480 --> 00:00:26.200
<b>as efficiently as possible.</b>

9
00:00:33.840 --> 00:00:36.880
<b>As a consultant, I evaluate test equipment</b>

10
00:00:36.880 --> 00:00:39.520
<b>for batteries and cells which are energy efficient</b>

11
00:00:39.520 --> 00:00:42.880
<b>but also can reduce the total cost of ownership for the cu</b>s<b>tomers.</b>

12
00:00:47.760 --> 00:00:50.360
<b>Since energy prices soared in 2022, </b>

13
00:00:50.360 --> 00:00:53.800
<b>energy intensive industries like car makers or test labs</b>

14
00:00:53.800 --> 00:00:56.400
<b>needs to look into their efficiencies a lot more</b>

15
00:00:56.400 --> 00:00:58.400
<b>to reduce the cost of testing.</b>

16
00:01:01.640 --> 00:01:04.000
<b>Not only do they need to be operationally efficient,</b>

17
00:01:04.000 --> 00:01:06.280
<b>but under the pressure of their customers they now need</b>

18
00:01:06.280 --> 00:01:08.520
<b>to look into reducing the cost of energy</b>

19
00:01:08.520 --> 00:01:10.560
<b>to reduce the cost of the service they offer</b>

20
00:01:10.560 --> 00:01:11.640
<b>to their customers.</b>

21
00:01:15.160 --> 00:01:18.160
<b>As a result, low efficiency testing equipment</b>

22
00:01:18.160 --> 00:01:20.280
<b>will become obsolete in mature markets</b>

23
00:01:20.280 --> 00:01:22.800
<b>like Europe or America in the near future.</b>

24
00:01:27.280 --> 00:01:29.680
<b>At Keysight, we understand efficiency in laboratories</b>

25
00:01:29.680 --> 00:01:31.440
<b>to mean two main areas: </b>

26
00:01:31.440 --> 00:01:33.640
<b>Power efficiency and operational efficiency.</b>

27
00:01:34.280 --> 00:01:36.920
<b>We guarantee power efficiency by using the latest</b>

28
00:01:36.920 --> 00:01:39.480
<b>semiconductors and sophisticated control strategies.</b>

29
00:01:39.480 --> 00:01:41.120
<b>With our partially patented approaches,</b>

30
00:01:41.120 --> 00:01:44.320
<b>we guarantee high efficiency of the battery test systems</b>

31
00:01:44.320 --> 00:01:47.520
<b>of over 95% for a wide power range</b>

32
00:01:47.520 --> 00:01:49.080
<b>under real test conditions.</b>

33
00:01:50.960 --> 00:01:52.240
<b>But that’s not all,</b>

34
00:01:52.240 --> 00:01:54.560
<b>The operation of a large laboratories with thousands</b>

35
00:01:54.560 --> 00:01:57.240
<b>of test channels with different test procedures </b>

36
00:01:57.240 --> 00:01:59.960
<b>also requires a sophisticated operating strategy.</b>

37
00:02:00.920 --> 00:02:03.560
<b>So it is important to develop an operational strategy</b>

38
00:02:03.560 --> 00:02:05.040
<b>for the individual lab.</b>

39
00:02:05.040 --> 00:02:08.080
<b>A very simple measure is to switch on only those systems</b>

40
00:02:08.080 --> 00:02:10.680
<b>that really make a test contribution at that moment.</b>

41
00:02:11.320 --> 00:02:12.480
<b>This lowers the grid load.</b>

42
00:02:13.360 --> 00:02:15.360
<b>We also must keep the ratio between</b>

43
00:02:15.360 --> 00:02:18.400
<b>peak power and average power for the laboratories </b>

44
00:02:18.400 --> 00:02:21.120
<b>to the minimum grid load as small as possible.</b>

45
00:02:22.080 --> 00:02:24.360
<b>This can be done through the regenerative</b>

46
00:02:24.360 --> 00:02:26.280
<b>use of energy in the test systems,</b>

47
00:02:26.280 --> 00:02:29.640
<b>and delivered via our sophisticated Pathwave Lab Operations </b>

48
00:02:29.640 --> 00:02:31.640
<b>for battery test software to ensure</b>

49
00:02:31.640 --> 00:02:34.480
<b>the operational efficiency of the individual laboratory.</b>

50
00:02:41.160 --> 00:02:44.200
<b>Since 2011, it is our mission to support our customers</b>

51
00:02:44.200 --> 00:02:47.040
<b>in the development of high-performance battery systems </b>

52
00:02:47.040 --> 00:02:49.280
<b>to make them efficient and durable</b>

53
00:02:49.280 --> 00:02:51.400
<b>to accelerate the transformation to a</b>

54
00:02:51.400 --> 00:02:53.400
<b>CO2-neutral mobility.</b>

55
00:02:53.560 --> 00:02:55.480
<b>For this purpose, we build and operate</b>

56
00:02:55.480 --> 00:02:58.080
<b>state-of-the-art test benches in Bochum.</b>

57
00:02:58.080 --> 00:03:00.640
<b>On more than 4,600 square meters of</b>

58
00:03:00.640 --> 00:03:02.480
<b>laboratory space, we are testing</b>

59
00:03:02.480 --> 00:03:04.640
<b>cells, modules, and battery systems.</b>

60
00:03:05.000 --> 00:03:07.480
<b>We also use modular configurable</b>

61
00:03:07.480 --> 00:03:10.120
<b>Keysight cell and battery testers in our laboratories, </b>

62
00:03:10.120 --> 00:03:13.800
<b>which deliver reproducible and precise results.</b>

63
00:03:15.120 --> 00:03:17.040
<b>Our test bench automation reduces</b>

64
00:03:17.040 --> 00:03:18.960
<b>the energy consumption of the </b>

65
00:03:18.960 --> 00:03:20.520
<b>laboratories to a minimum.</b>

66
00:03:22.440 --> 00:03:24.920
<b>This is how Keysight supports customers towards a </b>

67
00:03:24.920 --> 00:03:27.600
<b>cleaner, cost-effective decarbonization, </b>

68
00:03:27.600 --> 00:03:30.200
<b>and more sustainable world through the power </b>

69
00:03:30.200 --> 00:03:32.160
<b>of future-oriented electric vehicle test.</b>