您希望搜索哪方面的内容?
Keysight’s New Test Solution Optimizes Performance of 5G Devices that Use MIMO Technology to Increase Data Throughput
Combines network and channel emulation solutions with over-the-air chambers and test cases
SANTA ROSA, Calif., July 7, 2020
Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that helps enterprises, service providers and governments accelerate innovation to connect and secure the world, has launched a new test solution that optimizes the performance of 5G devices that use MIMO* and massive MIMO technology to increase data throughput and improve network capacity.
Keysight's S8708A Advanced Performance Test Toolset enables an ecosystem consisting of eighty-four 5G device vendors to validate device performance under accurate and real-world conditions using 3D fading and mobility scenarios. Keysight's new toolset includes the company's PROPSIM FS16 or F64 channel emulator, UXM 5G Wireless Test Platform and 3D OTA multiprobe anechoic chambers, and supports test cases specified by 3GPP for MIMO over-the-air (OTA) testing in study item (TR38.827), which included contributions from Keysight.
"Adding advanced performance test capabilities to Keysight's network and channel emulation solutions enables an ecosystem investing in MIMO and massive MIMO technology to accelerate the launch of high performing 4G and 5G devices," said Kailash Narayanan, vice president of Keysight and general manager of Keysight's wireless test group. "Keysight's system solution, which includes 3D multiprobe anechoic chambers, provides for 5G device performance optimization across the full protocol stack in a frequency range 2 (FR2) OTA test environment."
Keysight's Advanced Performance Test Toolset, part of the company's suite of 5G device test solutions:
- uses common logging, analysis and channel modeling tools to speed testing across the workflow in MIMO OTA test environments.
- enables chipset and device makers, as well as test houses and mobile operators, to validate beam management, MIMO antenna performance and maximum data throughput of a 5G device across different massive MIMO configurations and 3D special fading conditions.
- allows users to gain access to geometric channel models with high-capacity fading options as well as test cases specified by 3GPP across FR1 and FR2.
- enables users to verify how a device performs by stressing the design in a 3D OTA test environment that uses multi-beam technology and multiple angles of arrival (AoA) to create accurate and realistic conditions.
*MIMO (multiple input, multiple output) – an antenna technology for wireless communications in which multiple antennas are used at both the source (transmitter) and the destination (receiver).
Additional Information
Additional information is available at https://www.keysight.com/en/pd-3068776-pn-S8708A/5g-advanced-performance-test-toolset?nid=-31763.1292512&cc=GB&lc=eng.
Images are available at https://www.keysight.com/find/APT-system-images.
About Keysight Technologies
Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps enterprises, service providers and governments accelerate innovation to connect and secure the world. Keysight's solutions optimize networks and bring electronic products to market faster and at a lower cost with offerings from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $4.3B in fiscal year 2019. More information is available at www.keysight.com.
# # #
Additional information about Keysight Technologies is available in the newsroom at https://www.keysight.com/go/news and on Facebook, LinkedIn, Twitter, and YouTube.
Keysight Contact:
Geri Lynne LaCombe, Americas/Europe
+1 303 662–4748
geri_lacombe@keysight.com
Fusako Dohi, Asia
+81 42 660–2162
fusako_dohi@keysight.com
Need to contact Media Relations at Keysight?