Evaluating Electrical Performance in Electrical-Optical-Electrical Link Systems
  • Cursos
  • 1 Itens

Data centers transport vast amounts of data using optical fiber connections. To truly understand and evaluate the electrical system’s performance, consider the entire link condition, which includes the optical channel under electrical-optical-electrical (E-O-E) systems. In this webinar, we examine a design approach for E-O-E systems that predicts design margin, such as eye height and eye width, at the desired system bit error rate.