Learn the Basics of Signal Generator Accuracy
Jumping into the world of signal generators for the first time can be a daunting journey. There are lots of technical considerations, and it is not always obvious which ones are the most important to focus on. In this article, I will provide guidance on the things you need to be aware of when selecting an RF signal generator.
What is a Signal Generator?
Signal generators provide precise, highly stable, and customizable test signals for a variety of components and system test applications that emulate real-world scenarios. The outputs can be anything from a simple continuous wave to more complex modulated digital signals. Signal generators are an important part of product development because they enable you to apply signal impairments to test your product in various conditions within and beyond design limitations.
What Affects Signal Generator Accuracy?
Amplitude Accuracy
Amplitude accuracy compares the proximity of the signal generator’s output to the desired amplitude set by a user. If we use the example of frequency sweeping to test filters and power amplifiers, choosing a signal generator with a tighter amplitude frequency specification provides a more uniform output across a frequency range. Figure 1 illustrates the flatness of a signal generator when determining the amplitude accuracy across a group of frequencies.
Frequency Accuracy
Two key factors for understanding the accuracy of a generated frequency are the stability of the reference oscillator and the time between source calibrations. The time between calibrations is also known as the ageing effect. Frequency accuracy is vital to RF applications especially where bands have data that are closer together. For example, in wireless communications, it is important to understand how well a receiver can process a signal while rejecting the signal from an adjacent channel. Poor frequency accuracy will cause the signals to be too close or too far and give a misleading indication of the performance for the device under test (DUT).
Spectral Purity
Every signal generator has unwanted amplitude and phase fluctuations on a signal that naturally occurs. Regardless of a source's signal stability, choosing a signal generator that has better spectral accuracy compared to the system requirements will prevent you from measuring the signal generator performance versus the DUT. Spectral purity is characterized by evaluating harmonics, sub-harmonics, spurs, and phase noise. In datasheets, it's common to see the spectral purity represented as the single side band (SSB) phase noise.
EVM Measurement
Error vector magnitude (EVM) is the vector difference between the ideal reference signal and the measured signal at a given time, as depicted in the Figure 4. This is commonly used to define the performance of a digital radio transmitter or receiver. Signal generators designed with smaller EVM percentages enable you to design and test systems to reach higher data capacity, better power efficiency, and increase wideband signal power.
The Impact of Distortion on Performance
Spectral regrowth refers to the distortion generated by amplitude and phase shifts in digital modulations. Spectral regrowth spreads outside the main channel and adjacent channel power ratio (ACPR) measurements enable examination of this characteristic. Similar to spectral purity, it’s important to choose a signal generator with a superior distortion test margin that won’t mask the performance of the DUT.
Learn More
Watch an in-depth training course on Keysight University: Introduction to Signal Generators. The learn more about signal generators visit our product landing page.